Hi,
We're currently using TMS320DM6467 processor on one of our new designs. We have the following questions related to the Davinci Processor
1. We're not planning to use the Ethernet interface and VLYNQ interface
on the TMS320DM6467. Can the pins be left as no connects or do we need
to connect pull-ups for some of them?
2. Is there any termination length requirement for the J19,J21 and R19, R21 pair?
Thanks