This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 DDR2 SDRAM DQS signaling configuration



The DQS signaling configuration seems to mismatch. The DQS traces in the datasheet are routed differentially, but the configuration by EMRS Command in Table 13 on the User's Guide (SPRUFI2) is the disabled differential signaling (/DQS enable = 1b). Is the value in Table 13 mistake? Is the correct value 0b?

When the DDR_DDQS bit in the SDCR is 1 (Differential DQS), is the /DQS enable set to 0b (enabled /DQS) by EMRS Command?

Best regards,

Daisuke

 

  • Hi,

    Please give me an answer as soon as possible. Your prompt reply would be appreciated.

    Best regards,

    Daisuke

     

  • Hi,
     
    In our customer boards, a read/write access can succeed, but the DQSn (negative) signal does not work correctly. The DQSn can be output at a write access, but it is always low at a read access.
     
    To configure the DDR2, the following UBL is used. The DDR_DDQS bit in the SDCR is set to 1b (Differential) in the UBL. Please see the DEVICE_DDR2Init() in the attached file.
     
    http://processors.wiki.ti.com/index.php/DaVinci_PSP_03.01_GA_(r39)_Release_Notes
     
    http://arago-project.org/files/releases/davinci-psp_03.01.01.39/sources/flash-utils-davinci.tar.gz
    \flash-utils\DM36x\Common\src\device.c

    /* --------------------------------------------------------------------------
      FILE        : device.c 				                             	 	        
      PROJECT     : TI Booting and Flashing Utilities
      AUTHOR      : Sandeep Paulraj
      DESC        : This file provides low-level, device-specific init functions
                    for use the DM36x device.
    -------------------------------------------------------------------------- */ 
    
    // General type include
    #include "tistdtypes.h"
    
    // This module's header file
    #include "device.h"
    
    // Debug module
    #include "debug.h"
    
    // Utility functions
    #include "util.h"
    
    //#define ARM270_DDR216_OSC24
    /************************************************************
    * Explicit External Declarations                            *
    ************************************************************/
    
    extern __FAR__ VUint32* DDRStart;
    
    
    /************************************************************
    * Local Macro Declarations                                  *
    ************************************************************/
    
    
    /************************************************************
    * Local Typedef Declarations                                *
    ************************************************************/
    
    
    /************************************************************
    * Local Function Declarations                               *
    ************************************************************/
    
    
    /************************************************************
    * Local Variable Definitions                                *
    \***********************************************************/
          
    
    /************************************************************
    * Global Variable Definitions                               *
    ************************************************************/
    
    const String devString = "DM36x";
    #define GPINT_GPEN		(unsigned int *)(0x01C21C08)		// WDT special function
    #define GPTDAT_GPDIR	(unsigned int *)(0x01C21C0c)		// WDT special function
    #define TMPBUF          (unsigned int *)(0x17ff8)
    #define TMPSTATUS		(unsigned int *)(0x17ff0)
    #define FLAG_PORRST		0x00000001
    #define FLAG_WDTRST		0x00000002
    #define FLAG_FLGON		0x00000004
    #define FLAG_FLGOFF		0x0000001
    
    static const Uint16 DDR_T_RFC = 1275;
    static const Uint16 DDR_T_RP = 200;
    static const Uint16 DDR_T_RCD = 200;
    static const Uint16 DDR_T_WR = 150 ;
    static const Uint16 DDR_T_RAS = 450;
    static const Uint16 DDR_T_RC = 650;
    static const Uint16 DDR_T_RRD = 100;
    static const Uint16 DDR_T_WTR = 100;
    static const Uint32 DDR_T_RASMAX = 700000;
    static const Uint16 DDR_T_XP = 2;
    static const Uint16 DDR_T_XSNR = 1375;
    static const Uint16 DDR_T_XSRD = 199;
    static const Uint16 DDR_T_RTP = 75;
    static const Uint16 DDR_T_CKE = 3;
    static const Uint16 DDR_RR = 78;
    
    
    /* PLL Divider settings for Various ARM/DDR Frequencies */
    #if defined(ARM297_DDR270_OSC24)
    
    #define PLL1_MUL		0x2d  
    #define PLL1_PREDIV		0x3
    #define PLL1_POSTDIV		0x0 	//PLL1 output ( 0x2d * 2* 24 / (0x3+ 1) = 540 MHZ )
    	
    #define PLL1_DIV1		0x2c	//USB 12 MHZ
    #define PLL1_DIV2		0x1	// POST DIV 540/2 -> HDVICP max =270 MHZ 
    #define PLL1_DIV3		0x1	// POST DIV 540/2  -> MJCP/HDVICP  max =270 MHZ 
    #define PLL1_DIV4		0x3	// POST DIV 540/4  -> EDMA/EDMA CFG	MAX =135 MHZ 
    #define PLL1_DIV5		0x1	// POST DIV 540/2 -> VPSS 	max =270 MHZ
    #define PLL1_DIV6		0x13	// 27Mhz POST DIV 540/20  -> VENC 27 MHZ	
    #define PLL1_DIV7		0x0	// POST DIV 540/2 -> DDR max =270 MHZ
    #define PLL1_DIV8		0x05	// POST DIV 540/6 -> 90 MMC0/SD0 <=100
    #define PLL1_DIV9		0x1	// POST DIV 540/2 -> CLKOUT
    
    
    #define PLL2_MUL		0x63
    #define PLL2_PREDIV		0x7
    #define PLL2_POSTDIV		0x0	//PLL2 Output (0x63 * 2 * 24 / (0x7 + 1) = 594MHZ
    
    #define PLL2_DIV1		0x18	// 594/25 23.6 MHZ USB
    #define PLL2_DIV2		0x1  	// 594/2 =297 Mhz -> ARM 
    #define PLL2_DIV3		0x1	// 297 MHZ 2 * ddr
    #define PLL2_DIV4		0x1c 	// POST DIV 594/29 = 20.48 -> VOICE
    #define PLL2_DIV5		0x07 	// POST DIV 594/8 = 74.25 ->VIDEO HD
    
    #define PERIPHERAL_CLK_CTRL_VAL	0x243F04FC
    
    #define DDR_FREQ	 270
    
    #elif defined(ARM270_DDR216_OSC24)
    
    #define PLL1_MUL		0x9  
    #define PLL1_PREDIV		0x0
    #define PLL1_POSTDIV		0x0 	//PLL1 output ( 0x9 * 2* 24 = 432 MHZ )
    
    #define PLL1_DIV1		0x11	// POST DIV 432/18 ->24 mhz
    #define PLL1_DIV2		0x1	// POST DIV 432/2  -> HDVICP max =216 MHZ
    #define PLL1_DIV3		0x1	// POST DIV 432/2  -> MJCP/HDVICP
    #define PLL1_DIV4		0x3	// POST DIV 432/4  -> EDMA/EDMA CFG
    #define PLL1_DIV5		0x1	// POST DIV 432/2 -> VPSS
    #define PLL1_DIV6		0x5	// POST DIV 432/(5+1) 72  -> VENC	
    #define PLL1_DIV7		0x0	// POST DIV 432 -> DDR
    #define PLL1_DIV8		0x04	// POST DIV 432/5 ->  86 MMC0/SD0
    #define PLL1_DIV9		0x1	// POST DIV 432/2 -> CLKOUT
    
    #define PLL2_MUL		0x2D
    #define PLL2_PREDIV		0x7
    #define PLL2_POSTDIV		0x0 	//PLL2 Output (0x2D * 2 * 24 / (0x7 + 1) = 270 MHZ
    
    
    #define PLL2_DIV1		0xA	// USB 24.5  MHZ
    #define PLL2_DIV2		0x0  	// 270 =270 Mhz -> ARM 
    #define PLL2_DIV3		0x0	// 270 2* DDR
    #define PLL2_DIV4		0x05 	// POST DIV 270/6  -> VOICE
    #define PLL2_DIV5		0x09 	// POST DIV 270/10 = 27 MHZ ->VIDEO HD
    
    #define PERIPHERAL_CLK_CTRL_VAL	0x243F04FC
    
    #define DDR_FREQ	 216
    
    #elif defined(ARM297_DDR277_OSC27) 
    
    #define PLL1_MUL		0x2c
    #define PLL1_PREDIV		0x03
    #define PLL1_POSTDIV		0x0 	//PLL1 output ( 0x2c * 2 * 27 /4  = 594 MHZ )
    
    #define PLL1_DIV1		0x17	//USB 24 MHZ
    #define PLL1_DIV2		0x1
    #define PLL1_DIV3		0x1	// POST DIV 594/2  -> MJCP/HDVICP
    #define PLL1_DIV4		0x3	// POST DIV 594/4  -> EDMA/EDMA CFG
    #define PLL1_DIV5		0x3	// POST DIV 540/4 -> VPSS
    #define PLL1_DIV6		0x15	// 27Mhz POST DIV 594/22  -> VENC	
    #define PLL1_DIV7		0x0	// POST DIV 597 -> DDR
    #define PLL1_DIV8		0x03	// POST DIV 594/4 -> 90 MMC0/SD0
    #define PLL1_DIV9		0x1	// POST DIV 594/2 -> CLKOUT
    
    #define PLL2_MUL		0x100  
    #define PLL2_PREDIV		0x18
    #define PLL2_POSTDIV	0x0 		//PLL2 Output (0x100 * 2 * 27 / (0x18 + 1) = 552 MHZ
    
    #define PLL2_DIV1		0x18	// 552.96/0x19  MHZ USB
    #define PLL2_DIV2		0x0 	// 552.96/1 = 552.96 Mhz -> ARM 
    #define PLL2_DIV3		0x1	// 552.96/2 = 276.48 mhz 2 * ddr
    #define PLL2_DIV4		0x8 	// POST DIV 552.96/9 =  -> VOICE
    #define PLL2_DIV5		0x0 	// POST DIV 552.96/1 = 552.96 ->VIDEO HD
    
    #define PERIPHERAL_CLK_CTRL_VAL	0x0BFF077C
    
    #define DDR_FREQ		 277
    
    #elif defined(ARM216_DDR173_OSC19P2)
    
    #define PLL1_MUL		0x2d 
    #define PLL1_PREDIV		0x3
    #define PLL1_POSTDIV		0x0 	//PLL1 output ( 0x2d * 2 * 19.2 /4  = 432  MHZ )
    
    #define PLL1_DIV1		0x11	// USB ~24 MHZ
    #define PLL1_DIV2		0x1	
    #define PLL1_DIV3		0x1	// POST DIV  432/2  -> MJCP/HDVICP
    #define PLL1_DIV4		0x3	// POST DIV  432/4  -> EDMA/EDMA CFG
    #define PLL1_DIV5		0x3	// POST DIV  432/4  -> VPSS
    #define PLL1_DIV6		0x0f	// POST DIV    432/16  -> VENC	
    #define PLL1_DIV7		0x0	// POST DIV  432 -> DDR
    #define PLL1_DIV8		0x04	// POST DIV  432/5 -> 86 MMC0/SD0
    #define PLL1_DIV9		0x1	// POST DIV  432/2 -> CLKOUT
    
    #define PLL2_MUL		0xE0
    #define PLL2_PREDIV		0x18
    #define PLL2_POSTDIV		0x0	//PLL2 Output (0xE0 * 2 * 19.2 / (0x18+ 1) = 344.064MHZ
    
    
    #define PLL2_DIV1		0xd     // POST DIV 344/15=24 Mhz  ->USB PHY
    #define PLL2_DIV2		0x0 	// 344/1 =344 Mhz -> DDR 
    #define PLL2_DIV3		0x1	// POST DIV 344/2 Mhz  -> DDRx2
    #define PLL2_DIV4		0x6 	// POST DIV 344/7 -> VOICE
    #define PLL2_DIV5		0x0 	// POST DIV 344/1 ->VIDEO HD
    
    #define PERIPHERAL_CLK_CTRL_VAL	0x0BFF05FC
    
    #define DDR_FREQ		 173
    
    #elif defined(ARM216_DDR173_OSC24)
    
    #define PLL1_MUL		0x73 	// VCO will 2M/N+1 = 345 Mhz
    #define PLL1_PREDIV		0xf
    #define PLL1_POSTDIV		0x0  
    
    #define PLL1_DIV1		0xD	// USB ~24 MHZ
    #define PLL1_DIV2		0x1
    #define PLL1_DIV3		0x1	// POST DIV 345/2  -> 172.5Mhz  MJCP/HDVICP
    #define PLL1_DIV4		0x3	// POST DIV 345/4  -> 86.25Mhz EDMA/EDMA CFG
    #define PLL1_DIV5		0x1	// POST DIV 345/2 -> 172.5 MHZ VPSS
    #define PLL1_DIV6		0x0C	// POST DIV 345/13  -> 26.53 MHZ VENC	
    #define PLL1_DIV7		0x0	// POST DIV 345 -> DDR
    #define PLL1_DIV8		0x3	// POST DIV 345/4 = 86.25 MHZ-> MMC0/SD0
    #define PLL1_DIV9		0x1	// POST DIV 345/2 = 172.5 MHZ-> CLKOUT
    
    #define PLL2_MUL		0x12
    #define PLL2_PREDIV		0x1
    #define PLL2_POSTDIV		0x0 	//PLL2 Output (0x12 * 2 * 27 / (0x1 + 1) = 432 MHZ
    
    
    #define PLL2_DIV1		0x11	// POST DIV 432/18=24 Mhz  ->USB PHY
    #define PLL2_DIV2		0x1  	// 432/2 =216 Mhz -> ARM 
    #define PLL2_DIV3		0x1	// POST DIV 432/2=216 Mhz  -> DDRx2
    #define PLL2_DIV4		0x14	// POST DIV 432/21 = 20.57-> VOICE
    #define PLL2_DIV5		0x0f 	// POST DIV 432/16 = 74.25 ->VIDEO HD
    
    #define PERIPHERAL_CLK_CTRL_VAL	0x243F04FC
    
    #define DDR_FREQ		 173
    
    #elif defined(ARM432_DDR340_OSC24)
    
    #define PLL1_MUL		0x55 
    #define PLL1_PREDIV		0x5
    #define PLL1_POSTDIV		0x0 	// PVCO will 24*2M/N+1 = 680 Mhz
    
    #define PLL1_DIV1		0x1B	// POST DIV 680/28=24.3 Mhz->USB PHY 
    #define PLL1_DIV2		0x1	// POST DIV 680/2=340Mhz->ARM926/ARM968
    #define PLL1_DIV3		0x1	// POST DIV 680/2 = 340Mhz  -> MJCP/HDVICP
    #define PLL1_DIV4		0x3	// POST DIV 680/4 = 170Mhz  -> EDMA/Peripheral CFG0 (1/2 Kaleido clock)
    #define PLL1_DIV5		0x1	// POST DIV 680/2 = 340Mhz -> VPSS (max 270)
    #define PLL1_DIV6		0x8	// POST DIV 680/9 = 75.6Mhz -> VENC	
    #define PLL1_DIV7		0x0	// POST DIV 680/1 = 680Mhz -> DDRx2
    #define PLL1_DIV8		0x6 	// POST DIV 680/7=  97 Mhz-> MMC0/SD0
    #define PLL1_DIV9		0x1B	// POST DIV 680/28 = 24.3Mhz-> CLKOUT 
    
    #define PLL2_MUL		0x9
    #define PLL2_PREDIV		0x0
    #define PLL2_POSTDIV	0x0 		// PLL2 Output (0x9 * 2 * 27 / (0x1 + 1) = 432MHZ
    
    #define PLL2_DIV1		0x11	// POST DIV 432/18=24 Mhz  ->USB PHY
    #define PLL2_DIV2		0x0 	// POST DIV 432/1=432 Mhz  -> ARM926/HDVICP 
    #define PLL2_DIV3		0x1	// POST DIV 432/2=216 Mhz  -> DDRx2
    #define PLL2_DIV4		0x14	// POST DIV 432/21= 20.5714 Mhz->VOICE
    #define PLL2_DIV5		0x0f 	// POST DIV 432/16=27 Mhz  -> VENC
    
    #define PERIPHERAL_CLK_CTRL_VAL	0x243F04FC
    
    #define DDR_FREQ		 340
    
    #else  //Arm 297 DDR 243 MHZ 
    
    #define PLL1_MUL		0x51
    #define PLL1_PREDIV		0x7
    #define PLL1_POSTDIV	0x0 		//PVCO will 24*2M/N+1 = 486 Mhz
    
    #define PLL1_DIV1		0x13	//POST DIV 486/20=24.3 Mhz->USB PHY 
    #define PLL1_DIV2		0x1	//POST DIV 486/2=243Mhz->ARM926/ARM968
    #define PLL1_DIV3		0x1	// POST DIV 486/2 = 243 Mhz  -> MJCP/HDVICP
    #define PLL1_DIV4		0x3	// POST DIV 486/4 = 121.5 Mhz  -> EDMA/Peripheral CFG0 (1/2 Kaleido clock)
    #define PLL1_DIV5		0x1	// POST DIV 486/2 = 243Mhz -> VPSS (max 270)
    #define PLL1_DIV6		0x11	// POST DIV 486/18 = 27 Mhz -> VENC	
    #define PLL1_DIV7		0x0	// POST DIV 486/1 = 486Mhz -> DDRx2
    #define PLL1_DIV8		0x4	// POST DIV 486/5 = 97.25Mhz-> MMC0/SD0
    #define PLL1_DIV9		0x1	// POST DIV 486/2 = 24.3Mhz-> CLKOUT 
    
    
    #define PLL2_MUL		0x63
    #define PLL2_PREDIV		0x7
    #define PLL2_POSTDIV	0x0 		//PLL2 Output (0x63 * 2 * 24 / (0x7 + 1) = 594MHZ
    
    #define PLL2_DIV1		0x18	// 594/25 23.6 MHZ USB
    #define PLL2_DIV2		0x1  	// 594/2 =297 Mhz -> ARM 
    #define PLL2_DIV3		0X1		// 297 MHZ 2 * ddr
    #define PLL2_DIV4		0x1c 	// POST DIV 594/29 = 20.48 -> VOICE
    #define PLL2_DIV5		0x07 	// POST DIV 594/8 = 74.25 ->VIDEO HD
    
    #define PERIPHERAL_CLK_CTRL_VAL	0x243F04FC
    
    #define DDR_FREQ		 243
    
    #endif
    
    
    
    /************************************************************
    * Global Function Definitions                               *
    ************************************************************/
    
    
    /*
     DDR uses PLL1 Sysclk 7
     Arm uses PLL2 Sysclk 2 
    
     DDR & ARM Source can be selected by configuring Peripheral ctl reg
     PERI_CLKCTL 0x48 System module Rrg 0x01c40000
     */
    
    
    
    Uint32 DEVICE_init()
    {
      Uint32 status = E_PASS;
     
       // Mask all interrupts
      AINTC->INTCTL = 0x4;
      AINTC->EABASE = 0x0;
      AINTC->EINT0  = 0x0;
      AINTC->EINT1  = 0x0;		
       
      // Clear all interrupts
      AINTC->FIQ0 = 0xFFFFFFFF;
      AINTC->FIQ1 = 0xFFFFFFFF;
      AINTC->IRQ0 = 0xFFFFFFFF;
      AINTC->IRQ1 = 0xFFFFFFFF;
    
      POR_RESET();
      WDT_RESET();
    
    #ifndef SKIP_LOW_LEVEL_INIT
    
       // System PSC setup - enable all
      DEVICE_PSCInit();
      
      DEVICE_pinmuxControl(0,0xFFFFFFFF,0x00FD0000);  // All Video Inputs
      DEVICE_pinmuxControl(1,0xFFFFFFFF,0x00145555);  // All Video Outputs
      DEVICE_pinmuxControl(2,0xFFFFFFFF,0x000000DA);  // EMIFA
      DEVICE_pinmuxControl(3,0xFFFFFFFF,0x00180000);  // SPI0, SPI1, UART1, I2C, SD0, SD1, McBSP0, CLKOUTs
      DEVICE_pinmuxControl(4,0xFFFFFFFF,0x55555555);  // MMC/SD0 instead of MS, SPI0
    
    	GPIO->DIR02 &= 0xfeffffff;
    	GPIO->CLRDATA02 = 0x01000000;
    
     
      if (status == E_PASS) status |= DEVICE_PLL1Init();
    
      if (status == E_PASS) status |= DEVICE_PLL2Init();
    
    	if (status == E_PASS) 
    		status |= DEVICE_DDR2Init();
    
    #endif
      // AEMIF Setup
      if (status == E_PASS) status |= DEVICE_EMIFInit();
    
      // UART0 Setup
      if (status == E_PASS) status |= DEVICE_UART0Init();
    
      // TIMER0 Setup
      if (status == E_PASS) status |= DEVICE_TIMER0Init();
    	
      // I2C0 Setup
      if (status == E_PASS) status |= DEVICE_I2C0Init();
    
      WDT_FLAG_ON();
    
      return status;
    }
    
    void POR_RESET()
    {
    
    	if ((PLL1->RSTYPE)&3) {
        
        	VPSS_SYNC_RESET();  // VPSS sync reset
        
    	*TMPBUF = 0;
    	*TMPSTATUS |= FLAG_PORRST;
        
        	*GPINT_GPEN = 0x00020000;
        
        	*GPTDAT_GPDIR = 0x00020002;
        
        	while(1);
      	}
    
    }
    
    void WDT_RESET()
    {
        volatile unsigned int s;
    
         if((*TMPBUF == 0x591b3ed7)){
            *TMPBUF = 0;
    		*TMPSTATUS |= FLAG_PORRST;
     		*TMPSTATUS |= FLAG_FLGOFF;  
            
            for (s=0;s<0x100;s++) {}
    
            VPSS_SYNC_RESET();
    
            *GPINT_GPEN = 0x00020000;                                   // WDT
    
            *GPTDAT_GPDIR = 0x00020002;                                 // execute >
      	     while(1);
        }
    }
    
    void WDT_FLAG_ON()
    {
    
    	SYSTEM->VPSS_CLKCTL &= 0xffffff7f;      // VPSS_CLKMD 1:2
    	*TMPBUF = 0x591b3ed7; 
    	*TMPSTATUS |= FLAG_FLGON;  
    }
    
    void VPSS_SYNC_RESET()
    {
    	unsigned int PdNum = 0;
    
    	SYSTEM->VPSS_CLKCTL |= 0x00000080;						// VPSS_CLKMD 1:1
    
    	//LPSC SyncReset DDR Clock Enable
    	PSC->MDCTL[47] = ((PSC->MDCTL[47] & 0xffffffe0) | 0x00000001);        
                
    	PSC->PTCMD = (1<<PdNum);
    
    	while(! (((PSC->PTSTAT >> PdNum) & 0x00000001) == 0));      
    
    	while(!((PSC->MDSTAT[47] &  0x0000001F) == 0x1));           
    }
    
    void DEVICE_LPSCTransition(Uint8 module, Uint8 domain, Uint8 state)
    {
      // Wait for any outstanding transition to complete
      while ( (PSC->PTSTAT) & (0x00000001 << domain) );
      
      // If we are already in that state, just return
      if (((PSC->MDSTAT[module]) & 0x1F) == state) return;
        
      // Perform transition
      PSC->MDCTL[module] = ((PSC->MDCTL[module]) & (0xFFFFFFE0)) | (state);
      PSC->PTCMD |= (0x00000001 << domain);
    
      // Wait for transition to complete
      while ( (PSC->PTSTAT) & (0x00000001 << domain) );
      
      // Wait and verify the state
      while (((PSC->MDSTAT[module]) & 0x1F) != state);	
    }
    
    void DEVICE_pinmuxControl(Uint32 regOffset, Uint32 mask, Uint32 value)
    {
      SYSTEM->PINMUX[regOffset] &= ~mask;
      SYSTEM->PINMUX[regOffset] |= (mask & value);
    }
    
    DEVICE_BootMode DEVICE_bootMode( void )
    {
      return (DEVICE_BootMode) ((SYSTEM->BOOTCFG & DEVICE_BOOTCFG_BOOTMODE_MASK) >> DEVICE_BOOTCFG_BOOTMODE_SHIFT);
    }
    
    DEVICE_BusWidth DEVICE_emifBusWidth( void )
    {
      if ( ( (SYSTEM->BOOTCFG & DEVICE_BOOTCFG_EMIFWIDTH_MASK) >> DEVICE_BOOTCFG_EMIFWIDTH_SHIFT) & 0x1 )
      {
        return DEVICE_BUSWIDTH_16BIT;
      }
      else
      {
        return DEVICE_BUSWIDTH_8BIT;
      }
    }
    
    void DEVICE_PSCInit()
    {
      
      unsigned char i=0;
      unsigned char lpsc_start;
      unsigned char lpsc_end,lpscgroup,lpscmin,lpscmax;
      unsigned int  PdNum = 0; 
     
      lpscmin  =0;
      lpscmax  =2;
      
      for(lpscgroup=lpscmin ; lpscgroup <=lpscmax; lpscgroup++) {
      if(lpscgroup==0)
      {
        lpsc_start = 0; // Enabling LPSC 3 to 28 SCR first
        lpsc_end   = 28;
      }
      else if (lpscgroup == 1) { /* Skip locked LPSCs [29-37] */
        lpsc_start = 38;
        lpsc_end   = 47;
       } else {
        lpsc_start = 50;
        lpsc_end   = 51;
       }
    
     	//NEXT=0x3, Enable LPSC's
     	for(i=lpsc_start; i<=lpsc_end; i++) {
       	     // CSL_FINS(CSL_PSC_0_REGS->MDCTL[i], PSC_MDCTL_NEXT, 0x3);	  
       	     PSC->MDCTL[i] |= 0x3; 
        }
    
     	//Program goctl to start transition sequence for LPSCs
     	//CSL_PSC_0_REGS->PTCMD = (1<<PdNum); /*Kick off Power Domain 0 Modules*/
           PSC->PTCMD = (1<<PdNum); 
           
     	//Wait for GOSTAT = NO TRANSITION from PSC for Powerdomain 0
     	//while(! (((CSL_PSC_0_REGS->PTSTAT >> PdNum) & 0x00000001) == 0));
     	 while(! (((PSC->PTSTAT >> PdNum) & 0x00000001) == 0)); 
    
     	//Wait for MODSTAT = ENABLE from LPSC's
     	for(i=lpsc_start; i<=lpsc_end; i++) {
       	     // while(!((CSL_PSC_0_REGS->MDSTAT[i] &  0x0000001F) == 0x3));   
       	     while(!((PSC->MDSTAT[i] &  0x0000001F) == 0x3));   
       	       	    		
        }	
      }	  
    
    }
    
    
    Uint32 DEVICE_PLL1Init()
    {
    	unsigned int CLKSRC=0x0;    			  
    		
    
    		/*Power up the PLL*/
    	PLL1->PLLCTL &= 0xFFFFFFFD;		
    
    	PLL1->PLLCTL &= 0xFFFFFEFF;  			
    	PLL1->PLLCTL |= CLKSRC<<8;
    	
    	/*Set PLLENSRC '0', PLL Enable(PLLEN) selection is controlled through MMR*/
    	PLL1->PLLCTL &= 0xFFFFFFDF;	
    	
    	/*Set PLLEN=0 => PLL BYPASS MODE*/
    	PLL1->PLLCTL &= 0xFFFFFFFE;
    	
    	UTIL_waitLoop(150); 				
    	
    	 // PLLRST=1(reset assert)
    	PLL1->PLLCTL |= 0x00000008; 
    	
        UTIL_waitLoop(300); 
    	
    	/*Bring PLL out of Reset*/ 
     	PLL1->PLLCTL &= 0xFFFFFFF7;
       
    	//Program the Multiper and Pre-Divider for PLL1
    	 PLL1->PLLM   =   PLL1_MUL;   // VCO will 24*2M/N+1 = 486Mhz
    	 PLL1->PREDIV =   0x8000 | PLL1_PREDIV; 
    	 
    		 
    	PLL1->SECCTL = 0x00470000;   // Assert TENABLE = 1, TENABLEDIV = 1, TINITZ = 1 
        //	for(j=0; j<0x100; j++) {} 
        PLL1->SECCTL = 0x00460000;   // Assert TENABLE = 1, TENABLEDIV = 1, TINITZ = 0 
    	//	for(j=0; j<0x100; j++) {}
        PLL1->SECCTL = 0x00400000;   // Assert TENABLE = 0, TENABLEDIV = 0, TINITZ = 0 
    	//	for(j=0; j<0x100; j++) {}
        PLL1->SECCTL = 0x00410000;   // Assert TENABLE = 0, TENABLEDIV = 0, TINITZ = 1
    
    
    
         //Program the PostDiv for PLL1
         PLL1->POSTDIV = 0x8000 | PLL1_POSTDIV;
        
         // Post divider setting for PLL1 
    
    		PLL1->PLLDIV1 = 0x8000 | PLL1_DIV1;
    	    PLL1->PLLDIV2 = 0x8000 | PLL1_DIV2;   
    	    PLL1->PLLDIV3 = 0x8000 | PLL1_DIV3;   // POST DIV 486/2  -> MJCP/HDVICP
    	    PLL1->PLLDIV4 = 0x8000 | PLL1_DIV4;   // POST DIV 486/4  -> EDMA/EDMA CFG
    	    PLL1->PLLDIV5 = 0x8000 | PLL1_DIV5;   // POST DIV 486/2 -> VPSS
    	    PLL1->PLLDIV6 = 0x8000 | PLL1_DIV6;   // 27Mhz POST DIV 486/18  -> VENC
            PLL1->PLLDIV7 = 0x8000 | PLL1_DIV7;   // POST DIV 486/2 -> DDR
    	    PLL1->PLLDIV8 = 0x8000 | PLL1_DIV8;   // POST DIV 486/4 -> MMC0/SD0
    	    PLL1->PLLDIV9 = 0x8000 | PLL1_DIV9;   // POST DIV 486/2 -> CLKOUT
    	    
    	 	UTIL_waitLoop(300);
    	    
    	    /*Set the GOSET bit */   
    		 PLL1->PLLCMD = 0x00000001;  // Go
    		 
    		 UTIL_waitLoop(300);
    		 
    		 
    		/*Wait for PLL to LOCK */
          
              while(! (((SYSTEM->PLL0_CONFIG) & 0x07000000) == 0x07000000));
            
         
            /*Enable the PLL Bit of PLLCTL*/
             PLL1->PLLCTL |= 0x00000001;   // PLLEN=0
    
      return E_PASS;
    }
    
    
    Uint32 DEVICE_PLL2Init()
    {
    	unsigned int CLKSRC=0x0;
     	/*Power up the PLL*/
    	PLL2->PLLCTL &= 0xFFFFFFFD;	
    			     	
    	/*Select the Clock Mode as Onchip Oscilator or External Clock on MXI pin*/
    	/*VDB has input on MXI pin */
    	
    	PLL2->PLLCTL &= 0xFFFFFEFF;  			
    	PLL2->PLLCTL |= CLKSRC<<8;
    	
    	/*Set PLLENSRC '0', PLL Enable(PLLEN) selection is controlled through MMR*/
    	PLL2->PLLCTL &= 0xFFFFFFDF;	
    	
    	/*Set PLLEN=0 => PLL BYPASS MODE*/
    	PLL2->PLLCTL &= 0xFFFFFFFE;
    	
    	UTIL_waitLoop(50); 				
    	
    	 // PLLRST=1(reset assert)
    	PLL2->PLLCTL |= 0x00000008;  
    
    
    	UTIL_waitLoop(300); 
    
    	  /*Bring PLL out of Reset*/
         PLL2->PLLCTL &= 0xFFFFFFF7;		
    			 
         //Program the Multiper and Pre-Divider for PLL2
    	 PLL2->PLLM   = PLL2_MUL;  // VCO will 24*2M/N+1 = 594Mhz
    	 PLL2->PREDIV = 0x8000 | PLL2_PREDIV; 
    	 
    	 PLL2->POSTDIV = 0x8000 | PLL2_POSTDIV;
        
    	 PLL2->SECCTL = 0x00470000;   // Assert TENABLE = 1, TENABLEDIV = 1, TINITZ = 1 
         PLL2->SECCTL = 0x00460000;   // Assert TENABLE = 1, TENABLEDIV = 1, TINITZ = 0 
         PLL2->SECCTL = 0x00400000;   // Assert TENABLE = 0, TENABLEDIV = 0, TINITZ = 0 
         PLL2->SECCTL = 0x00410000;   // Assert TENABLE = 0, TENABLEDIV = 0, TINITZ = 1
    			     
    	  // Post divider setting for PLL2 
    
    	 PLL2->PLLDIV1 = 0x8000 | PLL2_DIV1;
         PLL2->PLLDIV2 = 0x8000 | PLL2_DIV2;   // 594/2 =297 Mhz -> ARM 
    	 PLL2->PLLDIV3 = 0x8000 | PLL2_DIV3;   // POST DIV 594/29 = 20.48 -> VOICE
    	 PLL2->PLLDIV4 = 0x8000 | PLL2_DIV4;   // POST DIV 594/8 = 74.25 ->VIDEO HD
    	 PLL2->PLLDIV5 = 0x8000 | PLL2_DIV5;
    		     
    	  //GoCmd for PostDivider to take effect
                
         PLL2->PLLCMD = 0x00000001;  
         
         UTIL_waitLoop(150);
                  
          /*Wait for PLL to LOCK */
          while(! (((SYSTEM->PLL1_CONFIG) & 0x07000000) == 0x07000000)); 
         
         UTIL_waitLoop(4100);
                 
          //Enable the PLL2
    	    
    	  PLL2->PLLCTL |= 0x00000001;   // PLLEN=0
    
    	//do this after PLL's have been set up
    	SYSTEM->PERI_CLKCTRL = PERIPHERAL_CLK_CTRL_VAL;
    
      
      return E_PASS;
     
    }
    
    Uint32 DDR_Get_Val(Uint32 parm, Uint32 freq)
    {
    	Uint32 result;
    
    	
    	result = ((parm * freq) / 10000) - 1;
    
        /* Check if value calculated from formula results in decimal. 
        * If yes round off to next decimal, as the value to be
         * written to register should be >= calculated value.
         */
       if((parm * freq) % 10000)
               result++;
    
    	return result;
    }
    
    Uint32 DEVICE_DDR2Init()
    {
    
     Uint32 tRFC, tRP, tRCD, tWR, tRAS, tRC, tRRD, tWTR;
    
     DEVICE_LPSCTransition(LPSC_DDR2,0,PSC_ENABLE);
      
      SYSTEM->VTPIOCR = (SYSTEM->VTPIOCR) & 0xFFFF9F3F;
      
       // Set bit CLRZ (bit 13)
       SYSTEM->VTPIOCR = (SYSTEM->VTPIOCR) | 0x00002000;
      
       // Check VTP READY Status
       while( !(SYSTEM->VTPIOCR & 0x8000));     
      
       // Set bit VTP_IOPWRDWN bit 14 for DDR input buffers)
       //SYSTEM->VTPIOCR = SYSTEM->VTPIOCR | 0x00004000;         
      
       // Set bit LOCK(bit7) and PWRSAVE (bit8)
       SYSTEM->VTPIOCR = SYSTEM->VTPIOCR | 0x00000080;     
        
       // Powerdown VTP as it is locked (bit 6)
       // Set bit VTP_IOPWRDWN bit 14 for DDR input buffers)
       SYSTEM->VTPIOCR = SYSTEM->VTPIOCR | 0x00004040;
      
      // Wait for calibration to complete 
      UTIL_waitLoop( 150 );
      
      // Set the DDR2 to synreset, then enable it again
      DEVICE_LPSCTransition(LPSC_DDR2,0,PSC_SYNCRESET);
      DEVICE_LPSCTransition(LPSC_DDR2,0,PSC_ENABLE);
        
     	DDR->DDRPHYCR = 0x000000C5; 
    
    	DDR->SDBCR = 0x534832;
    	DDR->SDBCR = 0x53C832; // 0x53C832; Set the TIMUNLOCK to write into the TMR reg  
    
    
    	tRFC = DDR_Get_Val(DDR_T_RFC, DDR_FREQ);
        tRP  = DDR_Get_Val(DDR_T_RP, DDR_FREQ);
        tRCD = DDR_Get_Val(DDR_T_RCD, DDR_FREQ);
        tWR  = DDR_Get_Val(DDR_T_WR, DDR_FREQ);
        tRAS = DDR_Get_Val(DDR_T_RAS, DDR_FREQ);
        tRC  = DDR_Get_Val(DDR_T_RC, DDR_FREQ);
        tRRD = DDR_Get_Val(DDR_T_RRD, DDR_FREQ);
        tWTR = DDR_Get_Val(DDR_T_WTR, DDR_FREQ);
    
       DDR->SDTIMR =    tRFC << 25	|              
                        tRP  << 22	|
                        tRCD << 19	|
                        tWR  << 16	|
                        tRAS << 11	|
                        tRC  << 6	|
                        tRRD << 3	|
                        tWTR << 0;
    
        DDR->SDTIMR2 =  ((DDR_T_RASMAX / (DDR_RR * DDR_FREQ)) << 27) |
                        (DDR_T_XP << 25 )    |
                        (((DDR_T_XSNR * DDR_FREQ) / 10000) << 16)   |
                        (DDR_T_XSRD << 8)    |
                        (((DDR_T_RTP * DDR_FREQ) / 10000) << 5)  |   
                         (DDR_T_CKE << 0);
          
    	DDR->SDBCR = 0x534832; //0x534832; Reset the TIMUNLOCK TMR Write Disable
    
    	DDR->PBBPR = 0x000000FE;
    	
    	DDR->SDBCR = 0xD34A32;	 //Enable DDR2 and DDR and SDram. Write '1' to BOOTUNLOCK
    
    	DDR->SDBCR = 0x534A32;	//Enable DDR2 and DDR and SDram. Write '0' to BOOTUNLOCK
    
    	DDR->SDRCR = (DDR_RR * DDR_FREQ) / 10; //Program SDRAM Refresh Control Registers
    
    
      DEVICE_LPSCTransition(LPSC_DDR2,0,PSC_SYNCRESET);
      DEVICE_LPSCTransition(LPSC_DDR2,0,PSC_ENABLE);
    
    	return E_PASS;
    }
    
    
    Uint32 DEVICE_EMIFInit()
    {
    
      AEMIF->AWCCR = 0xff;
      
      AEMIF->A1CR = 0x40400204;
    
      AEMIF->NANDFCR |= 1;
    
      AEMIF->A2CR = 0x00a00505;
    
      return E_PASS;  
    
    }
     
    Uint32 DEVICE_UART0Init()
    {
      UART0->PWREMU_MGNT = 0;         // Reset UART TX & RX components
    
      UTIL_waitLoop( 100 );
    
      UART0->MDR = 0x0;
      UART0->DLL = 0xd;               // Set baud rate	
      UART0->DLH = 0;
     
    
      UART0->FCR = 0x0007;            // Clear UART TX & RX FIFOs
      UART0->FCR = 0x0000;            // Non-FIFO mode
      UART0->IER = 0x0007;            // Enable interrupts
      
      UART0->LCR = 0x0003;            // 8-bit words,
                                      // 1 STOP bit generated,
                                      // No Parity, No Stick paritiy,
                                      // No Break control
      
      UART0->MCR = 0x0000;            // RTS & CTS disabled,
                                      // Loopback mode disabled,
                                      // Autoflow disabled
    
      UART0->PWREMU_MGNT = 0xE001;    // Enable TX & RX componenets
            
      return E_PASS;
    }
    
    Uint32 DEVICE_I2C0Init()
    {
      I2C0->ICMDR   = 0;                // Reset I2C
      I2C0->ICPSC   = 26;               // Config prescaler for 27MHz
      I2C0->ICCLKL  = 20;               // Config clk LOW for 20kHz
      I2C0->ICCLKH  = 20;               // Config clk HIGH for 20kHz
      I2C0->ICMDR   |= I2C_ICMDR_IRS;   // Release I2C from reset
    
      return E_PASS;
    }
    
    Uint32 DEVICE_I2C0Reset()
    {
      I2C0->ICMDR &= ~I2C_ICMDR_IRS;
      UTIL_waitLoop(200);
    
      // Read and clear interrupt status register
      I2C0->ICSTR |= 0x00007FFF;
    
      // Read ICIVR until clear
      while ((I2C0->ICIVR & 0x7) != 0x0);
                      
      // Take I2C Out of Reset
      I2C0->ICMDR |= I2C_ICMDR_IRS;
      UTIL_waitLoop(200);
      return E_PASS;
    }
    
    Uint32 DEVICE_TIMER0Init()
    {
      // Put timer into reset
      TIMER0->EMUMGT_CLKSPD = 0x00000003;
      TIMER0->TCR           = 0x00000000;
      
      // Enable TINT0, TINT1 interrupt
      TIMER0->INTCTL_STAT   = 0x00000001;
    	
      // // Set to 64-bit GP Timer mode, enable TIMER12 & TIMER34
      TIMER0->TGCR = 0x00000003;
    
      // Reset timers to zero 
      TIMER0->TIM12 = 0x00000000;
      TIMER0->TIM34 = 0x00000000;
      
      // Set timer period (5 second timeout = (24000000 * 5) cycles = 0x07270E00) 
      TIMER0->PRD34 = 0x00000000;
      TIMER0->PRD12 = 0x07270E00;
    
      return E_PASS;
    }
    //interrupt for Timer0 in DM35x and DM36x is the same
    void DEVICE_TIMER0Start(void)
    {
      // Clear interrupt
      AINTC->IRQ1   |=  0x00000001;
    
      // Put timer in reset
      TIMER0->TGCR  =   0x00000000;
    
      // Reset timer count to zero 
      TIMER0->TIM12 =   0x00000000;
    
      // Setup for one-shot mode
      TIMER0->TCR   =   0x00000040;
    
      // Start TIMER12
      TIMER0->TGCR  = 0x00000005;
    }
    
    void DEVICE_TIMER0Stop(void)
    {
      // Clear interrupt
      AINTC->IRQ1   |=  0x00000001;
    
      // Put timer in reset
      TIMER0->TCR   = 0x00000000;
      TIMER0->TGCR  = 0x00000000;
    
      // Reset timer count to zero 
      TIMER0->TIM12 = 0x00000000;
    }
    
    Uint32 DEVICE_TIMER0Status(void)
    {
      return ((AINTC->IRQ1)&0x1);
    }
    
    
    /************************************************************
    * Local Function Definitions                                *
    ************************************************************/
    
    
    /***********************************************************
    * End file                                                 *
    ***********************************************************/
    
    
    
    
    

     
    Why is the DQSn always low at a read access? Is there any mistake in the DEVICE_DDR2Init()?
     
    The customer doubts whether DM365 really supports differential DQS, because Table 13 in the User's Guide (SPRUFI2) indicate only the disabled differential signaling (disabled DQSn).
     
    Please give me an answer as soon as possible. Your prompt reply would be appreciated.
     
    Best regards,
     
    Daisuke