This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

can't get "CC..." in boot

Guru 20755 points

Hello,

I am using DM814X with the following bootmode:

BTMODE[4:0]

1st

2nd

3rd

4th

10010b

NAND

NANDI2C

SPI

UART

I work with custom board, which worked fine till now, in which I use boot from serial and boot from nand. both worked OK.

The last action I did was nand scrub (not the first time which I did this with the custom board).

After this action I don't get "CCC..." in serial. I had similar issue some time ago and whenever I has this issue inserting the jtag cable, and resetting solved this issue. Now even this does not function.

Does anyone knows why I don't get "CC..." when there is nothing in nand (and other interfaces) ?

Thank you,

Ran