I'm using ti-sdk-am335x-evm-07.00.00.00 and the associated Graphics_SDK_5_01_01_01 to do my work. The steps are to build the TI SDK 07 first, then extract, setup, and build the Graphics SDK. I'm assuming it was done this way to save time/space for those not interested in the Graphical content in their builds... however, I'd really like to just do a single build and be done with all the content.
Are there any difficulties or issues I'll run into if I go to combine the two builds? Has anyone done this before? Any advice for me?