Other Parts Discussed in Thread: DP83630
I am using a Sitara (AM335x) processor which is connected to DP83630 PHY. And I am planning on connecting the PHY to SFP's. For example a SIGNAMAX 065-73TXMG SFP.
But it requires the DP83630 to be configured for100BaseFX.
We are currently doing this via a hardware strap on the DP83630 and our SFP venders are indicating that the hardware is setup correctly between the PHY and the SFP.
Unfortunately, this is not yet working.
So, a couple of firmware related questions:
1) Using ethtool, the status is indicating that the PHY is set to 10BaseT. So, is it possible that the firmware is overriding the hardware strap setting? I am using the 7.0 SDK with a DTS nearly identical to the am335x.
2) How does one force the DP83630 into 100BaseFX. The ethtool doesn't seem to have the capability.