This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 capture from vip0 with FPGA

Hi all

I want to capture 1600*3600 resolution image on VIP0 port of DM8168 with DVR-RDK without any external video decoder chip. This image will be provided through FPGA to VIP0 port of DM8168.  As capture driver supports standard video resolution only, so it would not be possible by DVR-RDK's present demos. 

I am using DVR-RDK04.00.01, My path would be something like, 1600*3000 RGB data from FPGA -> VIP ->  menory->sata  stream. 

1.Is this use case feasible ?

2.if yes then where and what changes i need to make to get work done ?

3.sometime there is no picture, FPGA stop put image to VIP0,when there is image,FPGA  put the image to VIP0. can DM8168 work like that?