When i try to resume the kernel, the problem as follows:
Texas Instruments X-Loader 1.41
Starting OS Bootloader...
U-Boot 1.1.4 (May 2 2008 - 18:40:55)
OMAP3-GP rev 2, CPU-OPP2 L3-165MHz
OMAP3EVM 1.0 Version + mPOP (Boot NAND)
DRAM: 128 MB
NAND:256 MiB
In: serial
Out: serial
Err: serial
Reseting CHIP... Done
LAN9x18 (0x01150002) detected.
Setting mac address: 00:50:c2:7e:8b:38
start Auto negotiation... (take ~2sec)
Auto negotiation complete, 100BaseTX, full duplex
Hit any key to stop autoboot: 0
NAND read: device 0 offset 2621440, size 2097152 ... 2097152 bytes read: OK
NAND read: device 0 offset 7864320, size 16777216 ... 16777216 bytes read: OK
## Booting image at 80000000 ...
Image Name: Linux-2.6.22.18-omap3
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1890548 Bytes = 1.8 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
OK
Starting kernel ...
Uncompressing Linux.............................................................
................................................................ done, booting t
he kernel.
When run to this, it stop,how can i do it ?