This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 reboot hangs.

Hi,

The reboot command from Linux  causes the hang with following log, (although this is not frequent but it hangs randomly)

The system is going down for reboot NOW!
         Starting /dev/initctl Compatibility Daemon...
[  OK  ] Started /dev/initctl Compatibility Daemon.
[  OK  ] Stopped Update UTMP about System Runlevel Changes.
[  OK  ] Stopped target Multi-User System.
         Stopping My script...
[  OK  ] Stopped target Login Prompts.
         Stopping Serial Getty on ttyO0...
         Stopping Getty on tty1...
         Stopping Wi-Fi Security Service...
         Stopping D-Bus System Message Bus...
         Stopping Login Service...
[  OK  ] Stopped Getty on tty1.
[  OK  ] Stopped Login Service.
[[  OK  ] Stopped D-Bus System Message Bus.
[  OK  ] Stopped Serial Getty on ttyO0.
[  OK  ] Stopped My script.
         Stopping Permit User Sessions...
[  OK  ] Stopped Permit User Sessions.
[  OK  ] Stopped target Remote File Systems.
         Stopping Connection service...

Thanks & Regards

Mike

  • Hello,

    Are you mean when you are trying to reboot the board from the console?

    What the is software release that you are using?

    Provide more details. 

    Best Regards,

    Margarita

  • Hi,

    Yes via 'reboot' command from Linux. I am using the  ti81xx-master branch from arago.

    Thanks & Regards,

    Mike

  • Mike,

    I suspect this might be HW related issue, as the 'reboot' command is working fine on the DM814x EVM:

    dm814x-evm login: root
    root@dm814x-evm:~# reboot

    Broadcast message from root (ttyO0) (Mon Dec 31 10:37:10 2012):

    The system is going down for reboot NOW!
    INIT: SendiStopping telnet daemon.
    Stopping system message bus: stopped process in pidfile '/var/run/dbus/pid' (pid 1245)
    dbus.
    Error opening /dev/fb0: No such file or directory
    Stopping thttpd.
    ALSA: Storing mixer settings...
    Deconfiguring network interfaces... done.
    Stopping syslogd/klogd: stopped syslogd (pid 1257)
    stopped klogd (pid 1259)
    done
    Sending all processes the TERM signal...
    Sending all processes the KILL signal...
    Unmounting remote filesystems...
    Deactivating swap...
    Unmounting local filesystems...
    Rebooting... musb-hdrc musb-hdrc.1: remove, state 1
    usb usb2: USB disconnect, address 1
    musb-hdrc musb-hdrc.1: USB bus 2 deregistered
    musb-hdrc musb-hdrc.0: remove, state 1
    usb usb1: USB disconnect, address 1
    musb-hdrc musb-hdrc.0: USB bus 1 deregistered
    Restarting system.


    U-Boot 2010.06 (Oct 17 2014 - 16:33:14)

    TI8148-GP rev 2.1

    ARM clk: 600MHz
    DDR clk: 400MHz

    DRAM:  1 GiB
    DCACHE:  Off
    NAND:  HW ECC BCH8 Selected
    256 MiB
    Using default environment

    The 2nd stage U-Boot will now be auto-loaded
    Please do not interrupt the countdown till TI8148_EVM prompt if 2nd stage is already flashed
    Hit any key to stop autoboot:  0

    NAND read: device 0 offset 0x20000, size 0x40000
     262144 bytes read: OK
    ## Starting application at 0x81000000 ...


    U-Boot 2010.06 (Oct 17 2014 - 16:34:42)

    TI8148-GP rev 2.1

    ARM clk: 600MHz
    DDR clk: 400MHz

    I2C:   ready
    DRAM:  1 GiB
    DCACHE:  On
    NAND:  HW ECC BCH8 Selected
    256 MiB
    MMC:   OMAP SD/MMC: 0
    *** Warning - bad CRC or NAND, using default environment

                              .:;rrr;;.                   
                        ,5#@@@@#####@@@@@@#2,             
                     ,A@@@hi;;;r5;;;;r;rrSG@@@A,          
                   r@@#i;:;s222hG;rrsrrrrrr;ri#@@r        
                 :@@hr:r;SG3ssrr2r;rrsrsrsrsrr;rh@@:      
                B@H;;rr;3Hs;rrr;sr;;rrsrsrsrsrsr;;H@B     
               @@s:rrs;5#;;rrrr;r#@H:;;rrsrsrsrsrr:s@@    
              @@;;srs&X#9;r;r;;,2@@@rrr:;;rrsrsrsrr;;@@   
             @@;;rrsrrs@MB#@@@@@###@@@@@@#rsrsrsrsrr;;@@  
            G@r;rrsrsr;#X;SX25Ss#@@#M@#9H9rrsrsrsrsrs;r@G
            @9:srsrsrs;2@;:;;:.X@@@@@H::;rrsrsrsrsrsrr:3@
           X@;rrsrsrsrr;XAi;;:&@@#@Bs:rrsrsrsrsrsrsrsrr;@X
           @#;rsrsrsrsrr;r2ir@@@###::rrsrsrsrsrsrsrsrsr:@@
           @A:rrsrsrsrr;:2@29@@M@@@;:;rrrrsrsrsrsrsrsrs;H@
           @&;rsrsrsrr;A@@@@@@###@@@s::;:;;rrsrsrsrsrsr;G@
           @#:rrsrsrsr;G@5Hr25@@@#@@@#9XG9s:rrrrsrsrsrs:#@
           M@;rsrsrsrs;r@&#;::S@@@@@@@M@@@@Grr:;rsrsrsr;@#
           :@s;rsrsrsrr:M#Msrr;;&#@@@@@@@@@@H@@5;rsrsr;s@,
            @@:rrsrsrsr;S@rrrsr;:;r3MH@@#@M5,S@@irrsrr:@@
             @A:rrsrsrsrrrrrsrsrrr;::;@##@r:;rH@h;srr:H@  
             ;@9:rrsrsrsrrrsrsrsrsr;,S@Hi@i:;s;MX;rr:h@;  
              r@B:rrrrsrsrsrsrsrr;;sA@#i,i@h;r;S5;r:H@r   
               ,@@r;rrrsrsrsrsrr;2BM3r:;r:G@:rrr;;r@@,    
                 B@Mr;rrrrsrsrsr@@S;;;rrr:5M;rr;rM@H      
                  .@@@i;;rrrrsrs2i;rrrrr;r@M:;i@@@.       
                    .A@@#5r;;;r;;;rrr;r:r#AsM@@H.         
                       ;&@@@@MhXS5i5SX9B@@@@G;            
                           :ihM#@@@@@##hs,                

    Net:   <ethaddr> not set. Reading from E-fuse
    Detected MACID:90:d7:eb:d5:13:96
    cpsw
    Hit any key to stop autoboot:  0
    TI8148_EVM#


    One question, which file system you are using for rootfs? I am using the arago fs (ti-ezsdk_dm814x-evm_5_05_02_00/filesystem/arago-base-tisdk-image-dm814x-evm.tar.gz)

    Regards,
    Pavel