Hi,
I have a custom made DSP Board.
C6713 is connected to FPGA through EMIF in CE3 space. The FPGA is connected to LCD.
C6713 --> FPGA --> LCD
I have a situation where the LCD has to be controlled by C6713 and not by FPGA.
I want to control the LCD through C6713 , the FPGA will be programmed to just route the lines from the DSP to LCD.
considering the LCD is a 12*6 character LCD with the Hardware driver on it !
How can this be done ? Which register do I have to configure ?
Any suggestions / advices will be very much appreciated !!
Thanks in advance.
Regards
Stevean