Hi TI Experts,
*********************************************************************************
My situation: C6670, CCSV5.3
*********************************************************************************
In my board, the C6670 connects with FPGA through SPI. I just generate the .bin file and load the .bin file into FPGA.
When C6670 is powered up under SPI master boot, C6670 read the .bin file from FPGA through SPI interface.
So the FPGA just simulates a SPI flash.
*********************************************************************************
My testing project is 7612.GPIO_test.zip
The main codes are below
#include <stdio.h>
#include <string.h>
#include <c6x.h>
#include <stdlib.h>
#include "csl_gpio.h"
#include "csl_gpioAux.h"
#include <csl_psc.h>
#include <csl_pscAux.h>
#include "csl_tsc.h"
#include "csl_chip.h"
#include "csl_chipAux.h"
#include "csl_semAux.h"
#include "cslr_device.h"
#include "cslr_psc.h"
#include "csl_psc.h"
extern volatile unsigned int cregister TSCL;
CSL_GpioHandle CSL_GPIO_open (int instNum);
void cycleDelay (uint32_t count);
extern void MulticoreBoot();
int main(void)
{
int i=0;
char * send_msg;
int coreId = 0;
CSL_GpioHandle hGpio;
//*****************************************************//
//Boot test
MulticoreBoot();
//*****************************************************//
//*****************************************************//
//BBU GPIO test
coreId = DNUM;
TSCL = 1;
hGpio = CSL_GPIO_open (0);
CSL_GPIO_setPinDirOutput(hGpio, 14);
CSL_GPIO_setPinDirOutput(hGpio, 15);
if(coreId == 0)
{
CSL_GPIO_setOutputData(hGpio,14);
CSL_GPIO_setOutputData(hGpio,15);
while(1)
{
cycleDelay(1000000000);
CSL_GPIO_setOutputData(hGpio,14);
cycleDelay(1000000000);
CSL_GPIO_clearOutputData(hGpio,14);
}
}
else if(coreId == 1)
{
while(1)
{
cycleDelay(100000000);
CSL_GPIO_setOutputData(hGpio,15);
cycleDelay(100000000);
CSL_GPIO_clearOutputData(hGpio,15);
}
}
//*****************************************************//
while(1);
return 0;
}
CSL_GpioHandle CSL_GPIO_open (int instNum)
{
if (instNum == 0)
return (CSL_GpioHandle) CSL_GPIO_REGS;
/* Control comes here implies that an invalid instance number was passed */
return (CSL_GpioHandle) 0;
}
void cycleDelay (uint32_t count)
{
uint32_t sat;
if (count <= 0)
return;
sat = TSCL + count;
while (TSCL < sat);
}
In this project, the Core0 controls the GPIO15 to blink one LED and the Core1 controls the GPIO14 to blink the other LED.
The MulticoreBoot code is below
#include <stdlib.h>
#include <stdio.h>
#include <string.h>
#include <ti/csl/csl_chip.h>
#define CORE_NUM_6670 4
void MulticoreBoot()
{
int *pBootMagicAddCore0;
int *IpcGr0;
int i;
int coreId = 0;
coreId = DNUM;
if(coreId == 0)
{
/*write Boot Magic add of other cores and send IPC interrupt*/
*((int *)(0x118FFFFC)) = 0x0c0008a0;
*((int *)(0x128FFFFC)) = 0x0c0008a0;
*((int *)(0x138FFFFC)) = 0x0c0008a0;
IpcGr0 = (int*)0x02620240;
/*warning:when running on no-boot mode,core0~core7 must all be connected to the target*/
for(i = 1;i < CORE_NUM_6670;i++)//core0 sent ipc interrupt to
{
*(IpcGr0+i) = (*(IpcGr0+i)) | 0x00000001;
}
}
}
The Core0 runs the MulticoreBoot func to write the _c_int00 into Core1's Black Magic Address.
*********************************************************************************
If I put the .text into the per core's L2SRAM like below showing in CMD file
.text > CORE0_L2_SRAM
and then generate the .bin file. The Core0 and Core1 can run OK.
*********************************************************************************
But if I put the .text into the MSMCSRAM like below showing in CMD file
.text > SHRAM
and then generate the .bin file. The Core0 can run but the Core1 can not run OK.
My bin file generating tool is 3884.dsp_SPITool.zip
So what's the difference? And what should I do next?
*********************************************************************************
I suppose that maybe the Core0 can not write the _c_int00 into Core1's Black Magic Address.
For test, I modify the MulticoreBoot code like below
*((int *)(0x118FFFFC)) = 0x12345678;
But I can not find the number string 12345678 in Core0 project's .out or .bin files!
Is this the key to solve this issue?
*********************************************************************************
Thanks for any replies!
Regards,
Feng