This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DVRRDK350 dm816x sclr link low Efficient with HD input?



Hi:

      recently I want to down framerate,so use sclr link to drop frame,link chain just link this: capture->sclr->....

     input is :

              3 channel 1280x720@60fps 

               1 channel 1024x768@30fps

    set sclr link output 30fps,but only one channel is 30fps,other channel drop too much frames

    below is some log:

   [m3vpss ]  *** Capture Driver Advanced Statistics ***
 [m3vpss ] 
 [m3vpss ]  VIP Parser Reset Count : 0
 [m3vpss ] 
 [m3vpss ]      |   Total    Even     Odd  Total  Even   Odd  Min /  Max  Min /  Max Dropped Fid Repeat Frame Error Y/C
 [m3vpss ]  CH  |  Fields  Fields  Fields    FPS   FPS   FPS       Width      Height  Fields      Count (Desc Error Y/C)
 [m3vpss ]  ------------------------------------------------------------------------------------------------------------
 [m3vpss ]  000 |    2495    2495       0     60    60     0 1280 / 1280  720 /  720       3          0 0/0 (0/0)
 [m3vpss ]  100 |    2494    2494       0     60    60     0 1280 / 1280  720 /  720       3          0 0/0 (0/0)
 [m3vpss ]  200 |    2495    2495       0     60    60     0 1280 / 1280  720 /  720       2          0 0/0 (0/0)
 [m3vpss ]  300 |    1243    1243       0     30    30     0 1024 / 1024  768 /  768       1          0 0/0 (0/0)
 [m3vpss ] 
 [m3vpss ]  VIP Capture Port 0 | DescMissMatch1 = 1, DescMissMatch2 = 0 , DescMissMatch3 = 0
 [m3vpss ]  VIP Capture Port 1 | DescMissMatch1 = 0, DescMissMatch2 = 0 , DescMissMatch3 = 0
 [m3vpss ]  VIP Capture Port 2 | DescMissMatch1 = 0, DescMissMatch2 = 0 , DescMissMatch3 = 0
 [m3vpss ]  VIP Capture Port 3 | DescMissMatch1 = 0, DescMissMatch2 = 0 , DescMissMatch3 = 0
 [m3vpss ] 
 [m3vpss ]  *** Capture List Manager Advanced Statistics ***
 [m3vpss ] 
 [m3vpss ]  List Post Count        : 822257
 [m3vpss ]  List Stall Count       : 0
 [m3vpss ]  List Post Time (ms)    : Max = 3, Min = 0, Avg = 0, Total = 1401
 [m3vpss ]  INTC Timeout Count     : (0, 0) (Min timeout value = 932, 987)
 [m3vpss ]  Descriptor miss found count : 0
 [m3vpss ] 
 [m3vpss ] 
 [m3vpss ]  VIP and VPDMA registers,
 [m3vpss ]  VIP0 : FIQ_STATUS  : 0x4810551c = 0x00000000
 [m3vpss ]  VIP1 : FIQ_STATUS  : 0x48105a1c = 0x00000000
 [m3vpss ]  VPDMA: LIST_BUSY   : 0x4810d00c = 0x00a20000
 [m3vpss ] 
 [m3vpss ] 
 [m3vpss ]  1820733: CAPTURE: Fields = 8717 (fps = 209, CPU Load = 0)
 [m3vpss ]  1820733: CAPTURE: Num Resets = 0 (Avg 0 ms per reset)
 [m3vpss ] 
 [m3vpss ]  *** [Scalar0   ] SCLR Statistics ***
 [m3vpss ] 
 [m3vpss ]  Elasped Time           : 27 secs
 [m3vpss ]  Total Fields Processed : 3080
 [m3vpss ]  Total Fields FPS       : 129 FPS
 [m3vpss ] 
 [m3vpss ] 
 [m3vpss ]  CH  | In Recv In Reject In Process Out Skip Out User Out Latency  
 [m3vpss ]  Num | FPS     FPS       FPS        FPS    FPS   Skip FPS Min / Max
 [m3vpss ]  ---------------------------------------------------------------------
 [m3vpss ]    0 |      61        11         29  29       20       11  20  66
 [m3vpss ]    1 |      61         8         22  22       30        8  19  64
 [m3vpss ]    2 |      61         5         16  16       39        5  18  64
 [m3vpss ]    3 |      30         0          5   5       25        0  18  54

 

is sclr link not supoort 60fps input?

another question: is there other link can used to reduce the stream framerate?

 

thanks very much!