Hi,
I am attempting to build and run the dcan_TxRx project in the AM335X StarterWare 02 00 01 01 (and CCS5.4). It is missing a number objects in the link:
DCANModuleClkConfig
DCANMsgRAMInit
DCANPinMuxSetup
These appear to be in the Platform library in the dcan.c file. It seems that I am building the platform library for the evmskAM335x but I have the Industrial Control AM335X board. Thus the debug version of the library does not get into the right place (bin\arm7a\cgt_css\evmAM335x\platform\Debug). Do I ether change the project or find the correct platform project to build for my board ?
I found I do have a a release version of the ICE platform library and if I copy that to debug I can build the dcan project.
This is not exactly the way it should work so are there any suggestions of what to try.