This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Pandaboard connect LCD module by MIPI interface

Hi,

My OS : ubuntu 12.04

download from:   http://www.omappedia.org/wiki/Ubuntu_Pre-Built_Binaries

My pandaboard has been already entered desktop. 

I see pandaboard's spec that can support MIPI I/F.

My LCD module has five ports(DATAP DATAN CLKP CLKN GND),

How to connect my pandaboard?

Is it right that connect pandaboard through J1 (LCD connector) ?

And the files which I have to modify are omapdss.h and board-omap4panda.c .

I can't find them.

I have just a image file to write in SD card.

Do you have any path to download the source code?

And how to modify the files ?

the web that referred to :http://wiijerry.blogspot.tw/2012/02/pandaboard-lcd-display.html?showComment=1415172313811#c2733309191175551080

Is it  using by MIPI interface?

THX