This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Building ELF NDK for DM6437 processor

Hello,

I am using Code Composer Studio version 5.5.00077, C6000 Bios version 6.35.4.50, C6000 Compiler version 7.4.11, and C6000 XDCTools version 3.25.4.88.  The IDE is running under Windows 7

I am trying to build NDK 2.24.00.11 for DM6437 processor using ELF binaries. 

I noticed that definitions for ELF C64P output are absent in both ndk.mak and ndk.bld.

Is there a way to add them?  When I rebuild the NDK using just C64P directives, incorrect libraries are generated,  with extension .a64p instead of .ae64p.  I edited ndk.bld, and modified C6xOpts to specify ELF abi (--abi=eabi).  From watching verbose build output, I believe that correct object files were generated, but they were packaged in libraries with incorrect extension (.a64P instead of .ae64P). 

What is (or is there) a correct way to generate ELF NDK libraries for C64P?

Will adding target "ti.targets.elf.C64P" do the trick?


Thank you in advance,

Dmitry.