Hello TI,
Some ADCs with SPI bus data interface require or recommend the serial clock to be stopped during the conversion phase. Examples include Analog Devices AD7985 and Linear Technology LTC2323-16.
Paragraph 2.10 of spruhh0 (entitled "SPI Operation Using the Clock Stop Mode") asserts that the McBSP on Keystone 1 devices does not support the SPI protocol, but other than that I cannot find any mention of discontinuous clocking of the McBSP or SPI peripherals for the TMS320C665x in the spruhh0 and sprugp2a documents.
Would it be possible to confirm or deny whether direct interfacing to such devices as are mentioned above is possible for TMS320C665x using the McBSP or SPI ports?