This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PRIME DC IEC-61334-4-32 API Specification: BIND_SAP

Hi E2E,

Is the expected use case that (1) the external app will call IEC_61334_4_32_LLC_BIND_SAP once and use this SAP for all, to potentially multiple destinations, IEC_61334_4_32_LLC_DATA_REQ calls, or (2) the external app calls IEC_61334_4_32_BIND_SAP for each destination it intends to call IEC_61334_4_32_LLC_DATA_REQ?

Thanks and Regards,
...doug