This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The error when I run scd in DVRRDK 02.00.00.23

Other Parts Discussed in Thread: TVP5158

Hi all:

I make enablescd=TRUE  in demo_vcap_venc_vdis.c   but when I run the demo ,the print is as below:

======= ==
Main Menu
======= ==
1: VCAP + VENC + VDEC + VDIS - Progressive SD Encode + Decode
3: VCAP + VENC + VDIS - SD Encode ONLY
4: VCAP + VENC + VDIS - HD Encode ONLY
5: VDEC + VDIS - SD/HD Decode ONLY
6: VCAP + VDIS - NO Encode or Decode
7: CUSTOM DEMO - 2Ch D1 Encode
8: CUSTOM DEMO - 1Ch D1 + 4CIF Encode
9: CUSTOM DEMO - 1Ch D1 Decode
e: Exit
Enter Choice: 3
--------------- CHANNEL DETAILS-----------
--
Capture Channels => 1
Enc Channels => Primary 1, Secondary 1
Disp Channels => 1
-----------------------------------------
--
Enable file write (YES - y / NO - n) : y
File write ENABLED !!!
Enter file write path : / data
Selected file write path [/data ]
Select File Write CH ID [0 .. 0] : 0
Selected CH ID = 0
[host] MCFW_IPCFRAMES:VcapVenc_ipcFramesSendRecvFxn:Entered...start process !!!
0: SYSTEM: System Common Init in progress !!!
Opened file [/data/VID_CH00.h264] for writing CH0
2: SYSTEM: IPC init in progress !!!
9: SYSTEM: Opening MsgQ Heap [IPC_MSGQ_MSG_HEAP] ...
12: SYSTEM: Creating MsgQ [HOST_MSGQ] ...
14: SYSTEM: Creating MsgQ [HOST_ACK_MSGQ] ...
17: SYSTEM: Opening MsgQ [DSP_MSGQ] ...
18: SYSTEM: Opening MsgQ [VIDEO-M3_MSGQ] ...
20: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ...
22: SYSTEM: Notify register to [DSP] line 0, event 12 ...
23: SYSTEM: Notify register to [VIDEO-M3] line 0, event 12 ...
25: SYSTEM: Notify register to [VPSS-M3] line 0, event 12 ...
26: SYSTEM: IPC init DONE !!!
28: SYSTEM: Creating ListMP [HOST_IPC_OUT_28] in region 0 ...
32: SYSTEM: Creating ListMP [HOST_IPC_IN_28] in region 0 ...
34: SYSTEM: ListElem Shared Addr = 0x41fc0e80
36: SYSTEM: Creating ListMP [HOST_IPC_OUT_29] in region 0 ...
39: SYSTEM: Creating ListMP [HOST_IPC_IN_29] in region 0 ...
42: SYSTEM: ListElem Shared Addr = 0x41fd9780
45: SYSTEM: Creating ListMP [HOST_IPC_OUT_23] in region 0 ...
48: SYSTEM: Creating ListMP [HOST_IPC_IN_23] in region 0 ...
50: SYSTEM: ListElem Shared Addr = 0x41ff2080
52: SYSTEM: Creating ListMP [HOST_IPC_OUT_24] in region 0 ...
56: SYSTEM: Creating ListMP [HOST_IPC_IN_24] in region 0 ...
58: SYSTEM: ListElem Shared Addr = 0x42011680
60: SYSTEM: Creating ListMP [HOST_IPC_OUT_25] in region 0 ...
64: SYSTEM: Creating ListMP [HOST_IPC_IN_25] in region 0 ...
67: SYSTEM: ListElem Shared Addr = 0x42030c80
68: SYSTEM: System Common Init Done !!!
70: MCFW : CPU Revision [ES2.0] !!!
71: MCFW : Detected [UNKNOWN] Board !!!
72: MCFW : Base Board Revision [REV A] !!!
CAPTURE: Detected video (720x288@50Hz, 1) !!!
CAPTURE ERROR: Could not get chip id for tvp instace 1 !!!
CAPTURE ERROR: Could not get chip id for tvp instace 2 !!!
CAPTURE ERROR: Could not get chip id for tvp instace 3 !!!
TVP5158: 0x58: Downloading patch ...
TVP5158: 0x58: Downloading patch ... DONE !!!
TVP5158: 0x58: 5158:0002: 0302
Audio Channels are not supported
Audio Channels are not supported
Audio Channels are not supported
Audio Channels are not supported

[m3vpss ] 31235: CAPTURE: Create in progress !!!
[m3vpss ] 31264: CAPTURE: VIP0 PortA capture mode is [ 8-bit, Non-mux Embedde

[m3vpss ] CAPTURE::HEAPID:0 USED: 192
[m3vpss ] 31292: CAPTURE: Create Done !!!
[m3vpss ] 31295: DUP : Create Done !!!
[m3vpss ] 31296: MERGE : Create Done !!!
[m3vpss ] 31298: SCLR: Create in progress !!!
[m3vpss ] 31300: SCLR : Loading Up-scaling Co-effs ...
[m3vpss ] 31300: SCLR : Co-effs Loading ... DONE !!!
[m3vpss ] SCLR:HEAPID:0 USED: 64
[m3vpss ] SCLR:HEAPID:1 USED: 5952
[m3vpss ] 31300: SCLR: Create Done !!!
[m3vpss ] 31301: NSF: Create in progress !!!
[m3vpss ] NSF::HEAPID:0 USED: 128
[m3vpss ] NSF::HEAPID:1 USED: 4928
[m3vpss ] 31303: NSF: Create Done !!!
[m3vpss ] 31305: DEI : Create in progress !!!

[m3vpss ] 31388: DEI : Loading Up-scaling Co- effs
out of the vpss
[m3vpss ] 31389: DEI : Co-effs Loading ... DONE !!!
[c6xdsp ] 30665: IPC_FRAMES_IN : Create in progress !!!
[c6xdsp ] 30665: SYSTEM: Opening ListMP [VPSS-M3_IPC_OUT_23] ...
[m3vpss ] DEI:HEAPID:0 USED: 64
[c6xdsp ] 30666: SYSTEM: Opening ListMP [VPSS-M3_IPC_IN_23] ...
[m3vpss ] DEI:HEAPID:1 USED: 5264
[c6xdsp ] 30666: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ...
[m3vpss ] 31389: DEI : Create Done !!!
[m3vpss ] 31390: MERGE : Create Done !!!
[m3vpss ] 31392: MERGE : Create Done !!!
[c6xdsp ] IPC_FRAMES_IN:HEAPID:0 USED: 240
[m3vpss ] 31395: IPC_FRAMES_OUT : Create in progress !!!
[c6xdsp ] 30667: IPC_FRAMES_IN : Create Done !!!
[c6xdsp ] 30669: ALG : Create in progress !!!
[c6xdsp ] 30678: SCD : Create in progress !!!
[m3vpss ] 31396: IPC_FRAMES_OUT : Create Done !!!
[c6xdsp ] 30678: SCD : Max WxH = 352 x 288, Max CH = 16, FPS = 2 !!!
[c6xdsp ] 30678: SCD : Create ERROR - SCD channels < InQueue Channels !!!
[c6xdsp ] 30678: Assertion @ Line: 133 in links_c6xdsp/alg_link/algLink_priv .!

PS : my viedo is 352*288    I dont kown how to solve  . Can you help me?