I seem to be finding conflicting information on if its possible to use the EMIF of TMS320C6424 with S29GL512 ( a 64 mb spansion flash). Doing so requires more than the standard 24 adress lines. Im assuming that this means using one of the chip select pins (i.e. EM_CS2) but it seems to me that the correct way of doing this is largely undocumented.
We use an old code example for the evaluation module from spectrum digital as the driver for the 32 mb version we have today. That file seems to have definitions for the 64 mb version as well so it seems like its possible to use a 64 mb flash seamlessly. Is that true? Are there any downsides or cave ats?