Other Parts Discussed in Thread: AM4377
Hello everyone,
I am using AM437x GP EVM Rev. 1.2A. I just need to ask whether we need to configure PMIC for 1GHz operating point as we do for Beagle bone black.
Thanks,
Umair Khan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: AM4377
Hello everyone,
I am using AM437x GP EVM Rev. 1.2A. I just need to ask whether we need to configure PMIC for 1GHz operating point as we do for Beagle bone black.
Thanks,
Umair Khan
Hi Umair,
AM437x GP EVM Rev. 1.2A is a pre-production build with limited quantities delivered. I have one of these and I think it has a 800MHz device on it (no "100" suffix).
Umair, the PMIC definitely needs to be configured for a higher voltage as higher MPU frequencies require higher voltages on the VDD_MPU rail. See Section 5.4 of the AM437x datasheet.
With that said, your device may be limited in its maximum supported frequency as Biser has pointed out.
Regards,
James
This is creating a bit of confusion in my mind. Can you please said something with surety about the maximum supported frequency? This will make my problem very easy.
Thanks for your cooperation.
Umair Khan.
To help you, please check this document http://www.ti.com/lit/ds/symlink/am4376.pdf
Addendum page 1 (right after page 255)
XAM437XAZDN100 = 1GHz
XAM437XAZDN = 800MHz
I consulted that manual but as in the manual:
DEVICE SPEED RANGE
80 = 800-MHz Cortex-A9
There was no 80 postfix. Thats why I was a bit confused.
Thanks. You solved my problem.
One more explanation:
once it goes to full production, then we will have AM4376BZDN80 = 800MHz and AM4376BZDN100 = 1GHz. (as well as AM4377/8/9). My post above was related to iniitial samples only....