Hi all
I can change the kernel logo to my product's logo by creating a .ppm image and putting it into logo folder.
Now there are two images as android-logo-mask.png and android-shine-text.png.. How to change them and get my custom shining logo?Are these images used for bootanimation? If I change these files with my files will they also create a bootanimation?
What is an rle file used for?
there are some files which are making me confused,
one is in kernel/drivers/video/logo/logo.c
one is in framework/base/core/init.c
one is in device/...overlay/bootanimation.cpp I think these files are for bootanimation
I compiled my android and there is no bootanimation.zip file created, still that shining logo appears.
If I want a custom bootanimation do I have to put that in out folder?