This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI Flash Writer

Other Parts Discussed in Thread: OMAP-L137

I've just received my new custom OMAP-L137 based boards (Revision 3, so I've been through this before) and I'm trying to flash u-boot, etc. In the past (last rev of board), I used spiflash_writer_ccsv3.out.

When I try to load this to my board, I get the error "File: C:\bin\spiflash_writer_ccsv3.out Does not match the target type, not loaded."

In the Component Manager, both TMS320C64xx and TMS320C67xx are set to "Texas Instruments C6000 Code Generation Tools <v6.1.9>" and "Texas Instruments DSP/BIOS <5.33.03>"

These settings have worked in the past, so I'm assuming that the board that I'm trying to bring up has a problem. We have verified power, ground, clock. I've also checked the GEL file for my expected settings (I have more SDRAM than the EVM board and my CAS latency is 3. These settings are the same as the previous revisions of the board.) Can anyone give me a suggestion as to what might be causing this error message? I have shut down CCS, power-reset the board, and brought CCS back up. I've removed the default GEL file and opened my own (although I've tried it both ways, and it fails with either GEL file in the same way).

CCS = 3.3.82.13, EDE = 5.98.0.393, BIOS = 5.33.03, CGT = v6.1.9, Board Revision = 00.00.86, Target Silicon Revision = 00.00.05.

Is it related to those last two? Can I do anything about that?