Hi,
I want to test my SRIO's transmitting speed, and performed an SWRITE command between two boards. If the completion code returns 0, could i regard it as an SWRITE transmitting over?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to test my SRIO's transmitting speed, and performed an SWRITE command between two boards. If the completion code returns 0, could i regard it as an SWRITE transmitting over?
Hi,
SRIO Throughput test code is available in the MCSDK package. I have tested this example on loopback or board to board modes successfully. Better to try this SRIO example for your testing
MCSDK Path: C:\ti\pdk_C6678_1_1_2_6\packages\ti\drv\exampleProjects\SRIO_TputBenchmarkingTestProject
Refer section "5.3 Two EVMs connected using breakout cards" and "9.4 Setting up B-E-B connection mode (board to board, external interface)" on SRIO_Benchmarking_Example_Code_Guide document.
Doc Path: \ti\pdk_C6678_1_1_2_6\packages\ti\drv\srio\test\tput_benchmarking\docs\SRIO_Benchmarking_Example_Code_Guide
Thanks,