This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP L138 hardware support

Other Parts Discussed in Thread: OMAP-L138, OMAPL138

Hello to you all ! This is my first post in TI community.
Until now, my main development board for educational purposes were C6713 DSPs. I own two boards, which are the OMAP-L138/C6748 DSP Experimenter Kit for Universities and L138/C6748 Development Kit (LCDK). The boards are for lab use, and also for Project developments in research work. In current time, i interested in developing computer vision algorithms and on this i have some concerns for the boards. Because i want to develop a GUI application that will control the vision algorithm my first concern is based on the LCD module that is included optionally in eXperimenter Kit. As far as I have read, the LCD Sharp TFT monitor that is compatible with the kit is LQ043T1DG01 4.3 ", but Sharp that consists of the manufacturing company stopped the production on 31 of March 2013 and replaced the monitor with LQ043DG28 that is not electrically compatible with the parts it replaces and as a consequence not compatible with eXperimenter Kit. So, my first question is where can i find an eXperimenter Kit with the proper monitor module with it (LQ043T1DG01). I already contact LOGIC PD and does not support neither the board nor the LCD module. Since the project that i want to develope consists of Real-time image processing, i want to have a live video streaming as an input. Unfortunately, eXperimenter Kit does not provide composite input in standard version, but the whole procedure can be made only with User Interface (UI) Board. Since this is not the case for me at the moment, i interested in Development Kit (LCDK) that has the composite video input jack by default. So, is LCDK board compatible with TFT LCD monitor that is being provided separately from third party cooperation companies, and what companies does still supply it? Best regards.