Hi,
I've a TI J6 Vayu EVK Infotainment kit running Android 6AK1.1. I'm very new to this development environment and Android internals in general. So, please bear with me.
Since this platform doesn't have wifi module, on my board eth1 is plugged into an Apple Airport Express (AE) (which acts as a wifi to ethernet converter).
Everything works ok (i.e. TI board gets internet) if AE connects to a regular wifi n/w such as home or office. However, if I connect AE to a cellular wifi hotspot the TI board doesn't like it and doesn't get IP address. I 100% made sure that other devices can connect to cellular hotspot and it's all good. I also tried T-Mobile and Verizon hotspots and it's the same problem.
So, can anyone shed some light on this, why the TI board doesn't like cell hotspots to ethernet connection. I read in several forums here, that eth0/eth1 MAC addresses are randomly assigned at power up and I did notice it on my setup. Could my issue be related to that?
Just to summarize, I need to get internet on the TI Vayu kit via cellular wifi hotspot to ethernet connection in eth1.
Thanks,
Kaushal