Hello Ti
We use am335x Starter Kit SDK6 on our custom board and don't found any command in u-boot level after I have build the u-boot.
===========================================
Hit any key to stop autoboot: 0
Unknown command 'mmc' - try 'help'
Unknown command 'mmc' - try 'help'
Unknown command 'run' - try 'help'
U-Boot# help
Unknown command 'help' - try 'help'
U-Boot#
=============================================
These steps we were taking:
1. cd <SDK_folder>/ti-sdk-am335x-evm-06.00.00.00/board-support/u-boot-2013.01.01-psp06.00.00.00$
2. export ARCH=arm
3. export CROSS_COMPILE=~/ti-sdk-am335x-evm-06.00.00.00/linux-devkit/sysroots/i686-arago-linux/usr/bin/arm-linux-gnueabihf-
4. export PATH="<SDK INSTALL DIR>/linux-devkit/sysroots/i686-arago-linux/usr/bin:$PATH
5. make am335x_evm_config
6 make
====================================================================================
These are my enviroments:
$ printenv
SSH_AGENT_PID=2583
GPG_AGENT_INFO=/tmp/keyring-ltTjJC/gpg:0:1
TERM=xterm-256color
SHELL=/bin/bash
XDG_SESSION_COOKIE=c5d844eaa486c24a959661d900000015-1415770149.412823-625948885
WINDOWID=67108869
OLDPWD=/home/bernie/ti-sdk-am335x-evm-06.00.00.00/board-support
GNOME_KEYRING_CONTROL=/tmp/keyring-ltTjJC
LC_ALL=en_US.UTF-8
USER=bernie
JRE_HOME=/usr/lib/jvm/java-6-oracle/jre
LS_COLORS=rs=0:di=01;34:ln=01;36:mh=00:pi=40;33:so=01;35:do=01;35:bd=40;33;01:cd=40;33;01:or=40;31;01:su=37;41:sg=30;43:ca=30;41:tw=30;42:ow=34;42:st=37;44:ex=01;32:*.tar=01;31:*.tgz=01;31:*.arj=01;31:*.taz=01;31:*.lzh=01;31:*.lzma=01;31:*.tlz=01;31:*.txz=01;31:*.zip=01;31:*.z=01;31:*.Z=01;31:*.dz=01;31:*.gz=01;31:*.lz=01;31:*.xz=01;31:*.bz2=01;31:*.bz=01;31:*.tbz=01;31:*.tbz2=01;31:*.tz=01;31:*.deb=01;31:*.rpm=01;31:*.jar=01;31:*.war=01;31:*.ear=01;31:*.sar=01;31:*.rar=01;31:*.ace=01;31:*.zoo=01;31:*.cpio=01;31:*.7z=01;31:*.rz=01;31:*.jpg=01;35:*.jpeg=01;35:*.gif=01;35:*.bmp=01;35:*.pbm=01;35:*.pgm=01;35:*.ppm=01;35:*.tga=01;35:*.xbm=01;35:*.xpm=01;35:*.tif=01;35:*.tiff=01;35:*.png=01;35:*.svg=01;35:*.svgz=01;35:*.mng=01;35:*.pcx=01;35:*.mov=01;35:*.mpg=01;35:*.mpeg=01;35:*.m2v=01;35:*.mkv=01;35:*.webm=01;35:*.ogm=01;35:*.mp4=01;35:*.m4v=01;35:*.mp4v=01;35:*.vob=01;35:*.qt=01;35:*.nuv=01;35:*.wmv=01;35:*.asf=01;35:*.rm=01;35:*.rmvb=01;35:*.flc=01;35:*.avi=01;35:*.fli=01;35:*.flv=01;35:*.gl=01;35:*.dl=01;35:*.xcf=01;35:*.xwd=01;35:*.yuv=01;35:*.cgm=01;35:*.emf=01;35:*.axv=01;35:*.anx=01;35:*.ogv=01;35:*.ogx=01;35:*.aac=00;36:*.au=00;36:*.flac=00;36:*.mid=00;36:*.midi=00;36:*.mka=00;36:*.mp3=00;36:*.mpc=00;36:*.ogg=00;36:*.ra=00;36:*.wav=00;36:*.axa=00;36:*.oga=00;36:*.spx=00;36:*.xspf=00;36:
XDG_SESSION_PATH=/org/freedesktop/DisplayManager/Session0
XDG_SEAT_PATH=/org/freedesktop/DisplayManager/Seat0
SSH_AUTH_SOCK=/tmp/keyring-ltTjJC/ssh
SESSION_MANAGER=local/ubuntu:@/tmp/.ICE-unix/2545,unix/ubuntu:/tmp/.ICE-unix/2545
DEFAULTS_PATH=/usr/share/gconf/ubuntu-2d.default.path
WORKON_HOME=/home/bernie/.virtualenvs
PROJECT_HOME=/home/bernie/Devel
XDG_CONFIG_DIRS=/etc/xdg/xdg-ubuntu-2d:/etc/xdg
PATH=/home/bernie/ti-sdk-am335x-evm-06.00.00.00/linux-devkit/sysroots/i686-arago-linux/usr/bin:~/ti-sdk-am335x-evm-06.00.00.00/linux-devkit/sysroots/i686-arago-linux/usr/bin:/home/bernie/bin:/usr/lib/jvm/java-6-oracle/bin:/usr/lib/jvm/java-6-oracle/jre/bin:/usr/lib/lightdm/lightdm:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games
DESKTOP_SESSION=ubuntu-2d
QT_IM_MODULE=ibus
PWD=/home/bernie/ti-sdk-am335x-evm-06.00.00.00/board-support/u-boot-2013.01.01-psp06.00.00.00
XMODIFIERS=@im=ibus
JAVA_HOME=/usr/lib/jvm/java-6-oracle
GNOME_KEYRING_PID=2534
LANG=en_US.UTF-8
MANDATORY_PATH=/usr/share/gconf/ubuntu-2d.mandatory.path
QMAKESPEC=/home/bernie/ti-sdk-am335x-evm-06.00.00.00/linux-devkit/arm-arago-linux-gnueabi/usr/share/qtopia/mkspecs/linux-g++
UBUNTU_MENUPROXY=libappmenu.so
GDMSESSION=ubuntu-2d
SHLVL=1
HOME=/home/bernie
GNOME_DESKTOP_SESSION_ID=this-is-deprecated
LOGNAME=bernie
XDG_DATA_DIRS=/usr/share/ubuntu-2d:/usr/share/gnome:/usr/local/share/:/usr/share/
DBUS_SESSION_BUS_ADDRESS=unix:abstract=/tmp/dbus-YPMLNReCd9,guid=86dc88ed93caf9c3a2b0aa750000005e
CLASSPATH=:.:/usr/lib/jvm/java-6-oracle/lib:/usr/lib/jvm/java-6-oracle/jre/lib
LESSOPEN=| /usr/bin/lesspipe %s
ARCH=arm
CROSS_COMPILE=/home/bernie/ti-sdk-am335x-evm-06.00.00.00/linux-devkit/sysroots/i686-arago-linux/usr/bin/arm-linux-gnueabihf-
DISPLAY=:0
XDG_CURRENT_DESKTOP=Unity
GTK_IM_MODULE=ibus
LESSCLOSE=/usr/bin/lesspipe %s %s
COLORTERM=gnome-terminal
XAUTHORITY=/home/bernie/.Xauthority
_=/usr/bin/printenv
============================================================================================
I don't think that my code is wrong , because I just revise the part of read eeprom. Thank you.
and I attache the patch with u-boot
diff --git a/MLO.byteswap b/MLO.byteswap
index c1b1af2..fa42848 100644
Binary files a/MLO.byteswap and b/MLO.byteswap differ
diff --git a/board/ti/am335x/board.c b/board/ti/am335x/board.c
index 7704718..0837d92 100644
--- a/board/ti/am335x/board.c
+++ b/board/ti/am335x/board.c
@@ -90,7 +90,7 @@ int board_is_evm_15_or_later(void)
* Read header information from EEPROM into global structure.
*/
static int read_eeprom(void)
-{
+{
/* Check if baseboard eeprom is available */
if (i2c_probe(CONFIG_SYS_I2C_EEPROM_ADDR)) {
puts("Could not probe the EEPROM; something fundamentally "
@@ -106,12 +106,12 @@ static int read_eeprom(void)
return -EIO;
}
- if (header.magic != 0xEE3355AA) {
+ //if (header.magic != 0xEE3355AA) {
/*
* read the eeprom using i2c again,
* but use only a 1 byte address
*/
- if (i2c_read(CONFIG_SYS_I2C_EEPROM_ADDR, 0, 1,
+ /* if (i2c_read(CONFIG_SYS_I2C_EEPROM_ADDR, 0, 1,
(uchar *)&header, sizeof(header))) {
puts("Could not read the EEPROM; something "
"fundamentally wrong on the I2C bus.\n");
@@ -123,7 +123,7 @@ static int read_eeprom(void)
header.magic);
return -EINVAL;
}
- }
+ }*/
return 0;
}
@@ -651,13 +651,16 @@ void s_init(void)
#endif
/* Initalize the board header */
- enable_i2c0_pin_mux();
+ enable_i2c1_pin_mux();
+ i2c_set_bus_num(1);
i2c_init(CONFIG_SYS_I2C_SPEED, CONFIG_SYS_I2C_SLAVE);
#ifndef CONFIG_NOR_BOOT
- if (read_eeprom() < 0)
- puts("Could not get board ID.\n");
+ //if (read_eeprom() < 0)
+ // puts("Could not get board ID.\n");
#endif
+
+
/* Check if baseboard eeprom is available */
if (i2c_probe(CONFIG_SYS_I2C_EEPROM_ADDR)) {
puts("Could not probe the EEPROM; something fundamentally "
@@ -671,12 +674,12 @@ void s_init(void)
" wrong on the I2C bus.\n");
}
- if (header.magic != 0xEE3355AA) {
+ //if (header.magic != 0xEE3355AA) {
/*
* read the eeprom using i2c again,
* but use only a 1 byte address
*/
- if (i2c_read(CONFIG_SYS_I2C_EEPROM_ADDR, 0, 1,
+ /*if (i2c_read(CONFIG_SYS_I2C_EEPROM_ADDR, 0, 1,
(uchar *)&header, sizeof(header))) {
puts("Could not read the EEPROM; something "
"fundamentally wrong on the I2C bus.\n");
@@ -688,8 +691,11 @@ void s_init(void)
header.magic);
hang();
}
- }
-
+ }*/
+ header.magic=0xEE3355AA;
+ strcpy(header.name,"A335X_SK");
+ strcpy(header.version,"1.2B");
+ strcpy(header.serial,"8SKU");
enable_board_pin_mux(&header);
if (!strncmp("A335X_SK", header.name, HDR_NAME_LEN)) {
/*
@@ -728,8 +734,8 @@ void s_init(void)
int board_init(void)
{
i2c_init(CONFIG_SYS_I2C_SPEED, CONFIG_SYS_I2C_SLAVE);
- if (read_eeprom() < 0)
- puts("Could not get board ID.\n");
+ //if (read_eeprom() < 0)
+ // puts("Could not get board ID.\n");
gd->bd->bi_boot_params = PHYS_DRAM_1 + 0x100;
diff --git a/board/ti/am335x/board.h b/board/ti/am335x/board.h
index 48e112e..598d4bd 100644
--- a/board/ti/am335x/board.h
+++ b/board/ti/am335x/board.h
@@ -50,5 +50,6 @@ void enable_uart3_pin_mux(void);
void enable_uart4_pin_mux(void);
void enable_uart5_pin_mux(void);
void enable_i2c0_pin_mux(void);
+void enable_i2c1_pin_mux(void);
void enable_board_pin_mux(struct am335x_baseboard_id *header);
#endif
diff --git a/board/ti/am335x/mux.c b/board/ti/am335x/mux.c
index 85e83bb..529a224 100644
--- a/board/ti/am335x/mux.c
+++ b/board/ti/am335x/mux.c
@@ -275,6 +275,11 @@ void enable_i2c0_pin_mux(void)
configure_module_pin_mux(i2c0_pin_mux);
}
+void enable_i2c1_pin_mux(void)
+{
+ configure_module_pin_mux(i2c1_pin_mux);
+}
+
/*
* The AM335x GP EVM, if daughter card(s) are connected, can have 8
* different profiles. These profiles determine what peripherals are
@@ -349,7 +354,7 @@ void enable_board_pin_mux(struct am335x_baseboard_id *header)
configure_module_pin_mux(mmc0_no_cd_pin_mux);
} else if (!strncmp(header->name, "A335X_SK", HDR_NAME_LEN)) {
/* Starter Kit EVM */
- configure_module_pin_mux(i2c1_pin_mux);
+ configure_module_pin_mux(i2c0_pin_mux);
configure_module_pin_mux(gpio0_7_pin_mux);
configure_module_pin_mux(rgmii1_pin_mux);
configure_module_pin_mux(mmc0_pin_mux_sk_evm);