I'm developing NVR solution on 8168 platform.
I use "ti-ezsdk_dm816x-evm_5_05_02_00" SDK.
My base code is "decode_mosaicdisplay" which can 4 decode and display h264 file at the same-time.
I need 16 decode & display by mosaicdisplay, I modify max decoder 4->8... It was successful.
But I set max decoder to 9... program go to hang. on
"eError = OMX_GetHandle(&pAppData->pScHandle[i], (OMX_STRING)"OMX.TI.VPSSM3.VFPC.INDTXSCWB",
pAppData->scILComp[i], &pAppData->pCbScaler)"
on the log.. OMX_GetHandle can make 8 instance. but over 8.. it goes to hang.
What is maximun instance of "OMX_GetHandle(OMX.TI.VPSSM3.VFPC.INDTXSCWB)" on 8169?
And How can I do ?