This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Hyperlink interrupt



Hi

I want to send interrupt from dspA to dspB via Hyperlink.

I have some question.

1) Is HYPERLINK_0_INT(111) event input of CIC0 which in remote side?

2) How can I use Hyperlink_int_i[x] for trigger interrupt to remote side? Are there any register for trigger and send interrupt via SerDes?

3) How can I understand that interrupt is received in remote side? Are there any register for it?

4)Should I use INTC or only CIC0is enough ? 

Thanks