Other Parts Discussed in Thread: OMAPL138
I am trying to set multiple serializers (2 TX and 2 RX) in OMAPL138 McASP0. I am using the linux-2.6.37-psp03.21.00.04.sdk that has code for 1 channel (1 TX and 1 RX ) only. I have gotten 1 TX and 1 RX working very well in my board using omapl138 McASP. But when I set 2tx + 2rx to this framework, I see that DMA IRQ is not coming. Following are the modifications I made to the default architecture. Please tell me if I am missing something?
/* davinci da850 evm audio machine driver */
static u8 da850_iis_serializer_direction[] = {
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
TX_MODE, TX_MODE, RX_MODE, RX_MODE,
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
};
static struct snd_platform_data da850_evm_snd_data = {
.tx_dma_offset = 0x2000,
.rx_dma_offset = 0x2000,
.op_mode = DAVINCI_MCASP_IIS_MODE,
.num_serializer = ARRAY_SIZE(da850_iis_serializer_direction),
.tdm_slots = 4,
.serial_dir = da850_iis_serializer_direction,
.asp_chan_q = EVENTQ_0,
.version = MCASP_VERSION_2,
.txnumevt =2,
.rxnumevt =2,
};