This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ECG implementation on TMS320VC5505 EVM



Hi,

I have 2 questions on ECG daughter card for VC5505.

1.  J22 is a 2x11 double row male header on VC5505 EVM which is used to interface the ECG front end daughter card  and VC5505 EVM. But the corresponding female on the daughter card is 2x10. I have the ECG daughter card as well as the digital stethescope daughter card. both seem to have the same problem.

2. To run the ECG DSP software in debug mode, the instruction mannual asks to copy a .gel file from the CD. But no such file is there on the CD. I've checked the myti software page as well, but the the files required for software intallation seem to be missing.

Thanks

Raghu