There seems to be a contradiction in the TRM. in section 8.1.6.12 it states the DMTIMER0 can only be sourced from the RC32k but yet in 20.1.2 it show it can be sourced from RC32,osc_32k or m_osc.
Which is correct?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There seems to be a contradiction in the TRM. in section 8.1.6.12 it states the DMTIMER0 can only be sourced from the RC32k but yet in 20.1.2 it show it can be sourced from RC32,osc_32k or m_osc.
Which is correct?
Hi David,
I will ask for confirmation but it seems that Section 8.1.6.12 is correct, at least I couldn't find a register to set DMTIMER0 clock source.