This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About BCP special feature



Hi,

There is a problem with bcp recently. My DSP is TCI6680, and I used it to implement the PDCCH. Can you have some example code to reference? or some articles to read?

As we known, the PDCCH should do DCI multiplexing when finish all DCI rate matching , After BCP do all DCI rate matching and finish multiplexing, it can input to bcp do modulation, so there is a problem: the multiplexing bit stream input to MOD submodule should have a format? and how I used the flush/drop to implement the synchronization?

Thank you in advance!