Other Parts Discussed in Thread: OMAPL138, OMAP-L138, SYSCONFIG
Hi,
I would like to build a OMAPL138 DSP firmware which activates the USB0 .
For the first stage I'm trying to use the evmomapl138_v1's example "usb".
Environment:
- LogicPD's Zoom OMAP-L138 eXperimenter Kit.
- CCS 3.3
- Gel file: OMAPL138_DSP.gel (from LogicPD site)
The problem:
------------------------------------------------------------
OMAP-L138 USB Test
Additional Equipment
--------------------
- None
Ghz