This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 set GPIO direction in u-boot



Hi,

i want set some of the gpio pins as output and also set the value, should this be done before the pinmuxing in 1st stage or should it be done after pinmuxing ?

Thanks & Regards,

mike

  • Mike,

    Please refer to the below links:

    http://processors.wiki.ti.com/index.php/TI81XX_PSP_GPIO_Driver_User_Guide

    http://processors.wiki.ti.com/index.php/TI81XX_PSP_User_Guide#TI814X.2FTI813X

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/383797.aspx

    Best regards,
    Pavel

  • Mike,

    If you want to set the GPIO in u-boot, you can do this after pinmux and with direct programming of the GPIO registers. See DM814x TRM, chapter 10 GPIO.

    See also the below e2e treads:

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/193691.aspx

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/152722.aspx

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/261383.aspx

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/146704.aspx

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/189465.aspx

    Regards,
    Pavel

  • Hi Pavel,

    Thanks for the response.

    For the unused pinmuxes do we need to explicitly pull down ?

    Thanks & Regards

    MIke

  • Mike,

    mike A said:
    For the unused pinmuxes do we need to explicitly pull down ?

    For how to handle unused pins, refer to the DM814x datasheet, section 4.4 Handling Unused Pins

    BR
    Pavel