Using dsplib_2.40 for TMS320C5507 family. Double precision iir32. Does it really work? When I process data with single precision routine works fine, double basically kills the signal entirely. Note, there is significant confusion on coefficient location. Library has one answer, example provided a second answer, source code two additional. I think the library was correct, B2,B1,B0,A2,A1
thanks -emil