This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 video capturing from camera interface



Hi,

I am using a DM8148 custom board in which the camera signals are connected to the CAM_D[0],CAM_D[1],...,CAM_D[7] lines in the processor.

Now I know that the OMX framework can be used for capturing video from VIN[0] or VIN[1] ports.

So, can we use the OMX framework for capturing video from CAM_D[0] interface?

If yes then can you please share some links for that or some documents if available?

Regards,

Debasish