Other Parts Discussed in Thread: TVP7002
Hello.
I need to write raw video frames to the USB mass storage device (DOK) on DM8148-EVM using the latest EXSDK. With standard Linux parameters I see relatively rare the phenomena of USB driver resetting the USB (see below).
To investigate the issue I tried:
1. Setting dirty_bytes=4M and a small application which does ONLY writing to the USB - USB reset happens almost immediately.
2. Setting as advised in e2e the INIT_PRIORITY_1 register of the USB controller to 0x000000F0 to increase the USB priority. This eliminated the USB reset in the test application, BUT:
3. When I added back the input capturing, the USB reset occurs again, just a bit later (about 30s).
Below is the Linux console output of the last case (looks the same each time the USB reset happens):
<15:48:18> vm.overcommit_memory = 2
<15:48:18> vm.overcommit_ratio = 90
<15:48:18> vm.dirty_bytes = 4194304
<15:48:20> Arago Project http://arago-project.org dm814x-evm ttyO0
<15:48:20> Arago 2011.09 dm814x-evm ttyO0
<15:53:05> ./avu0
<15:53:40> OMX_Init completed
<15:53:40> Capture component is created
<15:53:40> Buffer Size computed: 945000
<15:53:40> Set input port params (width = 720, height = 875)
<15:53:40> Enable capture output port
<15:53:40> Capture outport buffers allocated
<15:53:40> Capture is in IDLE state
<15:53:40> Capture state execute
<15:53:41> Control TVP7002 state execute
<15:53:41> File write thread created (RAW)
<15:53:41> Executing the application now!
<15:53:41> ===============================
<15:53:41> SetPrioStat(90)
<15:53:41> OPEN file - /dev/sda2
<15:53:41> FrameLengtht 512000
<15:54:13> usb 1-1: reset high speed USB device using musb-hdrc and address 2
<15:54:28> musb_h_ep0_irq 1159: no URB for end 0
<15:54:28> usb 1-1: device descriptor read/64, error -110
<15:54:44> musb_h_ep0_irq 1159: no URB for end 0
<15:54:44> usb 1-1: device descriptor read/64, error -110
<15:54:44> usb 1-1: reset high speed USB device using musb-hdrc and address 2
<15:54:59> musb_h_ep0_irq 1159: no URB for end 0
<15:54:59> usb 1-1: device descriptor read/64, error -110
<15:55:14> musb_h_ep0_irq 1159: no URB for end 0
<15:55:14> usb 1-1: device descriptor read/64, error -110
<15:55:14> usb 1-1: reset high speed USB device using musb-hdrc and address 2
<15:55:25> usb 1-1: device not accepting address 2, error -110
<15:55:25> usb 1-1: reset high speed USB device using musb-hdrc and address 2
<15:55:35> usb 1-1: device not accepting address 2, error -110
<15:55:35> usb 1-1: USB disconnect, address 2
<15:55:36> sd 1:0:0:0: Device offlined - not ready after error recovery
<15:55:36> sd 1:0:0:0: [sda] Unhandled error code
<15:55:36> sd 1:0:0:0: [sda] Result: hostbyte=0x01 driverbyte=0x00
<15:55:36> sd 1:0:0:0: [sda] CDB: cdb[0]=0x2a: 2a 00 00 20 96 10 00 00 f0 00
<15:55:36> end_request: I/O error, dev sda, sector 2135568
<15:55:36> Buffer I/O error on device sda2, logical block 4770
<15:55:36> lost page write due to I/O error on sda2
<15:55:36> Buffer I/O error on device sda2, logical block 4771
<15:55:36> lost page write due to I/O error on sda2
..........................
Is there any way to solve this issue?
Any hint will be highly appreciated.