Other Parts Discussed in Thread: TMS320DM6437, TVP5146
HI:
I am using a TMS320DM6437 EVM board(DEC6437), which is produced by Arrow-SEED. I want to capture the video input data and display the input video signal on a monitor with VGA interface.
Since the VPBE device driver(vpbe_bios_drv.lib) does not include VGA display mode, I modify the file DDC_vpbeVenc.C as follows:
case PSP_VPBE_DISPLAY_525P_PROGRESSIVE_COMPONENT:
{
LLC_setDisplayStartPosition(vpbeDeviceHandleCVMP->osd[0].OsdRegs,
0x78u,0x26u);
// VPBE_VENC_RGBCTL = 0x00;
LLC_ResetVencReg(vencHandleCVMP->VencRegs);
// VPBE_VENC_ARGBX0 = 1024;
// VPBE_VENC_ARGBX1 = 1404;
// VPBE_VENC_ARGBX2 = 345;
// VPBE_VENC_ARGBX3 = 715;
// VPBE_VENC_ARGBX4 = 1774;
LLC_ResetArgbxReg(vencHandleCVMP->VencRegs);
// VPBE_VENC_VMOD = 0x00002103;
// 0x02
LLC_setDigVideoOutputRGB666_18BIT(vencHandleCVMP->VencRegs);
// 0x01
//LLC_setVencItlcl_262NTSC_312PAL(vencHandleCVMP->VencRegs);
//LLC_setVencNonStandardProgressiveMode(vencHandleCVMP->VencRegs);
LLC_setVideoOutputHDTVMode(vencHandleCVMP->VencRegs);
// 0x00
LLC_setVideoOutputTYP_525p_HDTV(vencHandleCVMP->VencRegs);
LLC_setMasterMode(vencHandleCVMP->VencRegs);
LLC_setVideoTimingNTSCPAL(vencHandleCVMP->VencRegs);
// 0x03
LLC_setEnableBlankMode(vencHandleCVMP->VencRegs);
//LLC_setEnableCompositeOutput(vencHandleCVMP->VencRegs);
//LLC_setVencEnable(vencHandleCVMP->VencRegs);
// VPBE_VENC_VIOCTL = 0x00002000; VIDCTL
LLC_setYCOutputDir(vencHandleCVMP->VencRegs);
//LLC_setVLCKEnable(vencHandleCVMP->VencRegs);
LLC_setEnableVCLKOutputEnable(vencHandleCVMP->VencRegs);
LLC_setEnableVCLKPinOutputEn(vencHandleCVMP->VencRegs);
// VPBE_VENC_VDPRO = 0x00000870;
// 0x08
LLC_setVencFrefilterFreqOne(vencHandleCVMP->VencRegs);
LLC_setVencColorbarType75(vencHandleCVMP->VencRegs);
LLC_setVencColorbarNormal(vencHandleCVMP->VencRegs);
//ColorBar
//LLC_setVencColorbarType100(vencHandleCVMP->VencRegs);
//LLC_setVencColorbarOutput(vencHandleCVMP->VencRegs);
// 0x07
LLC_setVencAtRgbOn(vencHandleCVMP->VencRegs);
LLC_setVencAtYccOn(vencHandleCVMP->VencRegs);
LLC_setVencAtComOn(vencHandleCVMP->VencRegs);
// 0x00
LLC_setVencDacFreq27MHz(vencHandleCVMP->VencRegs);
//LLC_setVencDacFreq54MHz(vencHandleCVMP->VencRegs);
LLC_setVencDaupsOff(vencHandleCVMP->VencRegs);
//LLC_setVencDaupsOn(vencHandleCVMP->VencRegs);
LLC_setVencCupsOff(vencHandleCVMP->VencRegs);
LLC_setVencYupsOff(vencHandleCVMP->VencRegs);
// VPBE_VENC_OSDCLK0 = 0x0;
LLC_setOSDClockControl0(vencHandleCVMP->VencRegs,0u);
// VPBE_VENC_OSDCLK1 = 0x1;
LLC_setOSDClockControl1(vencHandleCVMP->VencRegs,1u);
// Enable DAC A, B and C
// VPBE_VENC_DACTST = 0x00000000;
LLC_setDacANormalMode(vencHandleCVMP->VencRegs);
LLC_setDacBNormalMode(vencHandleCVMP->VencRegs);
LLC_setDacCNormalMode(vencHandleCVMP->VencRegs);
// VPBE_VENC_CMPNT = 0x00008000;
LLC_setRGBModeForComponentOutput(vencHandleCVMP->VencRegs);
//20141123
//LLC_setRGBModeMSYROn(vencHandleCVMP->VencRegs);
//LLC_setRGBModeMSYBOn(vencHandleCVMP->VencRegs);
//LLC_setRGBModeMSYGOn(vencHandleCVMP->VencRegs);
LLC_setRGBModeMSYGOff(vencHandleCVMP->VencRegs);
//LLC_setSyncBuildUpTime100US(vencHandleCVMP->VencRegs);
//LLC_setBlankBuildUpTime150US(vencHandleCVMP->VencRegs);
// VPBE_VENC_DACSEL = 0x00000435;
LLC_setDacAOutVidFormatCompPr(vencHandleCVMP->VencRegs);
LLC_setDacBOutVidFormatCompY(vencHandleCVMP->VencRegs);
LLC_setDacCOutVidFormatCompPb(vencHandleCVMP->VencRegs)
// VPBE_VENC_SYNCCTL = 0x00000003;
LLC_setVencVDOutputEnable(vencHandleCVMP->VencRegs);
LLC_setVencHDOutputEnable(vencHandleCVMP->VencRegs);
// VPBE_VENC_HSTART = 0x0;
//LLC_setVencHorzStartPixel(vencHandleCVMP->VencRegs, 0);
// VPBE_VENC_HVALID = 0x0;
//LLC_setVencHorzValidData(vencHandleCVMP->VencRegs, 0);
// VPBE_VENC_VSTART = 0x0;
//LLC_setVencVertStartPixel(vencHandleCVMP->VencRegs, 0);
// VPBE_VENC_VVALID = 0x0;
//LLC_setVencVertValidData(vencHandleCVMP->VencRegs, 0);
LLC_setEnableCompositeOutput(vencHandleCVMP->VencRegs);
}
break;
Then build the project, and crete a new vpbe_bios_drv.lib.
I use the new VPBE device driver in the loopback project, and modifiy the OSD config parameters and VENC config parameters such as:
static PSP_VPFECcdcConfigParams ccdcParams =
{
//FVID_CCDC_YCBCR_8, /* dataFlow */
FVID_VI_BT656_8BIT,
//FVID_BAYER_PATTERN,
FVID_FRAME_MODE, /* ffMode */
480, // 576, /* height */
720, // 720, /* width */
(720 *2), //(720 *2), /* pitch */
0, /* horzStartPix */
0, /* vertStartPix */
NULL, /* appCallback */
{
PSP_VPFE_TVP5146_Open, /* extVD Fxn */
PSP_VPFE_TVP5146_Close,
PSP_VPFE_TVP5146_Control,
},
0 /*segId */
};
static PSP_VPBEOsdConfigParams vid0Params =
{
//FVID_FRAME_MODE, /* ffmode */
FVID_FIELD_MODE,
FVID_BPP_BITS16, /* bitsPerPixel */
FVID_YCbCr422_INTERLEAVED, /* colorFormat */
(720 * (16/8u)), /* pitch */
0, /* leftMargin */
0, /* topMargin */
720, /* width */
480, /* height */
0, /* segId */
PSP_VPBE_ZOOM_IDENTITY, /* hScaling */
PSP_VPBE_ZOOM_IDENTITY, /* vScaling */
//PSP_VPBE_ZOOM_2X,
PSP_VPBE_EXP_IDENTITY, /* hExpansion */
//PSP_VPBE_EXP_NINE_BY_EIGHT,
PSP_VPBE_EXP_IDENTITY, /* vExpansion */
NULL /* appCallback */
};
static PSP_VPBEVencConfigParams vencParams =
{
// PSP_VPBE_DISPLAY_NTSC_INTERLACED_COMPOSITE
// PSP_VPBE_DISPLAY_PAL_INTERLACED_COMPOSITE
PSP_VPBE_DISPLAY_525P_PROGRESSIVE_COMPONENT
};
Rebuild the project, and debug it with breakpoints.
.......
VPSS_DBG("VPSS :VPSS Loopback Started \r\n");
FVID_allocBuffer(CcdcHandle, &FBAddr);
for(num_frame = 0; num_frame < NumOfIterations; num_frame++)
{
CcdcallocFB[num_frame % NO_OF_BUFFERS] = FBAddr; //Breakpioint 1
if(IOM_COMPLETED != FVID_exchange(CcdcHandle,&FBAddr))
{
VPSS_DBG("VPSS :CCDC Exchange.......FAILED \r\n");
}
//Histogram(FBAddr->frame.iFrm.y1);
VidallocFB[num_frame % NO_OF_BUFFERS] = FBAddr; //Breakpioint 2
if(IOM_COMPLETED != FVID_exchange(Vid0Handle,&FBAddr))
{
VPSS_DBG("VPSS :Video -0 Exchange.......FAILED \r\n");
}
}
......
The trace window shows the message "VPSS :Video -0 Exchange.......FAILED", and the displayed image is shown bellow:

There are two questions:
1. The Image was splited in two half from both sides, how can I setup the OSD and VENC parameters to solve the problem?
2. FVID_exchange(Vid0Handle,&FBAddr) did not execute normally, why? How can I do?
When using NTSC_INTERLACED_COMPOSIT mode, the captured data was displayed on the monitor with composite interface correctly. That means the function
"FVID_exchange(Vid0Handle,&FBAddr)" is ok.
When I modify the VPBE_VENC_VDPRO register, the monitor can display ColorBar image on VGA monitor. that is to say VENC paramters are right, right?
When the VPBE works in FVID_FRAME_MODE, the displayed image is as follows:
Thank you for your consideration.