Other Parts Discussed in Thread: AM5728
Hi,
Im working in AM5728 Processor...
Im booting the board through SD card.
1-> The u-boot is booting and it is passing the control to the kernel.
2-> The kernel is not booting up and it is stuck at 'Starting Kernel....'
3-> This is strengthened by placing printfs statement after "Starting kernel ..." in the u-boot. The printf statements in the u-boot are printed till the control is passed to the kernel i.e till the statement 'kernel_entry(0,machid,r2)'(statement inside the u-boot ).
Pls kindly reply..
Regards,
Siva