Hello,
I have Spectrum Digital VAYU EVM(X5777) with 10.1' touch display. I tried to boot it with GLSDK 6.10.00.02.
But it stuck at the following point and I am not getting prompt after it.
[ 12.469083] Waiting for root device /dev/mmcblk1p2...
[ 12.507146] (stk) : timed out waiting for ldisc to be un-installed
[ 12.619983] (stk) :ldisc_install = 1(stk) :ldisc installation timeout
[ 13.615003] (stk) :ldisc_install = 0(stk) : timed out waiting for ldisc to be un-installed
[ 14.718750] (stk) :ldisc_install = 1(stk) :ldisc installation timeout
[ 15.715141] (stk) :ldisc_install = 0(stk) : timed out waiting for ldisc to be un-installed
[ 16.818917] (stk) :ldisc_install = 1(stk) :ldisc installation timeout
[ 17.815370] (stk) :ldisc_install = 0(stk) : timed out waiting for ldisc to be un-installed
[ 18.919056] (stk) :ldisc_install = 1(stk) :ldisc installation timeout
[ 19.915420] (stk) :ldisc_install = 0(stk) : timed out waiting for ldisc to be un-installed
[ 21.019172] (stk) :ldisc_install = 1(stk) :ldisc installation timeout
[ 22.015560] (stk) :ldisc_install = 0(stk) : timed out waiting for ldisc to be un-installed
[ 23.014807] Bluetooth: st_register failed -22
[ 70.654539] remoteproc0: failed to load dra7-dsp1-fw.xe66
[ 70.660361] remoteproc1: failed to load dra7-ipu2-fw.xem4
[ 70.666464] remoteproc2: failed to load dra7-dsp2-fw.xe66
[ 70.672281] remoteproc3: failed to load dra7-ipu1-fw.xem4
Please help on this.
I have attached full log of booting.7652.log.txt