Other Parts Discussed in Thread: DM385
Hi,
i have a Problem which was found during a Long time test.
I use the DVR RDK 04.00.00.04 with a DM385 Video Processor. The Long term Test was just start and stop the Video chain in a Loop which creates the links and deletes the links on stop. After ~900 cycles, the System Asserts with the following message. It is always after 900 cytles plus minus 10 cycles.
ASSERT (system_ipc_listMP.c|System_ipcListMPAllocListElemMem|213)
There is a Alloc_Memory function in that file which return just NULL which cause the Assertion.
Is there a bug in the DVR RDK or is there anybody who have the same issue? How can I debug that.
System log:
[ 1806.300151][ASC ] #CMD## is "VIDEO.stop"
[ 1806.300296][ASC ] Do command 'VIDEO.stop' array_index=0 E
[ 1806.300325][ASC ] ASC_stop
[ 1806.300344][ASC ] Stopping Audio Encoder
[ 1806.300362][ASC ] Stopping Threads
[ 1806.300376][ASC ] Stopping Links
[host] 1799255: IPC_BITS_IN : Stop Done !!!
[ 1806.305495][ASC ] Destryoing Semaphore
[ 1806.305515][ASC ] Destroying Links
[host] 1799255: IPCBITSIN:Link[3000001a]:
[host] RECV:6 FREE:0,DROPPED:0,AVGLATENCY:0,AVG_APP_CB_TIME:0
[host] 1799255: IPC_BITS_IN : Delete in progress !!!
[host] 1799256: IPC_BITS_IN : Delete Done !!!
[ 1806.315939][ASC ] System Deinint
1799265: SYSTEM: System Common De-Init in progress !!!
[host] OSA_tskDelete:In progress...
[host] OSA_tskDelete:In progress...
[host] OSA_tskDelete:In progress...
[host] OSA_tskDelete:In progress
[host] OSA_tskDelete:In progress
[host] OSA_tskDelete:In progress...
[host] OSA_tskDelete:In progress...
[host] OSA_tskDelete:In progress
[host] OSA_tskDelete:In progress
[host] OSA_tskDelete:In progress
1799271: SYSTEM: IPC de-init in progress !!!
1799277: SYSTEM: IPC de-init DONE !!!
1799277: SYSTEM: System Common De-Init Done !!!
[ 1809.310160][ASC ] #CMD## is "VIDEO.start"
[ 1809.310295][ASC ] Do command 'VIDEO.start' array_index=0 E
[ 1809.310394][ASC ] ASC_start
[ 1809.310419][ASC ] Set FPGA Video Mode
[ 1809.310436][ASC ] ---I: ASC_start: video format is:1280x720p60
[ 1809.310624][ASC ] captureID =0x20000021
[ 1809.310640][ASC ] nsfID =0x20000022
[ 1809.310656][ASC ] deiID =0x00000000
[ 1809.310671][ASC ] sclrID =0x20000034
[ 1809.310686][ASC ] ipcOutVpssId =0x20000000
[ 1809.310702][ASC ] ipcInVideoId =0x10000002
[ 1809.310717][ASC ] encId =0x10000021
[ 1809.310732][ASC ] ipcBitsOutVideoId=0x10000018
[ 1809.310748][ASC ] ipcBitsInHostId =0x3000001a
[ 1809.310763][ASC ] System Init
1802260: SYSTEM: System Common Init in progress !!!
1802260: SYSTEM: IPC init in progress !!!
1802270: SYSTEM: CPU [DSP] is NOT available on this platform !!!
1802270: SYSTEM: CPU [VIDEO-M3] syslink proc ID is [0] !!!
1802270: SYSTEM: CPU [VPSS-M3] syslink proc ID is [1] !!!
1802270: SYSTEM: CPU [HOST] syslink proc ID is [2] !!!
1802270: SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP_3] ...
1802274: SYSTEM: Creating MsgQ [HOST_MSGQ] ...
1802277: SYSTEM: Creating MsgQ [HOST_ACK_MSGQ] ...
1802279: SYSTEM: Opening MsgQ [VIDEO-M3_MSGQ] ...
1802280: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ...
1802281: SYSTEM: Notify register to [VIDEO-M3] line 0, event 15 ...
1802282: SYSTEM: Notify register to [VPSS-M3] line 0, event 15 ...
1802283: SYSTEM: IPC init DONE !!!
1802285: SYSTEM: Creating ListMP [HOST_IPC_OUT_24] in region 0 ...
1802288: SYSTEM: Creating ListMP [HOST_IPC_IN_24] in region 0 ...
1802290: SYSTEM: ListElem Shared Addr = 0x42761a80
1802292: SYSTEM: Creating ListMP [HOST_IPC_OUT_25] in region 0 ...
1802295: SYSTEM: Creating ListMP [HOST_IPC_IN_25] in region 0 ...
1802298: SYSTEM: ListElem Shared Addr = 0x427a3880
1802300: SYSTEM: Creating ListMP [HOST_IPC_OUT_19] in region 0 ...
1802303: SYSTEM: Creating ListMP [HOST_IPC_IN_19] in region 0 ...
1802306: SYSTEM: ListElem Shared Addr = 0x42828f00
1802307: SYSTEM: Creating ListMP [HOST_IPC_OUT_20] in region 0 ...
1802311: SYSTEM: Creating ListMP [HOST_IPC_IN_20] in region 0 ...
1802313: SYSTEM: ListElem Shared Addr = 0x4286bc00
1802315: SYSTEM: Creating ListMP [HOST_IPC_OUT_21] in region 0 ...
1802318: SYSTEM: Creating ListMP [HOST_IPC_IN_21] in region 0 ...
ASSERT (system_ipc_listMP.c|System_ipcListMPAllocListElemMem|213)
Regards
Andy