HI, everyone,
I see in Swpu249ab page 1070 and page 1076 that:
Four instructions per cycle, four execution units:
– Optimized instruction set for video and image processing
– Four 8 x 8 or 16 x 16 multiply accumulate (MAC) per cycle
– Four slave synchronous die (SAD) per cycle
– Eight interpolations (a + b + 1) >> 1 per cycle
– Two (32-bit x 32-bit -> 64-bit) multiply operations per cycle
As far as I know about C64x+, two 32x32->64/cycle requires 2 .M units.
Eight (a+b+1)>>1/cycle also requires 2 .M units running AVGU4 at the same time.
Is this implying that the IVA-HD, or IVA3 core has at least 2 .M units? If this is the case, what are the other two units available?
Thank you.
Dehuan