Is there an alternate signal from the am335x CPU that can be monitored that would coincide with "PORZ" to logic "1"
Is there any special timing to consider for powering up the CPU with the TPS65910 PMU?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Don,
You can check Figure 8-19 in the AM335X TRM Rev. K. nRESETIN_OUT goes high after a determined time, and CLKOUT1 (if SYSBOOT5 = 1) starts outputting the main oscillator frequency with approx. 1 clock cycle delay.
About the TPS65910A PMIC, there are no special considerations required. It's designed to provide all the necessary timings. See http://www.ti.com/lit/ug/swcu093c/swcu093c.pdf