Hi,
I got some errors when I built the IPC example.
EVM: TCI66AK2H12
Example code: /mcsdk_3_01_01_04/ipc_3_22_02_11/examples/C6678_bios_elf/ex11_ping.zip
I followed up the readme.txt file, and the configurations are:
BIOS_INSTALL_DIR = /mnt/sdb2/opt/ti/bios_6_41_00_26
IPC_INSTALL_DIR = /mnt/sdb2/opt/ti/mcsdk_3_01_00_03/ipc_3_22_02_11
XDC_INSTALL_DIR = /mnt/sdb2/opt/ti/individual_libs/xdctools_3_30_04_52_core
ti.targets.elf.C66 = /opt/ti/ccsv6/tools/compiler/c6000_7.4.8
I got some errors when I make it, the errors are:
undefined first referenced
symbol in file
--------- ----------------
ti_sdo_ipc_gates_GateHWSem_query__E /ping/core0/bin/debug/configuro/package/cfg/Core0_pe66.oe66
ti_sdo_ipc_gates_GateMPSupportNull_query__E /ping/core0/bin/debug/configuro/package/cfg/Core0_pe66.oe66
ti_sdo_ipc_heaps_HeapMemMP_isBlocking__E /ping/core0/bin/debug/configuro/package/cfg/Core0_pe66.oe66
Can you help me to solve this problem?
Thanks!