Dear TI E2E Community,
I am using uboot 2014.07 from ftp://ftp.denx.de/pub/u-boot/u-boot-2014.07.tar.bz2 instead of u-boot-2013.10-ti2013.12.01 which is part of ti sdk 7, am using this because the verified boot feature is not supported in u-boot-2013.10-ti2013.12.01 & moreover ti sdk 7 kernel & rootfs is coming up with this uboot 2014.07
Could you please let me know whether all the u-boot-2013.10-ti2013.12.01 BSP support features for Beaglebone black that exists in u-boot-2013.10-ti2013.12.01 also exists in u-boot-2014.07(since this is mainline version) or is there any feature that is being missed in u-boot-2014.07 (for beaglebone black) that needs to be ported to 2014.07 from u-boot-2013.10-ti2013.12.01
Could anybody please confirm on this, as I need to finalize which version of uboot to be used
Kindly do the needful as early as possible
Awaiting for your replies,
Many Thanks in advance