This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

External Memory Read out problem

Hi;

I am using xds100 to extart image from Micron Pre-programmed Flash memory (part# MT29F2G16ABAEAWP:E) using JTAG and facing the following issues. 

  • The current JTAG is using a TI flash programming utility (Nandflashwriter.out) to program but do not provide any read back option for flash read.
  • The CCS debugger provide options for memory read but we are not sure on it , is it for RAM or for flash ?

Please help on this.....................

  • Sumeet,

    From what I understand, you want to access NAND flash chip (MT29F2G16ABAEAWP:E) through XDS100 JTAG and CCS, on DM816x board, is that correct?

    BR
    Pavel

  • Hi Pavel;

    Yes you are correct; Please help to solve this problem.

    Thanks & Regards

    Sumeet Kumar

  • Sumeet,

    Let we first check that your XDS100 JTAG emulator is working fine with your DM816x board.

    I have USB560M JTAG Blackhawk emulator, and I test it like below:

    Create your target configuration, for connection put your JTAG emulator, for board/devcie put EVMDM8168 if you are using TI EVM or DM8168 if you are using custom board. Then click the "Test connection" button.

    You should power on the JTAG emulator and the board, and if connection is fine, you should have something like below:

    [Start: Blackhawk USB560-M Emulator, 20-pin JTAG Cable_0]

    Execute the command:

    %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

    [Result]


    -----[Print the board config pathname(s)]------------------------------------

    /home/users/pbotev/.ti/ti/0/0/BrdDat/testBoard.dat

    -----[Print the reset-command software log-file]-----------------------------

    This utility has selected a 560/2xx-class product.
    This utility will load the program 'bh560usbm.out'.
    The library build date was 'May 21 2014'.
    The library build time was '17:30:09'.
    The library package version is '5.1.507.0'.
    The library component version is '35.34.40.0'.
    The controller does use a programmable FPGA.
    The old VHDL code has a version number of '0' (0x00000000).
    The new VHDL code has a version number of '386336272' (0x17070610).
    The controller has a version number of '6' (0x00000006).
    The controller has an insertion length of '0' (0x00000000).
    The cable+pod has a version number of '6' (0x00000006).
    The cable+pod has a capability number of '1' (0x00000001).
    This utility will attempt to reset the controller.
    This utility has successfully reset the controller.

    -----[Print the reset-command hardware log-file]-----------------------------

    The scan-path will be reset by toggling the JTAG TRST signal.
    The controller is the Nano-TBC VHDL.
    The link is a 560-class version-D multi-purpose cable.
    The software is configured for Nano-TBC VHDL features.
    The controller will be software reset via its registers.
    The controller has a logic ONE on its EMU[0] input pin.
    The controller has a logic ONE on its EMU[1] input pin.
    The controller will use falling-edge timing on output pins.
    The controller cannot control the timing on input pins.
    The scan-path link-delay has been set to exactly '2' (0x0002).
    The utility logic has not previously detected a power-loss.
    The utility logic is not currently detecting a power-loss.

    -----[The log-file for the JTAG TCLK output generated from the PLL]----------

      Test  Size   Coord      MHz    Flag  Result       Description
      ~~~~  ~~~~  ~~~~~~~  ~~~~~~~~  ~~~~  ~~~~~~~~~~~  ~~~~~~~~~~~~~~~~~~~
        1   none  - 01 00  500.0kHz   -    similar      isit internal clock
        2   none  - 01 09  570.3kHz   -    similar      isit internal clock
        3    512  - 01 00  500.0kHz   O    good value   measure path length
        4    128  - 01 00  500.0kHz   O    good value   auto step initial
        5    128  - 01 0D  601.6kHz   O    good value   auto step delta
        6    128  - 01 1C  718.8kHz   O    good value   auto step delta
        7    128  - 01 2E  859.4kHz   O    good value   auto step delta
        8    128  + 00 02  1.031MHz   O    good value   auto step delta
        9    128  + 00 0F  1.234MHz   O    good value   auto step delta
       10    128  + 00 1F  1.484MHz   O    good value   auto step delta
       11    128  + 00 32  1.781MHz   O    good value   auto step delta
       12    128  + 01 04  2.125MHz   O    good value   auto step delta
       13    128  + 01 11  2.531MHz   O    good value   auto step delta
       14    128  + 01 21  3.031MHz   O    good value   auto step delta
       15    128  + 01 34  3.625MHz   O    good value   auto step delta
       16    128  + 02 05  4.312MHz   O    good value   auto step delta
       17    128  + 02 13  5.188MHz   O    good value   auto step delta
       18    128  + 02 23  6.188MHz   O    good value   auto step delta
       19    128  + 02 37  7.438MHz   O    good value   auto step delta
       20    128  + 03 07  8.875MHz   O    good value   auto step delta
       21    128  + 03 15  10.62MHz   O    good value   auto step delta
       22    128  + 03 1E  11.75MHz  {O}   good value   auto step delta
       23    512  + 02 3E  7.875MHz   O    good value   auto power initial
       24    512  + 03 0E  9.750MHz   O    good value   auto power delta
       25    512  + 03 16  10.75MHz   O    good value   auto power delta
       26    512  + 03 1A  11.25MHz   O    good value   auto power delta
       27    512  + 03 1C  11.50MHz   O    good value   auto power delta
       28    512  + 03 1D  11.62MHz   O    good value   auto power delta
       29    512  + 03 1D  11.62MHz   O    good value   auto power delta
       30    512  + 03 13  10.38MHz  {O}   good value   auto margin initial

    The first internal/external clock test resuts are:
    The expect frequency was 500000Hz.
    The actual frequency was 499872Hz.
    The delta frequency was 128Hz.

    The second internal/external clock test resuts are:
    The expect frequency was 570312Hz.
    The actual frequency was 569976Hz.
    The delta frequency was 336Hz.

    In the scan-path tests:
    The test length was 16384 bits.
    The JTAG IR length was 6 bits.
    The JTAG DR length was 1 bits.

    The IR/DR scan-path tests used 30 frequencies.
    The IR/DR scan-path tests used 500.0kHz as the initial frequency.
    The IR/DR scan-path tests used 11.75MHz as the highest frequency.
    The IR/DR scan-path tests used 10.38MHz as the final frequency.

    -----[Measure the source and frequency of the final JTAG TCLKR input]--------

    The frequency of the JTAG TCLKR input is measured as 10.37MHz.

    The frequency of the JTAG TCLKR input and TCLKO output signals are similar.
    The target system likely uses the TCLKO output from the emulator PLL.

    -----[Perform the standard path-length test on the JTAG IR and DR]-----------

    This path-length test uses blocks of 512 32-bit words.

    The test for the JTAG IR instruction path-length succeeded.
    The JTAG IR instruction path-length is 6 bits.

    The test for the JTAG DR bypass path-length succeeded.
    The JTAG DR bypass path-length is 1 bits.

    -----[Perform the Integrity scan-test on the JTAG IR]------------------------

    This test will use blocks of 512 32-bit words.
    This test will be applied just once.

    Do a test using 0xFFFFFFFF.
    Scan tests: 1, skipped: 0, failed: 0
    Do a test using 0x00000000.
    Scan tests: 2, skipped: 0, failed: 0
    Do a test using 0xFE03E0E2.
    Scan tests: 3, skipped: 0, failed: 0
    Do a test using 0x01FC1F1D.
    Scan tests: 4, skipped: 0, failed: 0
    Do a test using 0x5533CCAA.
    Scan tests: 5, skipped: 0, failed: 0
    Do a test using 0xAACC3355.
    Scan tests: 6, skipped: 0, failed: 0
    All of the values were scanned correctly.

    The JTAG IR Integrity scan-test has succeeded.

    -----[Perform the Integrity scan-test on the JTAG DR]------------------------

    This test will use blocks of 512 32-bit words.
    This test will be applied just once.

    Do a test using 0xFFFFFFFF.
    Scan tests: 1, skipped: 0, failed: 0
    Do a test using 0x00000000.
    Scan tests: 2, skipped: 0, failed: 0
    Do a test using 0xFE03E0E2.
    Scan tests: 3, skipped: 0, failed: 0
    Do a test using 0x01FC1F1D.
    Scan tests: 4, skipped: 0, failed: 0
    Do a test using 0x5533CCAA.
    Scan tests: 5, skipped: 0, failed: 0
    Do a test using 0xAACC3355.
    Scan tests: 6, skipped: 0, failed: 0
    All of the values were scanned correctly.

    The JTAG DR Integrity scan-test has succeeded.

    [End: Blackhawk USB560-M Emulator, 20-pin JTAG Cable_0]

  • Hi Pavel;

    Thanks for your reply.

    The XDS560 is faster but comparatively much costlier (approx. 10x) than the XDS100V2.

     We already able to setup the environment with XDS100V2 emulator but the problem is how to read the image from on board flash in desirable format.

    Please help to solve the problem.

    Thanks & Regards

    Sumeet Kumar

  • Sumeet,

    Sumeet Kumar1 said:
    We already able to setup the environment with XDS100V2 emulator but the problem is how to read the image from on board flash in desirable format.

    Please refer to the NAND flash SW test from Spectrum Digital for reference:

    http://support.spectrumdigital.com/boards/evm816x/revg/

    Test Code -> evm816x -> tests -> nandflash

    Also the NAND flash writer might be in help:

    http://processors.wiki.ti.com/index.php/TI81XX_PSP_UBOOT_User_Guide#Flashing_U-Boot_using_CCS

    http://processors.wiki.ti.com/index.php/TI81XX_PSP_Flashing_Tools_Guide#Burning_images_to_NAND_Flash_.28using_CCS.29

    Regards,
    Pavel