This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HeapBufMP_open failed



I meet a problem when run the messageQ module.I use the  MessageQ example in the IPC module as a reference.The difference is that I create two projects,that is  different exectuable (*.out)  files run on different cores.

in my project, core0 send message Q to core1.Some code is below:

the SharedRegion has been modified in the .cfg file.

core0 task:

{

·······························

HeapBufMP_Params_init(&heapBufParams);
heapBufParams.regionId = 0;
heapBufParams.name = HEAP_NAME;
heapBufParams.numBlocks = 1;
heapBufParams.blockSize = sizeof(MessageQ_MsgHeader);
heapHandle = HeapBufMP_create(&heapBufParams);


/* Register this heap with MessageQ */
MessageQ_registerHeap((IHeap_Handle)heapHandle, HEAPID);

·····················

}

core1 task:

{

··············

do
{
status = HeapBufMP_open(HEAP_NAME, &heapHandle);
} while (status < 0);

``````````````````

}

the problem is that core1 can't open the heap, I want to ask what should I notice before I call the HeapBufMP_open()?

Is there anything I should do to make sure the function runs properly?

Thank you very much!

  • Jane,

    Your code above looks correct. But there are several other factors which could be causing your failure. Let's start with product versions. Would you list the device and software components you are using.

    Also, which IPC example are you trying out? Does the example work if you don't modify it?

    ~Ramsey

  • Hi Ramsey,I have solved the question.the problem is that the ShareRigion defined in the two cores are different.After all,thank you very much for answering!