Other Parts Discussed in Thread: DM385
hello TI-friends,
we try to use DVRRDK4.1( from DM816X) on DM385, but we didn't success to do that.
May I know is it possible to use the composition?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DM385
hello TI-friends,
we try to use DVRRDK4.1( from DM816X) on DM385, but we didn't success to do that.
May I know is it possible to use the composition?
It is supported on TI8107.
You could use IPNC-RDK on DM385.
Regards,
brijesh
hello Brijesh,
Many thanks for your reply.
I try to use the pre-built binary inside DVR-RDK4.1 and boot up with NFS environment.and follow steps in DM81xx_DVR_RDK_Install_Guide.pdf.
But I can't see any video in the HDMI output.
Attach is my boot log. Please help to clarify the issue on output. Thanks.
U-Boot 2010.06 (Jun 23 2014 - 17:42:07)
TI813X-GP rev 1.0
L3 clk : 240MHz
IVA clk : 390MHz
ISS clk : 480MHz
DSS clk : 240MHz
ARM clk : 720MHz
DDR clk : 533MHz
------------ PLL Settings --------------
OSC_0_FREQ : 20MHz
MODENA_N : 1
MODENA_M : 72
MODENA_M2 : 1
L3_N : 19
L3_M : 960
L3_M2 : 4
DSP_N : 19
DSP_M : 750
DSP_M2 : 1
DSS_N : 19
DSS_M : 960
DSS_M2 : 4
IVA_N : 19
IVA_M : 780
IVA_M2 : 2
ISS_N : 19
ISS_M : 960
ISS_M2 : 2
USB_N : 19
USB_M : 960
USB_M2 : 5
DCO_HS2_MIN : 500
DCO_HS2_MAX : 1000
DCO_HS1_MIN : 1000
DCO_HS1_MAX : 2000
SELFREQDCO_HS2 : 2049
SELFREQDCO_HS1 : 4097
--------- DDR PLL ----------
DDR_N : 0x13
DDR_M : 0x42A
DDR_M2 : 0x2
----------EMIF Timings (identical for 0 & 1)-------
DDR3_EMIF_READ_LATENCY : 0x170209
DDR3_EMIF_TIM1 : 0x132BB953
DDR3_EMIF_TIM2 : 0x20437FDA
DDR3_EMIF_TIM3 : 0x501F87FF
DDR3_EMIF_REF_CTRL : 0xC30
DDR3_EMIF_SDRAM_CONFIG : 0x61C11B32
DDR3_EMIF_SDRAM_ZQCR : 0x50074BE1
----------SW LEVEL Info (EMIF 0) -------
DDR3_PHY_RD_DQS_CS0_BYTE0: 0x00000041
DDR3_PHY_RD_DQS_CS0_BYTE1: 0x00000038
DDR3_PHY_RD_DQS_CS0_BYTE2: 0x00000046
DDR3_PHY_RD_DQS_CS0_BYTE3: 0x00000037
DDR3_PHY_WR_DQS_CS0_BYTE0: 0x00000039
DDR3_PHY_WR_DQS_CS0_BYTE1: 0x0000003F
DDR3_PHY_WR_DQS_CS0_BYTE2: 0x00000046
DDR3_PHY_WR_DQS_CS0_BYTE3: 0x00000045
DDR3_PHY_RD_DQS_GATE_CS0_BYTE0: 0x000000BD
DDR3_PHY_RD_DQS_GATE_CS0_BYTE1: 0x000000E0
DDR3_PHY_RD_DQS_GATE_CS0_BYTE2: 0x00000105
DDR3_PHY_RD_DQS_GATE_CS0_BYTE3: 0x0000012B
DDR3_PHY_WR_DATA_CS0_BYTE0: 0x0000007C
DDR3_PHY_WR_DATA_CS0_BYTE1: 0x00000073
DDR3_PHY_WR_DATA_CS0_BYTE2: 0x00000078
DDR3_PHY_WR_DATA_CS0_BYTE3: 0x0000006D
----------SW LEVEL Info (EMIF 1) -------
DDR3_PHY_RD_DQS_CS0_BYTE0: 0x00000041
DDR3_PHY_RD_DQS_CS0_BYTE1: 0x00000038
DDR3_PHY_RD_DQS_CS0_BYTE2: 0x00000046
DDR3_PHY_RD_DQS_CS0_BYTE3: 0x00000037
DDR3_PHY_WR_DQS_CS0_BYTE0: 0x00000039
DDR3_PHY_WR_DQS_CS0_BYTE1: 0x0000003F
DDR3_PHY_WR_DQS_CS0_BYTE2: 0x00000046
DDR3_PHY_WR_DQS_CS0_BYTE3: 0x00000045
DDR3_PHY_RD_DQS_GATE_CS0_BYTE0: 0x000000BD
DDR3_PHY_RD_DQS_GATE_CS0_BYTE1: 0x000000E0
DDR3_PHY_RD_DQS_GATE_CS0_BYTE2: 0x00000105
DDR3_PHY_RD_DQS_GATE_CS0_BYTE3: 0x0000012B
DDR3_PHY_WR_DATA_CS0_BYTE0: 0x0000007C
DDR3_PHY_WR_DATA_CS0_BYTE1: 0x00000073
DDR3_PHY_WR_DATA_CS0_BYTE2: 0x00000078
DDR3_PHY_WR_DATA_CS0_BYTE3: 0x0000006D
I2C: ready
DRAM: 1 GiB
NAND: HW ECC BCH8 Selected
256 MiB
MMC: OMAP SD/MMC: 0
Card did not respond to voltage select!
MMC init failed
@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
@@ @@
@@ @@
@@ @@
@@ @@
@@ @@@ @. @. @@@@ @@ @@@@@ @@@@@@@@@ @@
@@ @@@@@ L@@ @@@ @@@@@i @@@@ @@ @@ @@ @@ @@
@@ @@ @@@. @@@ @@@ @, @@ @@ @@ @@ @@ @@
@@ @@ @@ @@@ @@@ @@;@@: @@ @@ @@ @@ @@
@@ @@ @@ @@@.l@L@ ,@@@@ @@ @@ @@ @@ @@
@@ @@ @@ l@ @@@@ @. @@ L@@ @@ @@ @@ @@ @@
@@ @@ @@ @@ @@@@ @@ C@ @@ @@ @@ @@ @@ @@
@@ @@ ,@C @@ @@@ @@ C@ @@ @@ @@ @@ @@ @@
@@ @@@@@@@ @@ @@ @@ @@@@@@ @@ @@ @@ @@ @@
@@ @@@@@ @ @ @ @@@, @@@@ @@@@@ @@ @@
@@ @@
@@ @@
@@ @@
@@ @@
@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
Net: Ethernet clocking: 0x0
<ethaddr> not set. Reading from E-fuse
Detected MACID:8:0:28:32:7a:46
cpsw
TI813X_EVM#setenv ethaddr 30:38:3a:30:30:3a; setenv nfsserver 192.168.107.86; setenv serverip 192.168.107.86 ;setenv ipaddr 192.168.107.167 ; setenv gatewayip 192.168.107.254; setenv netmask 255.255.255.0;
TI813X_EVM#setenv bootcmd 'i2c mw 0x2d 0x24 0x3f 1;i2c mw 0x2d 0x25 0x3f 1;i2c mw 0x2d 0x26 0x3f 1; tftp 81000000 uImage_810x;bootm'
TI813X_EVM#setenv bootargs 'console=ttyO0,115200n8 root=/dev/nfs nfsroot=192.168.107.86:/home/medwin/Projects/TI-8168/DVRRDK_04.01.00.xx/DVRRDK_04.01.00.02/target/rfs_810x,nolock rw mem=128M ip=192.168.107.167:192.168.107.86:192.168.107.254:255.255.255.0::eth0:off notifyk.vpssm3_sva=0xbffd0000 i2c_bus=3,400 ddr_mem=512M vram=3M'
TI813X_EVM#boot
link up on port 0, speed 100, full duplex
Using cpsw device
TFTP from server 192.168.107.86; our IP address is 192.168.107.167
Filename 'uImage_810x'.
Load address: 0x81000000
Loading: #################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
####################
done
Bytes transferred = 2761904 (0x2a24b0)
## Booting kernel from Legacy Image at 81000000 ...
Image Name: Linux-2.6.37
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2761840 Bytes = 2.6 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37 (dm8168@ubuntu) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #1 Mon Jun 23 17:57:34 CST 2014
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: dm385evm
vram size = 3145728 at 0x0
ti81xx_reserve: ### Reserved DDR region @87f00000
reserved size = 3145728 at 0x0
FB: Reserving 4194304 bytes SDRAM for VRAM
Memory policy: ECC disabled, Data cache writeback
OMAP chip is DM385 1.0
SRAM: Mapped pa 0x402f1000 to va 0xfe400000 size: 0xf000
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 31232
Kernel command line: console=ttyO0,115200n8 root=/dev/nfs nfsroot=192.168.107.86:/home/medwin/Projects/TI-8168/DVRRDK_04.01.00.xx/DVRRDK_04.01.00.02/target/rfs_810x,nolock rw mem=128M ip=192.168.107.167:192.168.107.86:192.168.107.254:255.255.255.0::eth0:off notifyk.vpssm3_sva=0xbffd0000 i2c_bus=3,400 ddr_mem=512M vram=3M
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 122MB 1MB = 123MB total
Memory: 118840k/118840k available, 12232k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
vmalloc : 0xc8800000 - 0xf8000000 ( 760 MB)
lowmem : 0xc0000000 - 0xc8000000 ( 128 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.init : 0xc0008000 - 0xc0041000 ( 228 kB)
.text : 0xc0041000 - 0xc053b000 (5096 kB)
.data : 0xc053c000 - 0xc0591f80 ( 344 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:407
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
GPMC revision 6.0
Trying to install interrupt handler for IRQ400
Trying to install interrupt handler for IRQ401
Trying to install interrupt handler for IRQ402
Trying to install interrupt handler for IRQ403
Trying to install interrupt handler for IRQ404
Trying to install interrupt handler for IRQ405
Trying to install interrupt handler for IRQ406
Trying to install type control for IRQ407
Trying to set irq flags for IRQ407
OMAP clockevent source: GPTIMER1 at 20000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 719.25 BogoMIPS (lpj=3596288)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
TI81XX: Map 0x87f00000 to 0xfe500000 for dram barrier
TI81XX: Map 0x40300000 to 0xfe600000 for sram barrier
omap_voltage_early_init: voltage driver support not added
regulator: core version 0.5
regulator: dummy:
NET: Registered protocol family 16
omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting!
omap_voltage_add_dev: VDD specified does not exist!
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
omap_mux_init: Add partition: #1: core, flags: 4
NOR: Can't request GPMC CS
clk get on i2c3 fck failed
Cannot clk_get ck_32
Debugfs: Only enabling/disabling deep sleep and wakeup timer is supported now
registered ti81xx_vpss device
registered ti81xx_vidout device
registered ti81xx on-chip HDMI device
registered ti81xx_fb device
registered ti81xx_vin device
NSS Crypto DMA hardware revision 1.9 @ IRQ 116
ti81xx_pcie: Invoking PCI BIOS...
ti81xx_pcie: Setting up Host Controller...
ti81xx_pcie: Register base mapped @0xc8830000
ti81xx_pcie: forcing link width - x1
ti81xx_pcie: Starting PCI scan...
PCI: bus0: Fast back to back transfers enabled
ti81xx_pcie: PCI scan done.
bio: create slab <bio-0> at 0
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
USBSS revision 4ea2080b
registerd cppi-dma Intr @ IRQ 17
Cppi41 Init Done
omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
regulator: VRTC: 1800 mV
regulator: VIO: 1500 mV
regulator: VDD1: 600 <--> 1500 mV at 1200 mV
regulator: VDD2: 600 <--> 1500 mV at 1350 mV
regulator: VDDCTRL: 600 <--> 1400 mV at 1200 mV
regulator: LDO1: 1100 <--> 3300 mV at 1800 mV
regulator: LDO2: 1100 <--> 3300 mV at 1800 mV
regulator: LDO3: 1100 <--> 3300 mV at 3300 mV
regulator: LDO4: 1100 <--> 3300 mV at 1800 mV
regulator: LDO5: 1100 <--> 3300 mV at 3300 mV
regulator: LDO6: 1100 <--> 3300 mV at 3300 mV
regulator: LDO7: 1100 <--> 3300 mV at 3300 mV
regulator: LDO8: 1100 <--> 3300 mV at 1800 mV
tps65910 1-002d: No interrupt support, no core IRQ
omap_i2c omap_i2c.3: bus 3 rev4.0 at 400 kHz
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource gp timer
musb-hdrc: version 6.0, host, debug=0
musb-hdrc musb-hdrc.0: dma type: dma-cppi41
MUSB controller-0 revision 4ea20800
usb2phy: computed values rxcalib(15)DACs(25 13 14)
usb2phy: override computed values rxcalib(15)DACs(25 13 14)
usb2phy_config: musb(0) rxcalib done, rxcalib read value 6f6cdb76
musb-hdrc musb-hdrc.0: MUSB HDRC host driver
musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: MUSB HDRC host driver
usb usb1: Manufacturer: Linux 2.6.37 musb-hcd
usb usb1: SerialNumber: musb-hdrc.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
musb-hdrc musb-hdrc.0: USB Host mode controller at c881e000 using DMA, IRQ 18
musb-hdrc musb-hdrc.1: dma type: dma-cppi41
MUSB controller-1 revision 4ea20800
usb2phy: computed values rxcalib(15)DACs(30 13 15)
usb2phy: override computed values rxcalib(15)DACs(30 13 15)
usb2phy_config: musb(1) rxcalib done, rxcalib read value 6f6f5b7e
musb-hdrc musb-hdrc.1: MUSB HDRC host driver
musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: MUSB HDRC host driver
usb usb2: Manufacturer: Linux 2.6.37 musb-hcd
usb usb2: SerialNumber: musb-hdrc.1
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
musb-hdrc musb-hdrc.1: USB Host mode controller at c882a800 using DMA, IRQ 19
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
NetWinder Floating Point Emulator V0.97 (double precision)
PMU: registered new PMU device of type 0
omap-iommu omap-iommu.0: ducati registered
omap-iommu omap-iommu.1: sys registered
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 232
alg: No test for stdrng (krng)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
nss_rng nss_rng: NSS Random Number Generator ver. 2.0
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
console [ttyO0] enabled
omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
brd: module loaded
loop: module loaded
ahci probe: devid name is ahci
ahci CAP register dump =0x6726ff80
Modified ahci CAP register dump =0x6f26ff80
ahci ahci.0: forcing PORTS_IMPL to 0x1
ahci: SSS flag set, parallel bus scan disabled
ahci ahci.0: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci ahci.0: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst
scsi0 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16
ahci probe: devid name is ahci
ahci CAP register dump =0x6726ff80
Modified ahci CAP register dump =0x6f26ff80
ahci ahci.1: forcing PORTS_IMPL to 0x1
ahci: SSS flag set, parallel bus scan disabled
ahci ahci.1: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci ahci.1: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst
scsi1 : ahci_platform
ata2: SATA max UDMA/133 mmio [mem 0x4a0ae000-0x4a0befff] port 0x100 irq 59
m25p80 spi1.0: w25x32 (4096 Kbytes)
Creating 5 MTD partitions on "spi_flash":
0x000000000000-0x000000020000 : "U-Boot-min"
0x000000020000-0x000000060000 : "U-Boot"
0x000000060000-0x000000062000 : "U-Boot Env"
0x000000062000-0x0000002e2000 : "Kernel"
0x0000002e2000-0x000000400000 : "File System"
omap2-nand driver initializing
ONFI param page 0 valid
ONFI flash detected
NAND device: Maf ID: 0x2c, Chip ID: 0xca (Micron, NAND 256MiB 3,3V 16-bit)
erasesize: 0x20000, writesize: 2048, oobsize: 64
omap2-nand: detected x16 NAND flash
Creating 7 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000020000 : "U-Boot-min"
0x000000020000-0x000000260000 : "U-Boot"
0x000000260000-0x000000280000 : "U-Boot Env"
0x000000280000-0x000000580000 : "U-Boot Logo"
0x000000580000-0x0000009c0000 : "Kernel"
0x0000009c0000-0x00000d1e0000 : "File System"
0x00000d1e0000-0x000010000000 : "Reserved"
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask fffffff8
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
davinci_mdio davinci_mdio.0: phy[2]: device 0:02, driver unknown
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver dm9601
usbcore: registered new interface driver cdc_acm
cdc_acm: v0.26:USB Abstract Control Model driver for USB modems and ISDN adapters
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
mice: PS/2 mouse device common for all mice
qt602240_ts 1-004a: __qt602240_read_reg: i2c transfer failed
qt602240_ts: probe of 1-004a failed with error -5
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v1.0.0)
OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
nss_aes_mod_init: loading NSS AES driver
nss-aes nss-aes: NSS AES hw accel rev: 3.2 (context 0 @0x41140000)
nss-aes nss-aes: NSS AES hw accel rev: 3.2 (context 1 @0x41141000)
nss-aes nss-aes: NSS AES hw accel rev: 3.2 (context 2 @0x411a0000)
nss-aes nss-aes: NSS AES hw accel rev: 3.2 (context 3 @0x411a1000)
ata2: SATA link down (SStatus 0 SControl 300)
nss_aes_probe: probe() done
nss_des_mod_init: loading NSS DES driver
nss-des nss-des: NSS DES hw accel rev: 2.2 (context 0 @0x41160000)
nss-des nss-des: NSS DES hw accel rev: 2.2 (context 1 @0x41161000)
ata1: SATA link down (SStatus 0 SControl 300)
nss_des_probe: probe() done
nss_sham_mod_init: loading NSS SHA/MD5 driver
nss-sham nss-sham: NSS SHA/MD5 hw accel rev: 4.03 (context 0 @0x41100000)
nss-sham nss-sham: NSS SHA/MD5 hw accel rev: 4.03 (context 1 @0x41101000)
nss-sham nss-sham: NSS SHA/MD5 hw accel rev: 4.03 (context 2 @0x411c0000)
nss-sham nss-sham: NSS SHA/MD5 hw accel rev: 4.03 (context 3 @0x411c1000)
nss_sham_probe: probe() done
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
notify_shm_drv: no DSP present (MULTIPROC_INVALIDID)
notify_init : notify drivercreated for remote proc id 1 at physical Address 0xbffd0000
usbcore: registered new interface driver snd-usb-audio
Registered tvp5158 audio codec
*** Forcing SW CTS!
asoc: tvp5158-hifi <-> davinci-mcasp.0 mapping ok
asoc: tlv320aic3x-hifi <-> davinci-mcasp.1 mapping ok
asoc: HDMI-DAI-CODEC <-> hdmi-dai mapping ok
ALSA device list:
#0: TI81XX SOUND0
#1: TI81XX SOUND1
TCP cubic registered
NET: Registered protocol family 17
Registering the dns_resolver key type
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omap_voltage_late_init: Voltage driver support not added
Power Management for TI81XX.
Detected MACID=8:0:28:32:7a:46
omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
CPSW phy found : id is : 0x4dd074
CPSW phy found : id is : 0x4dd074
IP-Config: Complete:
device=eth0, addr=192.168.107.167, mask=255.255.255.0, gw=192.168.107.254,
host=192.168.107.167, domain=, nis-domain=(none),
bootserver=192.168.107.86, rootserver=192.168.107.86, rootpath=
PHY: 0:01 - Link is Up - 0/Half
PHY: 0:01 - Link is Down
PHY: 0:00 - Link is Up - 100/Full
VFS: Mounted root (nfs filesystem) on device 0:15.
devtmpfs: mounted
Freeing init memory: 228K
INIT: version 2.88 booting
Mounting /dev/shm : Mounting /dev/pts : Mounting other filesystems : Mounting /dev/sda1 : mount: mounting /dev/sda1 on /media/sda1 failed: No such file or directory
Sync command ...Error opening /dev/fb0: No such file or directory
Starting udev
udev[116]: starting version 164
Starting Bootlog daemon: bootlogd.
Applying sync command
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org dm810x ttyO0
Arago 2012.10 dm810x ttyO0
dm810x login: root
root@dm810x:~# cd /opt/dvr_rdk/ti810x
root@dm810x:/opt/dvr_rdk/ti810x# ls
bin init.sh run.sh unload.sh
demo_ini kermod run_dvr.sh validate.sh
env_512M_128M.sh load.sh run_nvr.sh
firmware parseEnv.sh scripts
root@dm810x:/opt/dvr_rdk/ti810x# ./init.sh
*** Bootargs Validated for mem param ***
*** Bootargs Validated for notifyk.vpssm3 params ***
Kernel bootargs validated
numid=101,iface=MIXER,name='Left DAC Mux'
; type=ENUMERATED,access=rw------,values=1,items=3
; Item #0 'DAC_L1'
; Item #1 'DAC_L3'
; Item #2 'DAC_L2'
: values=2
numid=99,iface=MIXER,name='Right DAC Mux'
; type=ENUMERATED,access=rw------,values=1,items=3
; Item #0 'DAC_R1'
; Item #1 'DAC_R3'
; Item #2 'DAC_R2'
: values=2
[c6xdsp ] Remote Debug Shared Memory @ 0xbfff0000
[m3video] Remote Debug Shared Memory @ 0xbfff5020
[m3vpss ] Remote Debug Shared Memory @ 0xbfffa040
SysLink version : 2.20.02.20
SysLink module created on Date:Jun 23 2014 Time:17:59:52
Trace enabled
Trace SetFailureReason enabled
./lo Setting L3 bandwidth regulator for [HDVICP0 ] to [press=[3,3] BW=2000, WM Cycles=4000]
Setting DMM priority for [DUCATI ] to [0] ( 0x4e000624 = 0x08000000 )
Setting DMM priority for [HDVICP0 ] to [2] ( 0x4e000634 = 0x0000000a )
root@dm810x:/opt/dvr_rdk/ti810x# ./load.sh
Attached to slave procId 1.
Loaded file ../firmware/dvr_rdk_fw_m3vpss_512M_128M.xem3 on slave procId 1.
Started slave procId 1.
After Ipc_loadcallback status [0x00000000]
[m3vpss ] ISS Freq : 560 MHz
After Ipc_startcallback status [0x00000000]
[m3vpss ] ***** VPSS Firmware build time 18:23:11 Jun 23 2014 EDG gcc 3.0 mode
[m3vpss ] ***** SYSTEM : Frequency <ORG> - 200000000, <NEW> - 280000000
[m3vpss ] notify_attach rtnVal 0
[m3vpss ] initProxyServer rtnVal 0
[m3vpss ]
[m3vpss ] *** UTILS: CPU KHz = 560000 Khz ***
[m3vpss ]
[m3vpss ] 38: SYSTEM : System Common Init in progress !!!
[m3vpss ] 38: SYSTEM: IPC init in progress !!!
[m3vpss ] 39: SYSTEM: Attaching to [HOST] ...
[m3vpss ] 41: SYSTEM: Attaching to [HOST] ... SUCCESS !!!
Attached to slave procId 0.
Loaded file ../firmware/dvr_rdk_fw_m3video_512M_128M.xem3 on slave procId 0.
Started slave procId 0.
After Ipc_loadcallback status [0x00000000]
[m3video] ISS Freq : 560 MHz
After Ipc_startcallback status [0x00000000]
[m3vpss ] 390: SYSTEM: Attaching to [VIDEO-M3] ... SUCCESS !!!
[m3video] ***** VIDEO Firmware build time 18:25:29 Jun 23 2014 EDG gcc 3.0 mode
[m3vpss ] 390: SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP_2] ...
[m3video] ***** SYSTEM : Frequency <ORG> - 200000000, <NEW> - 280000000
[m3vpss ] 391: SYSTEM: Creating MsgQ [VPSS-M3_MSGQ] ...
[m3video]
[m3vpss ] 391: SYSTEM: Creating MsgQ [VPSS-M3_ACK_MSGQ] ...
DMA: Module install successful, device major num = 251
[m3vpss ] 393DRV: Module install successful
: SYSTEM: NotifyDRV: Module built on Jun 23 2014 18:00:58
register to [HOST] line 0, event 15 ...
[m3video]
[m3vpss ] 393: SYSTEM: Notify register to [VIDEO-M3] line 0, event 15 ...
[m3video] 385: SYSTEM : System Common Init in progress !!!
[m3vpss ] 393: SYSTEM: IPC init DONE !!!
[m3video] 385: SYSTEM: IPC init in progress !!!
[m3video] 385: SYSTEM: Attaching to [HOST] ...
[m3video] 388: SYSTEM: Attaching to [HOST] ... SUCCESS !!!
[m3video] 390: SYSTEM: Attaching to [VPSS-M3] ... SUCCESS !!!
[m3video] 390: SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP_1] ...
[m3video] 391: SYSTEM: Creating MsgQ [VIDEO-M3_MSGQ] ...
[m3video] 391: SYSTEM: Creating MsgQ [VIDEO-M3_ACK_MSGQ] ...
[m3video] 393: SYSTEM: Notify register to [HOST] line 0, event 15 ...
[m3video] 393: SYSTEM: Notify register to [VPSS-M3] line 0, event 15 ...
[m3vpss ] 399: MEM: Shared Region 2: Base = 0xb6310000, Length = 0x09210000 (146 MB)
[m3video] 393: SYSTEM: IPC init DONE !!!
[m3vpss ] 400: MEM: Shared Region 1: Base = 0x88000000, Length = 0x05a00000 (90 MB)
[m3video] 399: MEM: Shared Region 2: Base = 0xb6310000, Length = 0x09210000 (146 MB)
[m3vpss ] 401: SYSTEM : System Common Init Done !!!
[m3video] 400: MEM: Shared Region 1: Base = 0x88000000, Length = 0x05a00000 (90 MB)
[m3vpss ] 401: SYSTEM : System VPSS Init in progress !!!
[m3video] 402: SYSTEM : System Common Init Done !!!
[m3vpss ] === I2C0/2 Clk is active ===
[m3video] 402: SYSTEM : System Video Init in progress !!!
[m3vpss ] 407: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_0] in region 0 ...
[m3video] 402: SYSTEM : System Video Init Done !!!
[m3vpss ] 407: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_0] in region 0 ...
[m3video] 402: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_0] in region 0 ...
[m3vpss ] 407: SYSTEM: ListElem Shared Addr = 0xbf61b080
[m3video] 403: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_0] in region 0 ...
[m3vpss ] 409: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_1] in region 0 ...
[m3video] 403: SYSTEM: ListElem Shared Addr = 0xbf614680
[m3vpss ] 410: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_1] in region 0 ...
[m3video] 405: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_1] in region 0 ...
[m3vpss ] 410: SYSTEM: ListElem Shared Addr = 0xbf61e580
[m3video] 406: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_1] in region 0 ...
[m3video] 406: SYSTEM: ListElem Shared Addr = 0xbf617b80
[m3video] 412: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_19] in region 0 ...
[m3video] 412: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_19] in region 0 ...
[m3video] 413: SYSTEM: ListElem Shared Addr = 0xbf621a80
[m3video] 415: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_20] in region 0 ...
[m3video] 416: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_20] in region 0 ...
[m3video] 416: SYSTEM: ListElem Shared Addr = 0xbf647280
[m3video] 419: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_21] in region 0 ...
[m3video] 419: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_21] in region 0 ...
[m3video] 419: SYSTEM: ListElem Shared Addr = 0xbf66ca80
[m3vpss ] 426: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_19] in region 0 ...
[m3vpss ] 426: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_19] in region 0 ...
[m3vpss ] 426: SYSTEM: ListElem Shared Addr = 0xbf692280
[m3vpss ] 429: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_20] in region 0 ...
[m3vpss ] 429: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_20] in region 0 ...
[m3vpss ] 429: SYSTEM: ListElem Shared Addr = 0xbf6b7a80
[m3video] 434: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_24] in region 0 ...
[m3vpss ] 432: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_21] in region 0 ...
[m3video] 435: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_24] in region 0 ...
[m3vpss ] 432: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_21] in region 0 ...
[m3video] 435: SYSTEM: ListElem Shared Addr = 0xbf702a80
[m3vpss ] 433: SYSTEM: ListElem Shared Addr = 0xbf6dd280
[m3video] 437: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_25] in region 0 ...
[m3vpss ] 434: SYSTEM : HDVPSS Drivers Version: HDVPSS_01_00_01_37
[m3video] 437: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_25] in region 0 ...
[m3vpss ] 434: SYSTEM : FVID2 Init in progress !!!
[m3video] 438: SYSTEM: ListElem Shared Addr = 0xbf721500
[m3video] 439: HDVICP: Doing PRCM for IVAHD[0] ...
[m3video] 439: HDVICP: PRCM for IVAHD[0] ... DONE.
[m3video] 440: UTILS: DMA: HWI Create for INT62 !!!
[m3video] 441: SYSTEM : ISS Init in progress !!!
[m3vpss ] TILER_STATS: CNT :8BIT
[m3video] 441: SYSTEM : ISS Power-ON in progress !!!
[[module] vpss probe done.
m3video] 451: SYSTEM : ISS Power-ON in progress DONE !!!
[m3vpss ] TILER_STATS: CNT RESOLUTION: 16384 x 3776
[m3video] 451: SYSTEM : ISS Init in progress DONE !!!
[m3video] 451: VCOP BOOST BIT is Set
[m3vpss ] TILER_STATS: BUCKET RESOLUTION: 16384 x 3772
[m3video] 451: SYSTEM : VCOP [module] ti81xxfb probe done.
Init in progress !!!
[m3video] 451: SYSTEM : VCOP needs 172 B of memory !!!
[m3vpss ] TILER_STATS: NUM FREE BUCKETS: 1
[m3video] 453: SYSTEM : VCOP Init in progress DONE !!!
[m3video] 453: SYSTEM : Initializing Links !!!
[m3vpss ] TILER_STATS: NUM USED BUCKETS: 0
[c6xdsp ] Remote Debug Shared Memory @ 0xbfff0000
HDMI W1 rev 4.0
[m3video] RemotHDMI CEC Spec version 1.2
e Debug Shared Memory @ 0xbfff5020
[m3vpss ] Remote Debug Shared Memory @ 0xbfffa040
[m3vpss ] Received character 's'
[m3video] 453: SYSTEM : FREE SPACE : System Heap = 6264504 B, Mbx = 10240 msgs)
[m3vpss ] TILER_STATS: TOTAL FREE AREA: 61800448 (99 %)
[c6xdsp ] Remote Debug Shared Memory @ 0xbfff0000
[m3video] Remote Debug Shared Memory @ 0xbfff5020
[m3vpss ] Remote Debug Shared Memory @ 0xbfffa040
[m3video] Received character 's'
/opt/dvr_rdk/ti810x
[m3video] 453: SYSTEM : FREE SPACE : SR0 Heap = 5113472 B (4 MB)
[m3vpss ] TILER_STATS: TOTAL USED AREA: 0 (0 %)
[m3video] 453: SYSTEM : FREE SPACE : Frame Buffer = 153157504 B (146 MB)
[m3video] 453: SYSTEM : FREE SPACE : Bitstream Buffer = 94371712 B (89 MB)
[m3video] 454: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ...
[m3vpss ] TILER_STATS: CNT :16BIT
[m3video] 455: SYSTEM : FREE SPACE : Tiler 8-bit = 61800448 B (58 MB) - TILER ON
[m3vpss ] TILER_STATS: CNT RESOLUTION: 32768 x 1280
[m3video] 456: SYSTEM : FREE SPACE : Tiler 16-bit = 41943040 B (40 MB) - TILER ON
[m3vpss ] TILER_STATS: BUCKET RESOLUTION: 32768 x 1280
[m3video] 511: SYSTEM : Initializing Links ... DONE !!!
[m3vpss ] TILER_STATS: NUM FREE BUCKETS: 1
[m3vpss ] TILER_STATS: NUM USED BUCKETS: 0
[m3vpss ] TILER_STATS: TOTAL FREE AREA: 41943040 (100 %)
[m3vpss ] TILER_STATS: TOTAL USED AREA: 0 (0 %)
[m3vpss ] 516: SYSTEM : FVID2 Init in progress DONE !!!
[m3vpss ] 516: SYSTEM : Device Init in progress !!!
[m3vpss ] 597: SYSTEM : Device Init in progress DONE !!!
[m3vpss ] HDVPSS: is NOT Locked
[m3vpss ] 636: SYSTEM : System VPSS Init Done !!!
[m3vpss ] 637: UTILS: DMA: HWI Create for INT63 !!!
[m3vpss ] 637: SYSTEM : Initializing Links !!!
[m3vpss ] 637: SYSTEM : FREE SPACE : System Heap = 251488 B, Mbx = 10240 msgs)
[m3vpss ] 638: SYSTEM : FREE SPACE : SR0 Heap = 5113472 B (4 MB)
[m3vpss ] 638: SYSTEM : FREE SPACE : Frame Buffer = 148847488 B (141 MB)
[m3vpss ] 638: SYSTEM : FREE SPACE : Bitstream Buffer = 94371712 B (89 MB)
[m3vpss ] TILER_STATS: CNT :8BIT
[m3vpss ] TILER_STATS: CNT RESOLUTION: 16384 x 3776
[m3vpss ] TILER_STATS: BUCKET RESOLUTION: 16384 x 3772
[m3vpss ] TILER_STATS: NUM FREE BUCKETS: 1
[m3vpss ] TILER_STATS: NUM USED BUCKETS: 0
[m3vpss ] TILER_STATS: TOTAL FREE AREA: 61800448 (99 %)
[m3vpss ] TILER_STATS: TOTAL USED AREA: 0 (0 %)
[m3vpss ] TILER_STATS: CNT :16BIT
[m3vpss ] TILER_STATS: CNT RESOLUTION: 32768 x 1280
[m3vpss ] TILER_STATS: BUCKET RESOLUTION: 32768 x 1280
[m3vpss ] TILER_STATS: NUM FREE BUCKETS: 1
[m3vpss ] TILER_STATS: NUM USED BUCKETS: 0
[m3vpss ] TILER_STATS: TOTAL FREE AREA: 41943040 (100 %)
[m3vpss ] TILER_STATS: TOTAL USED AREA: 0 (0 %)
[m3vpss ] 639: SYSTEM : FREE SPACE : Tiler 8-bit = 61800448 B (58 MB) - TILER ON
[m3vpss ] 639: SYSTEM : FREE SPACE : Tiler 16-bit = 41943040 B (40 MB) - TILER ON
[m3vpss ] 778: SYSTEM : Initializing Links ... DONE !!!
[m3vpss ] 778: SYSTEM : Set Static L3 pressure for HDVPSS as High
ORG 0x46c00524: 0
NEW 0x46c00524: 2
root@dm810x:/opt/dvr_rdk/ti810x# ./run.sh
=========
Main Menu
=========
1: 4CH VCAP + VENC + VDEC + VDIS - Progressive SD Encode + Decode
2: 8CH <D1+CIF> VCAP + VENC + VDEC + VDIS - Progressive SD Encode + Decode
3: 16CH RT VCAP + VENC + VDEC + VDIS - Progressive SD Encode + Decode
4: 16CH NRT <D1+CIF> VCAP + VENC + VDEC + VDIS - Progressive SD Encode + Decode
5: VDEC + VDIS - SD/HD Decode ONLY
e: Exit
Enter Choice: 1
--------------- CHANNEL DETAILS-------------
Capture Channels => 4
Enc Channels => Primary 4, Secondary 4
Dec Channels => 4
Disp Channels => 8
-------------------------------------------
0: SYSTEM: System Common Init in progress !!!
0: SYSTEM: IPC init in progress !!!
12: SYSTEM: CPU [DSP] is NOT available on this platform !!!
12: SYSTEM: CPU [VIDEO-M3] syslink proc ID is [0] !!!
12: SYSTEM: CPU [VPSS-M3] syslink proc ID is [1] !!!
12: SYSTEM: CPU [HOST] syslink proc ID is [2] !!!
12: SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP_3] ...
14: SYSTEM: Creating MsgQ [HOST_MSGQ] ...
16: SYSTEM: Creating MsgQ [HOST_ACK_MSGQ] ...
17: SYSTEM: Opening MsgQ [VIDEO-M3_MSGQ] ...
18: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ...
19: SYSTEM: Notify register to [VIDEO-M3] line 0, event 15 ...
20: SYSTEM: Notify register to [VPSS-M3] line 0, event 15 ...
20: SYSTEM: IPC init DONE !!!
21: SYSTEM: Creating ListMP [HOST_IPC_OUT_24] in region 0 ...
24: SYSTEM: Creating ListMP [HOST_IPC_IN_24] in region 0 ...
26: SYSTEM: ListElem Shared Addr = 0x40580200
27: SYSTEM: Creating ListMP [HOST_IPC_OUT_25] in region 0 ...
29: SYSTEM: Creating ListMP [HOST_IPC_IN_25] in region 0 ...
30: SYSTEM: ListElem Shared Addr = 0x405b7000
32: SYSTEM: Creating ListMP [HOST_IPC_OUT_19] in region 0 ...
34: SYSTEM: Creating ListMP [HOST_IPC_IN_19] in region 0 ...
35: SYSTEM: ListElem Shared Addr = 0x405ede00
36: SYSTEM: Creating ListMP [HOST_IPC_OUT_20] in region 0 ...
38: SYSTEM: Creating ListMP [HOST_IPC_IN_20] in region 0 ...
39: SYSTEM: ListElem Shared Addr = 0x40631100
40: SYSTEM: Creating ListMP [HOST_IPC_OUT_21] in region 0 ...
42: SYSTEM: Creating ListMP [HOST_IPC_IN_21] in region 0 ...
44: SYSTEM: ListElem Shared Addr = 0x40674400
60: SYSTEM: System Common Init Done !!!
[host] HDMI Ctrl :Initializing
[HOST]
ThreadName:Vdis_hdmiControlThread_0,ThreadID:699
[host] HDMI Ctrl :Initialized
[host] HDMI Ctrl :Sink Connected
Enable file write (YES - y / NO - n) : n
File write DISABLED !!!
[HOST]
ThreadName:VcapVencVdecVdis_ipcBitsRecvFxn,ThreadID:700
AUDIO: Do you enable Audio <Y/N>: Y
-------- Starting Audio Capture ----------
Enter AUDIO: Enter number of channels to be encoded - [Valid values, 0 .. 4] : 0
Entered value = 0
AUDIO: Do you enable playback <Y/N>: Y
Enter Playback Device 0-AIC3x 1-HDMI Out [Valid values, 0 .. 1] : 1
Entered value = 1
AUDIO: Playback enabled for Ch 0 on HDMI device
[HOST]
ThreadName:App_captureTaskFxn_0,ThreadID:701
[HOST]
ThreadName:App_playbackTaskFxn_0,ThreadID:702
[FBDEV]
[FBDEV] FB: Starting !!!
[FBDEV] FB: Opened device [/dev/fb0] (fd=24) !!!
[FBDEV]
[FBDEV] Fix Screen Info
[FBDEV] ---------------
[FBDEV] Line Length - 1600
[FBDEV] Physical Address = 87a00000
[FBDEV] Buffer Length = 2097152
[FBDEV]
[FBDEV]
[FBDEV] Var Screen Info
[FBDEV] ---------------
[FBDEV] Xres - 800
[FBDEV] Yres - 600
[FBDEV] Xres Virtual - 800
[FBDEV] Yres Virtual - 600
[FBDEV] Bits Per Pixel - 16
[FBDEV] Pixel Clk - 6734
[FBDEV] Rotation - 0
[FBDEV]
[FBDEV]
[FBDEV] Reg Params Info
[FBDEV] ---------------
[FBDEV] region 0, postion 0 x 0, prioirty 1
[FBDEV] first 1, last 1
[FBDEV] sc en 1, sten en 0
[FBDEV] tran en 1, type 0, key 16777215
[FBDEV] blend 0, alpha 0
[FBDEV] bb en 0, alpha 0
[FBDEV]
[FBDEV]
[FBDEV] ### BUF SIZE = 960000 Bytes !!!
[FBDEV]
[FBDEV]
[FBDEV] Fix Screen Info
[FBDEV] ---------------
[FBDEV] Line Length - 1600
[FBDEV] Physical Address = 87a00000
[FBDEV] Buffer Length = 2097152
[FBDEV]
[FBDEV]
[FBDEV] Var Screen Info
[FBDEV] ---------------
[FBDEV] Xres - 800
[FBDEV] Yres - 600
[FBDEV] Xres Virtual - 800
[FBDEV] Yres Virtual - 600
[FBDEV] Bits Per Pixel - 16
[FBDEV] Pixel Clk - 6734
[FBDEV] Rotation - 0
[FBDEV]
[FBDEV]
[FBDEV] Reg Params Info
[FBDEV] ---------------
[FBDEV] region 0, postion 0 x 0, prioirty 1
[FBDEV] first 1, last 1
[FBDEV] sc en 1, sten en 0
[FBDEV] tran en 1, type 0, key 16777215
[FBDEV] blend 0, alpha 0
[FBDEV] bb en 0, alpha 0
[FBDEV]
[FBDEV]
[FBDEV] ### BUF SIZE = 960000 Bytes !!!
[FBDEV]
[FBDEV] grpx_fb_draw ...
[FBDEV] grpx_fb_draw ... Done !!!
[FBDEV] FB: Start DONE !!!
[FBDEV]
********* Entered usecase 4CH <8107> Enc/Dec OSD Enabled SCD Enabled
14394: MCFW : CPU Revision [ES1.0] !!!
VCAP: DEVICE-0 (0x58): Chip ID 0x5158, Rev 0x0002, Firmware 0x0000 !!!
VCAP: DEVICE-0 (0x58): Detected video (720x240@59Hz, 1) !!!
TVP5158: 0x58: Downloading patch ...
TVP5158: 0x58: Downloading patch ... DONE !!!
TVP5158: 0x58: 5158:0002:0302
[m3vpss ] 27382: CAPTURE: Create in progress !!!
[m3vpss ] 27393: CAPTURE: VIP0 PortA capture mode is [ 8-bit, Pixel-mux Embedded Sync] !!!
[m3vpss ] CAPTURE:Create args numBufsPerCh[5] < min[6]Overriding create args
[m3vpss ] 27440: CAPTURE: Non-mux Embedded Sync capture mode is [ 8-bit, Pixel-mux Embedded Sync] !!!
[m3vpss ] UTILS: DMA: Allocated CH (TCC) = 58 (58)
[m3vpss ] UTILS: DMA: 0 of 4: Allocated PaRAM = 58 (0x49004740)
[m3vpss ] UTILS: DMA: 1 of 4: Allocated PaRAM = 64 (0x49004800)
[m3vpss ] UTILS: DMA: 2 of 4: Allocated PaRAM = 65 (0x49004820)
[m3vpss ] UTILS: DMA: 3 of 4: Allocated PaRAM = 66 (0x49004840)
[m3vpss ] CAPTURE::HEAPID:0 USED:520
[m3vpss ] CAPTURE::HEAPID:4 USED:51646464
[m3vpss ] 27629: CAPTURE: Create Done !!!
[m3vpss ] 27630: NSF: Create in progress !!!
[m3vpss ] NSF::HEAPID:0 USED:128
[m3vpss ] NSF::HEAPID:1 USED:9152
[m3vpss ] NSF::HEAPID:4 USED:5406720
[m3vpss ] 27656: NSF: Create Done !!!
[m3vpss ] 27656: DEI : Create in progress !!!
[m3vpss ] DEI: Ch 0, Outformat is PROGRESSIVE
[m3vpss ] 27670: DEI: OUT0: 0: Format: PROGRESSIVE, 0xb9d95480, 704 x 480, 4 frames
[m3vpss ] DEI: Ch 1, Outformat is PROGRESSIVE
[m3vpss ] 27682: DEI: OUT0: 1: Format: PROGRESSIVE, 0xba029480, 704 x 480, 4 frames
[m3vpss ] DEI: Ch 2, Outformat is PROGRESSIVE
[m3vpss ] 27695: DEI: OUT0: 2: Format: PROGRESSIVE, 0xba2bd480, 704 x 480, 4 frames
[m3vpss ] DEI: Ch 3, Outformat is PROGRESSIVE
[m3vpss ] 27707: DEI: OUT0: 3: Format: PROGRESSIVE, 0xba551480, 704 x 480, 4 frames
[m3vpss ] DEI: Ch 0, Outformat is PROGRESSIVE
[m3vpss ] 27708: DEI: OUT1: 0: Format: PROGRESSIVE, 0x00010000, 704 x 480, 3 frames
[m3vpss ] DEI: Ch 1, Outformat is PROGRESSIVE
[m3vpss ] 27708: DEI: OUT1: 1: Format: PROGRESSIVE, 0x00010840, 704 x 480, 3 frames
[m3vpss ] DEI: Ch 2, Outformat is PROGRESSIVE
[m3vpss ] 27709: DEI: OUT1: 2: Format: PROGRESSIVE, 0x00011080, 704 x 480, 3 frames
[m3vpss ] DEI: Ch 3, Outformat is PROGRESSIVE
[m3vpss ] 27710: DEI: OUT1: 3: Format: PROGRESSIVE, 0x000118c0, 704 x 480, 3 frames
[m3vpss ] DEI: Ch 0, Outformat is PROGRESSIVE
[m3vpss ] 27712: DEI: OUT2: 0: Format: PROGRESSIVE, 0xba7e5480, 352 x 240, 3 frames
[m3vpss ] DEI: Ch 1, Outformat is PROGRESSIVE
[m3vpss ] 27714: DEI: OUT2: 1: Format: PROGRESSIVE, 0xba842180, 352 x 240, 3 frames
[m3vpss ] DEI: Ch 2, Outformat is PROGRESSIVE
[m3vpss ] 27716: DEI: OUT2: 2: Format: PROGRESSIVE, 0xba89ee80, 352 x 240, 3 frames
[m3vpss ] DEI: Ch 3, Outformat is PROGRESSIVE
[m3vpss ] 27718: DEI: OUT2: 3: Format: PROGRESSIVE, 0xba8fbb80, 352 x 240, 3 frames
[m3vpss ] 27724: DEI : Loading Up-scaling Co-effs
[m3vpss ] 27724: DEI : Co-effs Loading ... DONE !!!
[m3video] 27746: IPC_IN_M3 : Create in progress !!!
[m3vpss ] DEI:HEAPID:0 USED:64
[m3video] 27746: SYSTEM: Opening ListMP [VPSS-M3_IPC_OUT_0] ...
[m3vpss ] DEI:HEAPID:1 USED:9600
[m3video] 27746: SYSTEM: Opening ListMP [VPSS-M3_IPC_IN_0] ...
[m3vpss ] DEI:HEAPID:4 USED:13009920
[m3vpss ] 27725: DEI : Create Done !!!
[m3vpss ] 27729: DUP: 0: Format: PROGRESSIVE, 704 x 480
[m3vpss ] 27729: DUP: 1: Format: PROGRESSIVE, 704 x 480
[m3vpss ] 27729: DUP: 2: Format: PROGRESSIVE, 704 x 480
[m3vpss ] 27729: DUP: 3: Format: PROGRESSIVE, 704 x 480
[m3vpss ] 27730: DUP : Create Done !!!
[m3vpss ] 27731: NSF: Create in progress !!!
[m3video] 27749: IPC_IN_M3 : Create Done !!!
[m3video] 27750: ALG : Create in progress !!!
[m3vpss ] NSF::HEAPID:0 USED:128
[m3vpss ] NSF::HEAPID:1 USED:5632
[m3vpss ] NSF::HEAPID:4 USED:2027520
[m3vpss ] 27741: NSF: Create Done !!!
[m3vpss ] 27742: MERGE: 0: Format: PROGRESSIVE, 704 x 480
[m3vpss ] 27742: MERGE: 1: Format: PROGRESSIVE, 704 x 480
[m3vpss ] 27742: MERGE: 2: Format: PROGRESSIVE, 704 x 480
[m3vpss ] 27742: MERGE: 3: Format: PROGRESSIVE, 704 x 480
[m3vpss ] 27743: MERGE: 4: Format: PROGRESSIVE, 352 x 240
[m3vpss ] 27743: MERGE: 5: Format: PROGRESSIVE, 352 x 240
[m3vpss ] 27743: MERGE: 6: Format: PROGRESSIVE, 352 x 240
[m3vpss ] 27743: MERGE: 7: Format: PROGRESSIVE, 352 x 240
[m3vpss ] 27744: MERGE: 8: Format: PROGRESSIVE, 704 x 480
[m3vpss ] 27744: MERGE: 9: Format: PROGRESSIVE, 704 x 480
[m3vpss ] 27744: MERGE: 10: Format: PROGRESSIVE, 704 x 480
[m3vpss ] 27744: MERGE: 11: Format: PROGRESSIVE, 704 x 480
[m3vpss ] 27744: MERGE : Create Done !!!
[m3vpss ] 27744: IPC_OUT_M3 : Create in progress !!!
[m3vpss ] 27746: IPC_OUT_M3 : Create Done !!!
[m3video] 27762: ALG : Prev Link ID = 10000002 !!!
[m3video] 27763: OSD: Opening algorithm ... !!!
[m3video] 27774: OSD: Opening algorithm ... DONE !!!
[m3video] UTILS: DMA: Allocated CH (TCC) = 51 (51)
[m3video] UTILS: DMA: 0 of 8: Allocated PaRAM = 51 (0x49004660)
[m3video] UTILS: DMA: 1 of 8: Allocated PaRAM = 479 (0x49007BE0)
[m3video] UTILS: DMA: 2 of 8: Allocated PaRAM = 480 (0x49007C00)
[m3video] UTILS: DMA: 3 of 8: Allocated PaRAM = 481 (0x49007C20)
[m3video] UTILS: DMA: 4 of 8: Allocated PaRAM = 482 (0x49007C40)
[m3video] UTILS: DMA: 5 of 8: Allocated PaRAM = 483 (0x49007C60)
[m3video] UTILS: DMA: 6 of 8: Allocated PaRAM = 484 (0x49007C80)
[m3video] UTILS: DMA: 7 of 8: Allocated PaRAM = 485 (0x49007CA0)
[m3video] 27789: SCD: Opening algorithm ... !!!
[m3video] 27789: SCD: Opening algorithm ... DONE !!!
[HOST]
ThreadName:IpcBitsOutLink_tskMain_30000018,ThreadID:691
[host] 16457: IPC_BITS_OUT : Create in progress !!!
[host] IPC_BITSOUT:BitBuffer Alloc.ChID:0,Size:0x25F800
[host]
******* RingBuf 0 created ********
[host] IPCBITSOUTLINK:Translated Addr Virt:0x40a5c080 To Phy:0x88000080
[host]
###Bit buff of size from the SR # 1 : 2488320 / bufsize 414720, maxQueueDepth 50
[host] ###Bit buff BasePtr: 40A5C080 / PhyAddr 88000080
[host] IPC_BITSOUT:BitBuffer Alloc.ChID:1,Size:0x25F800
[host]
******* RingBuf 1 created ********
[host] IPCBITSOUTLINK:Translated Addr Virt:0x40cbb880 To Phy:0x8825f880
[host]
###Bit buff of size from the SR # 1 : 2488320 / bufsize 414720, maxQueueDepth 50
[host] ###Bit buff BasePtr: 40CBB880 / PhyAddr 8825F880
[host] IPC_BITSOUT:BitBuffer Alloc.ChID:2,Size:0x25F800
[host]
******* RingBuf 2 created ********
[host] IPCBITSOUTLINK:Translated Addr Virt:0x40f1b080 To Phy:0x884bf080
[host]
###Bit buff of size from the SR # 1 : 2488320 / bufsize 414720, maxQueueDepth 50
[host] ###Bit buff BasePtr: 40F1B080 / PhyAddr 884BF080
[host] IPC_BITSOUT:BitBuffer Alloc.ChID:3,Size:0x25F800
[host]
******* RingBuf 3 created ********
[host] IPCBITSOUTLINK:Translated Addr Virt:0x4117a880 To Phy:0x8871e880
[host]
###Bit buff of size from the SR # 1 : 2488320 / bufsize 414720, maxQueueDepth 50
[host] ###Bit buff BasePtr: 4117A880 / PhyAddr 8871E880
[host] 16795: IPC_BITS_OUT : Create Done !!!
[HOST]
ThreadName:IpcBitsOutLink_periodicTaskFxn_30000018,ThreadID:703
[m3video] UTILS: DMA: Allocated CH (TCC) = 56 (56)
[m3video] UTILS: DMA: 0 of 1: Allocated PaRAM = 56 (0x49004700)
[m3video] ALGLINK:HEAPID:0 USED:30672
[m3video] ALGLINK:HEAPID:3 USED:6294656
[m3video] 27806: ALG : Create Done !!!
[m3video] 28147: IPC_BITS_IN : Create in progress !!!
[m3video] 28147: SYSTEM: Opening ListMP [HOST_IPC_OUT_24] ...
[m3video] 28147: SYSTEM: Opening ListMP [HOST_IPC_IN_24] ...
[m3video] 28148: SYSTEM: Opening MsgQ [HOST_MSGQ] ...
[m3video] 28150: IPC_BITS_IN : Create Done !!!
[m3video] 28150: DECODE: Create in progress ... !!!
[m3video] DECLINK_H264:HEAPID:0 USED:4264
[m3video] DECLINK_H264:HEAPID:3 USED:1433600
[m3video] 28163: DECODE: Creating CH0 of 720 x 576 [PROGRESSIVE] [TILED ],target bitrate = 2000 Kbps ...
[m3video] DECLINK_H264:HEAPID:0 USED:2368
[m3video] DECLINK_H264:HEAPID:3 USED:1433600
[m3video] 28173: DECODE: Creating CH1 of 720 x 576 [PROGRESSIVE] [TILED ],target bitrate = 2000 Kbps ...
[m3video] DECLINK_H264:HEAPID:0 USED:2368
[m3video] DECLINK_H264:HEAPID:3 USED:1433600
[m3video] 28185: DECODE: Creating CH2 of 720 x 576 [PROGRESSIVE] [TILED ],target bitrate = 2000 Kbps ...
[m3video] DECLINK_H264:HEAPID:0 USED:2368
[m3video] DECLINK_H264:HEAPID:3 USED:1433600
[m3video] 28196: DECODE: Creating CH3 of 720 x 576 [PROGRESSIVE] [TILED ],target bitrate = 2000 Kbps ...
[m3video] 28197: DECODE: All CH Create ... DONE !!!
[host] IpcBitsInLink_tskMain:Entered[HOST]
ThreadName:IpcBitsInLink_tskMain_3000001a,ThreadID:689
[host] 16915: IPC_BITS_IN : Create in progress !!!
[host] 16915: IPC_BITS_IN : ListMPOpen start !!!
[host] 16915: SYSTEM: Opening ListMP [VIDEO-M3_IPC_OUT_24] ...
16917: SYSTEM: Opening ListMP [VIDEO-M3_IPC_IN_24] ...
[m3video] DECLINK:HEAPID:0 USED:11408
[m3video] DECLINK:HEAPID:3 USED:5734400
[m3video] 28200: DECODE: Create ... DONE !!!
[m3video] 28201: ENCODE: Create in progress ... !!!
[m3video] ENCLINK:INFO: !!!Number of output buffers for ch[8] set to [1]
[m3video] 28229: ENCODE: Creating CH0 of 704 x 480, pitch = (16384, 32768) [PROGRESSIVE] [TILED ], bitrate = 2000 Kbps, I-P Interval 1...
[host] 16918: IPC_BITS_IN : ListMPOpen done !!!
[host] 16919: IPC_BITS_IN : System_linkGetInfo done !!!
[host] 16920: IPC_BITS_IN : Create Done !!!
[HOST]
ThreadName:IpcBitsInLink_periodicTaskFxn_3000001a,ThreadID:704
[m3vpss ] 28273: IPC_IN_M3 : Create in progress !!!
[m3video] ENCLINK_H264:HEAPID:0 USED:11912
[m3vpss ] 28273: SYSTEM: Opening ListMP [VIDEO-M3_IPC_OUT_0] ...
[m3video] ENCLINK_H264:HEAPID:3 USED:45056
[m3vpss ] 28273: SYSTEM: Opening ListMP [VIDEO-M3_IPC_IN_0] ...
[m3video] 28233: ENCODE: Creating CH1 of 704 x 480, pitch = (16384, 32768) [PROGRESSIVE] [TILED ], bitrate = 2000 Kbps, I-P Interval 1...
[m3vpss ] 28274: SYSTEM: Opening MsgQ [VIDEO-M3_MSGQ] ...
[m3vpss ] 28276: IPC_IN_M3 : Create Done !!!
[m3vpss ] 28277: MERGE: 0: Format: PROGRESSIVE, 704 x 480
[m3video] ENCLINK_H264:HEAPID:0 USED:11912
[m3vpss ] 28277: MERGE: 1: Format: PROGRESSIVE, 704 x 480
[m3video] ENCLINK_H264:HEAPID:3 USED:45056
[m3vpss ] 28277: MERGE: 2: Format: PROGRESSIVE, 704 x 480
[m3video] 28237: ENCODE: Creating CH2 of 704 x 480, pitch = (16384, 32768) [PROGRESSIVE] [TILED ], bitrate = 2000 Kbps, I-P Interval 1...
[m3vpss ] 28277: MERGE: 3: Format: PROGRESSIVE, 704 x 480
[m3vpss ] 28277: MERGE: 4: Format: PROGRESSIVE, 720 x 576
[m3vpss ] 28278: MERGE: 5: Format: PROGRESSIVE, 720 x 576
[m3video] ENCLINK_H264:HEAPID:0 USED:11912
[m3vpss ] 28278: MERGE: 6: Format: PROGRESSIVE, 720 x 576
[m3video] ENCLINK_H264:HEAPID:3 USED:45056
[m3vpss ] 28278: MERGE: 7: Format: PROGRESSIVE, 720 x 576
[m3video] 28240: ENCODE: Creating CH3 of 704 x 480, pitch = (16384, 32768) [PROGRESSIVE] [TILED ], bitrate = 2000 Kbps, I-P Interval 1...
[m3vpss ] 28278: MERGE : Create Done !!!
[m3vpss ] 28282: DUP: 0: Format: PROGRESSIVE, 704 x 480
[m3video] ENCLINK_H264:HEAPID:0 USED:11912
[m3vpss ] 28282: DUP: 1: Format: PROGRESSIVE, 704 x 480
[m3video] ENCLINK_H264:HEAPID:3 USED:45056
[m3vpss ] 28282: DUP: 2: Format: PROGRESSIVE, 704 x 480
[m3video] 28244: ENCODE: Creating CH4 of 352 x 240, pitch = (352, 352) [PROGRESSIVE] [NON-TILED ], bitrate = 500 Kbps, I-P Interval 1...
[m3vpss ] 28282: DUP: 3: Format: PROGRESSIVE, 704 x 480
[m3vpss ] 28282: DUP: 4: Format: PROGRESSIVE, 720 x 576
[m3vpss ] 28282: DUP: 5: Format: PROGRESSIVE, 720 x 576
[m3video] ENCLINK_H264:HEAPID:0 USED:11912
[m3vpss ] 28282: DUP: 6: Format: PROGRESSIVE, 720 x 576
[m3video] ENCLINK_H264:HEAPID:3 USED:503808
[m3vpss ] 28283: DUP: 7: Format: PROGRESSIVE, 720 x 576
[m3video] 28248: ENCODE: Creating CH5 of 352 x 240, pitch = (352, 352) [PROGRESSIVE] [NON-TILED ], bitrate = 500 Kbps, I-P Interval 1...
[m3vpss ] 28284: DUP : Create Done !!!
[m3vpss ] 28284: SWMS: Create in progress !!!
[m3vpss ] UTILS: DMA: Allocated CH (TCC) = 59 (59)
[m3video] ENCLINK_H264:HEAPID:0 USED:11912
[m3vpss ] UTILS: DMA: 0 of 1: Allocated PaRAM = 59 (0x49004760)
[m3video] ENCLINK_H264:HEAPID:3 USED:503808
[m3vpss ] SWMS: instance 0, sc id 4, start win 0 end win 17
[m3video] 28252: ENCODE: Creating CH6 of 352 x 240, pitch = (352, 352) [PROGRESSIVE] [NON-TILED ], bitrate = 500 Kbps, I-P Interval 1...
[m3vpss ] 28326: SWMS0 : Loading Vertical Co-effs (UPSCALE)x ...
[m3vpss ] 28326: SWMS0 : Loading Horizontal Co-effs (UPSCALE)x ...
[m3vpss ] 28327: SWMS : Co-effs Loading ... DONE !!!
[m3video] ENCLINK_H264:HEAPID:0 USED:11912
[m3video] ENCLINK_H264:HEAPID:3 USED:503808
[m3vpss ] AVSYNC:WARNING!! Application wrongly configureddisplayID[-1]. Reseting to correct displayID[0]
[m3video] 28256: ENCODE: Creating CH7 of 352 x 240, pitch = (352, 352) [PROGRESSIVE] [NON-TILED ], bitrate = 500 Kbps, I-P Interval 1...
[m3vpss ] 28327: SWMS: 0: Format: PROGRESSIVE, 704 x 480
[m3vpss ] 28328: SWMS: 1: Format: PROGRESSIVE, 704 x 480
[m3vpss ] 28328: SWMS: 2: Format: PROGRESSIVE, 704 x 480
[m3video] ENCLINK_H264:HEAPID:0 USED:11912
[m3vpss ] 28328: SWMS: 3: Format: PROGRESSIVE, 704 x 480
[m3video] ENCLINK_H264:HEAPID:3 USED:503808
[m3vpss ] 28328: SWMS: 4: Format: PROGRESSIVE, 720 x 576
[m3video] 28260: ENCODE: Creating CH8 of 704 x 480, pitch = (704, 704) [PROGRESSIVE] [NON-TILED ], bitrate = 100 Kbps, I-P Interval 0...
[m3vpss ] 28328: SWMS: 5: Format: PROGRESSIVE, 720 x 576
[m3vpss ] 28328: SWMS: 6: Format: PROGRESSIVE, 720 x 576
[m3vpss ] 28328: SWMS: 7: Format: PROGRESSIVE, 720 x 576
[m3video] ENCLINK_JPEG:HEAPID:0 USED:2064
[m3vpss ] 28328: SWMS : ******* Configuring clock 30 secs...
[m3video] 28260: ENCODE: Creating CH9 of 704 x 480, pitch = (704, 704) [PROGRESSIVE] [NON-TILED ], bitrate = 100 Kbps, I-P Interval 0...
[m3vpss ] 28328: SWMS0 : Loading Vertical Co-effs (11/16)x ...
[m3vpss ] 28328: SWMS0 : Loading Horizontal Co-effs (7/16)x ...
[m3vpss ] 28329: SWMS : Co-effs Loading ... DONE !!!
[m3video] ENCLINK_JPEG:HEAPID:0 USED:2064
[m3vpss ]
[m3vpss ] *** [SWMS0] Mosaic Parameters ***
[m3vpss ]
[m3vpss ] Output FPS: 30
[m3vpss ]
[m3vpss ] Win | Ch | Input | Input | Input | Input | Output | Output | Output | Output | Scan | Low Cost | SWMS | Data | Blank |
[m3vpss ] Num | Num | Start X, Y | Width x Height | Pitch Y / C | Memory Type | Start X, Y | Width x Height | Pitch Y / C | Memory Type | Fmt | ON / OFF | Inst | Format| Frame |
[m3vpss ] ------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
[m3video] 28261: ENCODE: Creating CH10 of 704 x 480, pitch = (704, 704) [PROGRESSIVE] [NON-TILED ], bitrate = 100 Kbps, I-P Interval 0...
[m3vpss ] 0 | 0 | 0, 0 | 704 x 240 | 2816 / 2816 | NON-TILED | 0, 0 | 320 x 180 | 1280 / 1280 | NON-TILED | PROGRESSIVE | ON | 0 | 422I | OFF |
[m3vpss ] 1 | 1 | 0, 0 | 704 x 240 | 2816 / 2816 | NON-TILED | 320, 0 | 320 x 180 | 1280 / 1280 | NON-TILED | PROGRESSIVE | ON | 0 | 422I | OFF |
[m3vpss ] 2 | 2 | 0, 0 | 704 x 240 | 2816 / 2816 | NON-TILED | 640, 0 | 320 x 180 | 1280 / 1280 | NON-TILED | PROGRESSIVE | ON | 0 | 422I | OFF |
[m3video] ENCLINK_JPEG:HEAPID:0 USED:2064
[m3vpss ] 3 | 3 | 0, 0 | 704 x 240 | 2816 / 2816 | NON-TILED | 960, 0 | 320 x 180 | 1280 / 1280 | NON-TILED | PROGRESSIVE | ON | 0 | 422I | OFF |
[m3video] 28262: ENCODE: Creating CH11 of 704 x 480, pitch = (704, 704) [PROGRESSIVE] [NON-TILED ], bitrate = 100 Kbps, I-P Interval 0...
[m3vpss ] 4 | 4 | 0, 0 | 720 x 576 | 16384 / 32768 | TILED | 0, 180 | 320 x 180 | 1280 / 1280 | NON-TILED | PROGRESSIVE | ON | 0 | 420SP | OFF |
[m3vpss ] 5 | 5 | 0, 0 | 720 x 576 | 16384 / 32768 | TILED | 320, 180 | 320 x 180 | 1280 / 1280 | NON-TILED | PROGRESSIVE | ON | 0 | 420SP | OFF |
[m3vpss ] 6 | 6 | 0, 0 | 720 x 576 | 16384 / 32768 | TILED | 640, 180 | 320 x 180 | 1280 / 1280 | NON-TILED | PROGRESSIVE | ON | 0 | 420SP | OFF |
[m3video] ENCLINK_JPEG:HEAPID:0 USED:2064
[m3vpss ] 7 | 7 | 0, 0 | 720 x 576 | 16384 / 32768 | TILED | 960, 180 | 320 x 180 | 1280 / 1280 | NON-TILED | PROGRESSIVE | ON | 0 | 420SP | OFF |
[m3video] 28262: ENCODE: All CH Create ... DONE !!!
[m3vpss ]
[m3video] ENCLINK:HEAPID:0 USED:103592
[m3vpss ] SWMS:HEAPID:0 USED:224
[m3video] ENCLINK:HEAPID:2 USED:5426432
[m3vpss ] SWMS:HEAPID:1 USED:47296
[m3video] ENCLINK:HEAPID:3 USED:2195456
[m3vpss ] SWMS:HEAPID:4 USED:6912000
[m3video] 28263: ENCODE: Create ... DONE !!!
[m3vpss ] 28332: SWMS: Create Done !!!
[m3video] 28264: IPC_BITS_OUT : Create in progress !!!
[m3vpss ] 28333: DISPLAY: Create in progress !!!
[m3vpss ] 28334: DISPLAY: Create Done !!!
[m3vpss ] 28334: DISPLAY: Create in progress !!!
[m3video] 28266: IPC_BITS_OUT : Create Done !!!
[m3vpss ] 28335: DISPLAY: 43: Field Separate Mode ENABLED for Que 0 !!!
[m3video] 28271: IPC_OUT_M3 : Create in progress !!!
[m3vpss ] 28336: DISPLAY: Create Done !!!
[m3video] 28272: IPC_OUT_M3 : Create Done !!!
[m3vpss ] 28344: DISPLAY: Start in progress !!!
By testing, we should use two stage to boot-up then it will be successful.
I have one more question
Q1. I can boot up successfully and execute the application below
2: 8CH <D1+CIF> VCAP + VENC + VDEC + VDIS - Progressive SD Encode + Decode
and it looks like it doesn't "real" 8ch D1/CIF
because I observer the following
*** Encode Bitstream Received Statistics ***
and found in the beginning
CH | Bitrate (Kbps) | FPS | Key-frame FPS | Width (max/min) | Height (max/min) | Latency (max/min)
--------------------------------------------------------------------------------------------------
0 | 1769.74 | 27.2 | 0.9 | 704 / 704 | 480 / 480 | 210 / 41
1 | 1772.93 | 27.2 | 0.9 | 704 / 352 | 480 / 240 | 216 / 47
2 | 1773.34 | 27.2 | 0.9 | 704 / 352 | 480 / 240 | 218 / 50
3 | 1773.24 | 27.2 | 0.9 | 704 / 352 | 480 / 240 | 219 / 52
4 | 1768.64 | 27.2 | 0.9 | 704 / 704 | 480 / 480 | 166 / 40
5 | 1770.17 | 27.2 | 0.9 | 704 / 352 | 480 / 240 | 171 / 40
6 | 1770.36 | 27.2 | 0.9 | 704 / 352 | 480 / 240 | 181 / 40
7 | 1771.78 | 27.2 | 0.9 | 704 / 352 | 480 / 240 | 184 / 40
8 | 442.82 | 27.2 | 0.9 | 352 / 176 | 240 / 120 | 112 / 37
9 | 443.58 | 27.2 | 0.9 | 352 / 176 | 240 / 120 | 115 / 39
10 | 443.45 | 27.2 | 0.9 | 352 / 176 | 240 / 120 | 115 / 39
11 | 443.44 | 27.2 | 0.9 | 352 / 176 | 240 / 120 | 112 / 39
12 | 442.39 | 27.2 | 0.9 | 352 / 176 | 240 / 120 | 165 / 28
13 | 442.54 | 27.2 | 0.9 | 352 / 176 | 240 / 120 | 165 / 28
14 | 443.47 | 27.2 | 0.9 | 352 / 176 | 240 / 120 | 165 / 28
15 | 443.46 | 27.2 | 0.9 | 352 / 176 | 240 / 120 | 165 / 28
and 3~4 minutes later
CH | Bitrate (Kbps) | FPS | Key-frame FPS | Width (max/min) | Height (max/min) | Latency (max/min)
--------------------------------------------------------------------------------------------------
0 | 1949.84 | 30.0 | 1.0 | 704 / 704 | 480 / 480 | 117 / 43
1 | 1948.57 | 30.0 | 1.0 | 352 / 352 | 240 / 240 | 117 / 47
2 | 1948.35 | 30.0 | 1.0 | 352 / 352 | 240 / 240 | 117 / 48
3 | 1948.48 | 30.0 | 1.0 | 352 / 352 | 240 / 240 | 117 / 49
4 | 1949.70 | 30.0 | 1.0 | 704 / 704 | 480 / 480 | 118 / 38
5 | 1948.52 | 30.0 | 1.0 | 352 / 352 | 240 / 240 | 118 / 40
6 | 1948.60 | 30.0 | 1.0 | 352 / 352 | 240 / 240 | 118 / 40
7 | 1948.62 | 30.0 | 1.0 | 352 / 352 | 240 / 240 | 118 / 40
8 | 487.33 | 30.0 | 1.0 | 176 / 176 | 120 / 120 | 108 / 36
9 | 487.33 | 30.0 | 1.0 | 176 / 176 | 120 / 120 | 108 / 38
10 | 487.35 | 30.0 | 1.0 | 176 / 176 | 120 / 120 | 108 / 38
11 | 487.31 | 30.0 | 1.0 | 176 / 176 | 120 / 120 | 108 / 31
12 | 487.36 | 30.0 | 1.0 | 176 / 176 | 120 / 120 | 108 / 25
13 | 487.32 | 30.0 | 1.0 | 176 / 176 | 120 / 120 | 108 / 27
14 | 487.33 | 30.0 | 1.0 | 176 / 176 | 120 / 120 | 108 / 27
15 | 487.32 | 30.0 | 1.0 | 176 / 176 | 120 / 120 | 108 / 27
Is there something wrong??
see attach for full log6114.COM3_2014_11_27.log
we got the answer as below
after checking following description inside DM81xx_DVR_RDK_Demo_Guide.pdf
c: Change 8CH modes (8CH usecase ONLY!!!!)
In 8 CH usecase, there are different modes of captured resolutions like 2D1 + 6 CIF, 8 D1 etc. These modes can be
selected using “Change modes” .
and we found the topic in DM810x_DVR_RDK_UseCaseGuide_4D1_8CIF_16CIF_DVR.pdf
Use Case 1: CH0 and CH4 will be D1, others will be CIF. No dynamic switching between D1 and CIF channels,
8CH QCIF H264 30fps, 8CH D1 JPEG 1fps