Hi,
I am currently using ndk_2_21_01_38 version for CCS v5.5.0.00077 and this gives me the following error:
"An error occurred while collecting items to be installed session context was:(profile=epp.package.cpp, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=). Problems downloading artifact: osgi.bundle,com.ti.rtsc.NDK.product_2.21.1.38,2.21.1.38."
I went through TI forum and understood that this NDK version is not compatible with CCS v5.5. I am sorry if this question has been answered before,but I am still not clear about which NDK version has to be installed. I also made sure that I installed CCS for windows 8 in Windows 7 compatible mode and also as an administrator.
Thanks for your advice!