This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BeagleBone Black simple device driver

Hi, guys!

I've been trying for three weeks now to write a simple device driver on a BeagleBone Black. I wanted to toggle pin GPIO0_7 on header P9. I've read tons of books on Linux device drivers and I still cannot figure out what approach should I use.

I'm trying to use DIRECT REGISTER ACCESS just like we're doing this on an MSP430 for example:

P1DIR = BIT1 | BIT2;

P1OUT |= BIT1 | BIT2;

Any idea how to do this in Beaglebone Debian or Ubuntu?

So far: I've been trying to use request_mem_region( ) or request_region( ) and the header files from BBB StarterWare. No luck - the pin does not toggle. Furthermore - each module I want to use first I remove it from the /boot/uboot/dtbs/am335x-boneblack.dtb and sometimes drivers that use the dtb crash. I can register a device node in /dev directory but dunno where to go on from there ...

Thanks in advance!