Other Parts Discussed in Thread: DM385
hello TI-friends,
Is it possible to achieve the spec 8xD1 30fps encoding on dm385 ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DM385
hello TI-friends,
Is it possible to achieve the spec 8xD1 30fps encoding on dm385 ?
hi Eason,
I need to use DVRRDK 4.1 to prove that. After running the application below
=========
Main Menu
=========
1: 4CH VCAP + VENC + VDEC + VDIS - Progressive SD Encode + Decode
2: 8CH <D1+CIF> VCAP + VENC + VDEC + VDIS - Progressive SD Encode + Decode
3: 16CH RT VCAP + VENC + VDEC + VDIS - Progressive SD Encode + Decode
4: 16CH NRT <D1+CIF> VCAP + VENC + VDEC + VDIS - Progressive SD Encode + Decode
5: VDEC + VDIS - SD/HD Decode ONLY
I use "case 2" for the beginning, I want to remove the path of 8xD1 MJPG. So I modify the code as below
in multich_progressive_8ch_vcap_venc_vdec_vdis.c
/*************** MJPEG DEI1_VIP1_SC Settings ******************************/
set_DEI_BYPASS_VIP1_SC_MJPEG_params(
&deiPrm[DEI_BYPASS_VIP1_SC_FOR_MJPEG],
dupId[CAPTURE_DUP_LINK_IDX],
3,
SYSTEM_LINK_ID_INVALID,
mergeId[D1_CIF_QCIF_MERGE_LINK_IDX]); => SYSTEM_LINK_ID_INVALID);
/* CH0..7 - D1 FOR MJPEG */
mergePrm[D1_CIF_QCIF_MERGE_LINK_IDX].inQueParams[2].prevLinkId =
gVcapModuleContext.deiId[DEI_BYPASS_VIP1_SC_FOR_MJPEG]; ==> SYSTEM_LINK_ID_INVALID;
//gVcapModuleContext.nsfId[NSF_AFTER_SCALAR_LINK];
mergePrm[D1_CIF_QCIF_MERGE_LINK_IDX].inQueParams[2].prevLinkQueId =
DEI_LINK_OUT_QUE_VIP_SC; ==> 0;
mergePrm[D1_CIF_QCIF_MERGE_LINK_IDX].notifyNextLink = TRUE;
mergePrm[D1_CIF_QCIF_MERGE_LINK_IDX].numInQue = 3; ==> 2
and I got following messages
[m3vpss ] CAPTURE : Capture FPS: 0.0 fps ... in 4294952.7 secs
[m3vpss ] 14691: Assertion @ Line: 61 in links_common/system/system_linkApi.c: procId < SYSTEM_PROC_MAX : failed !!!
[m3vpss ] 14695: CAPTURE: Dynamic resolution change: width: 720, height: 480!
Please help me that~ thanks